Status Reg data structure.
More...
Status Reg data structure.
Definition at line 131 of file LTC681x.h.
◆ flags
Byte array that contains the uv/ov flag data.
Definition at line 134 of file LTC681x.h.
◆ mux_fail
Mux self test status flag.
Definition at line 135 of file LTC681x.h.
◆ pec_match
If a PEC error was detected during most recent read cmd.
Definition at line 137 of file LTC681x.h.
◆ stat_codes
| uint16_t st::stat_codes[4] |
◆ thsd
Thermal shutdown status.
Definition at line 136 of file LTC681x.h.
The documentation for this struct was generated from the following file: