IC register structure.
More...
IC register structure.
Definition at line 141 of file LTC681x.h.
◆ rx_data
| uint8_t ic_register::rx_data[8] |
Stores received data.
Definition at line 144 of file LTC681x.h.
◆ rx_pec_match
| uint8_t ic_register::rx_pec_match |
If a PEC error was detected during most recent read cmd.
Definition at line 145 of file LTC681x.h.
◆ tx_data
| uint8_t ic_register::tx_data[6] |
Stores data to be transmitted.
Definition at line 143 of file LTC681x.h.
The documentation for this struct was generated from the following file: