The alarm conditions which cause the LTC3335 to activate the /INT pin.
More...
The alarm conditions which cause the LTC3335 to activate the /INT pin.
Definition at line 152 of file LTC3335.h.
|
| unsigned | ac_on_time_overflow:1 |
| | AC(ON) time operating fault (tAC > tFS) due to improperly chosen inductor value timing out the AC(ON) measurement. More...
|
| |
| unsigned | coulomb_counter_overflow:1 |
| | Coulomb counter operating fault due to an improperly chosen prescalar causing the ripple counter to overflow. More...
|
| |
| unsigned | alarm_trip:1 |
| | Accumulator value has met or exceeded the alarm threshold value. More...
|
| |
| unsigned | unused:5 |
| |
◆ ac_on_time_overflow
| unsigned LTC3335_ALARM_TYPE::ac_on_time_overflow |
AC(ON) time operating fault (tAC > tFS) due to improperly chosen inductor value timing out the AC(ON) measurement.
Definition at line 154 of file LTC3335.h.
◆ alarm_trip
| unsigned LTC3335_ALARM_TYPE::alarm_trip |
Accumulator value has met or exceeded the alarm threshold value.
Definition at line 156 of file LTC3335.h.
◆ coulomb_counter_overflow
| unsigned LTC3335_ALARM_TYPE::coulomb_counter_overflow |
Coulomb counter operating fault due to an improperly chosen prescalar causing the ripple counter to overflow.
Definition at line 155 of file LTC3335.h.
◆ unused
| unsigned LTC3335_ALARM_TYPE::unused |
The documentation for this struct was generated from the following file: