![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Copyright 2018(c) Analog Devices, Inc. More...
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Library File
Definition in file hex_file_parser.cpp.
Go to the source code of this file.
Functions | |
| uint8_t | ascii_to_hex (uint8_t ascii) |
| uint8_t | filter_terminations (uint8_t(*get_data)(void)) |
| uint8_t | detect_colons (uint8_t(*get_data)(void)) |
| void | reset_parse_hex () |
| uint8_t | parse_hex (uint8_t(*get_data)(void)) |
| uint16_t | parse_records (uint8_t *in_data, uint16_t in_length, tRecordHeaderLengthAndType **out_records) |
| pRecordHeaderLengthAndType | parse_record (uint8_t(*get_data)(void)) |
| pRecordHeaderLengthAndType | print_record (pRecordHeaderLengthAndType(*get_record)(void)) |
Macros | |
| #define | DEBUG_PARSE_DATA 0 |
| #define | PARSE_DATA_LEN 64 |
Variables | |
| static uint8_t | parse_data [PARSE_DATA_LEN] |
| static uint16_t | parse_data_length = 0 |
| static uint16_t | parse_data_position = 0 |
| uint8_t ascii_to_hex | ( | uint8_t | ascii | ) |
Definition at line 48 of file hex_file_parser.cpp.
| uint8_t detect_colons | ( | uint8_t(*)(void) | get_data | ) |
Definition at line 63 of file hex_file_parser.cpp.
| uint8_t filter_terminations | ( | uint8_t(*)(void) | get_data | ) |
Definition at line 53 of file hex_file_parser.cpp.
| uint8_t parse_hex | ( | uint8_t(*)(void) | get_data | ) |
Definition at line 95 of file hex_file_parser.cpp.
| pRecordHeaderLengthAndType parse_record | ( | uint8_t(*)(void) | get_data | ) |
Definition at line 213 of file hex_file_parser.cpp.
| uint16_t parse_records | ( | uint8_t * | in_data, |
| uint16_t | in_length, | ||
| tRecordHeaderLengthAndType ** | out_records | ||
| ) |
Definition at line 190 of file hex_file_parser.cpp.
| pRecordHeaderLengthAndType print_record | ( | pRecordHeaderLengthAndType(*)(void) | get_record | ) |
Definition at line 255 of file hex_file_parser.cpp.
| void reset_parse_hex | ( | void | ) |
Definition at line 79 of file hex_file_parser.cpp.
| #define DEBUG_PARSE_DATA 0 |
Definition at line 45 of file hex_file_parser.cpp.
| #define PARSE_DATA_LEN 64 |
Definition at line 46 of file hex_file_parser.cpp.
|
static |
Definition at line 75 of file hex_file_parser.cpp.
|
static |
Definition at line 76 of file hex_file_parser.cpp.
|
static |
Definition at line 77 of file hex_file_parser.cpp.