Definition at line 36 of file LT_Wire.h.
|
|
| | LT_TwoWire () |
| |
| void | begin (uint32_t speed) |
| | Initiate Prep 10000 to 400000. More...
|
| |
| uint8_t | requestFrom (uint8_t address, uint8_t *acceptBuffer, uint16_t quantity) |
| | Read from a slave I2C device. More...
|
| |
| uint8_t | requestFrom (uint8_t address, uint8_t *acceptBuffer, uint16_t quantity, uint8_t sendStop) |
| | Read from a slave I2C device. More...
|
| |
| uint8_t | requestFrom (int address, uint8_t *acceptBuffer, int quantity) |
| | Read from a slave I2C device. More...
|
| |
| uint8_t | requestFrom (int address, uint8_t *acceptBuffer, int quantity, int sendStop) |
| | Read from a slave I2C device. More...
|
| |
◆ begin()
| void LT_TwoWire::begin |
( |
uint32_t |
speed | ) |
|
Initiate Prep 10000 to 400000.
- Returns
- void
Definition at line 52 of file LT_Wire.cpp.
◆ requestFrom() [1/4]
| uint8_t LT_TwoWire::requestFrom |
( |
uint8_t |
address, |
|
|
uint8_t * |
acceptBuffer, |
|
|
uint16_t |
quantity |
|
) |
| |
Read from a slave I2C device.
- Returns
- number of bytes read. If different from quantity, something bad happened.
- Parameters
-
| address | 7-bit I2C address |
| acceptBuffer | buffer pointer to fill |
| quantity | anticipated length of read |
Definition at line 67 of file LT_Wire.cpp.
◆ requestFrom() [2/4]
| uint8_t LT_TwoWire::requestFrom |
( |
uint8_t |
address, |
|
|
uint8_t * |
acceptBuffer, |
|
|
uint16_t |
quantity, |
|
|
uint8_t |
sendStop |
|
) |
| |
Read from a slave I2C device.
- Returns
- number of bytes read. If different from quantity, something bad happened.
- Parameters
-
| address | 7-bit I2C address |
| acceptBuffer | buffer pointer to fill |
| quantity | anticipated length of read |
| sendStop | whether to STOP or anticipate a repeated START |
Definition at line 58 of file LT_Wire.cpp.
◆ requestFrom() [3/4]
| uint8_t LT_TwoWire::requestFrom |
( |
int |
address, |
|
|
uint8_t * |
acceptBuffer, |
|
|
int |
quantity |
|
) |
| |
Read from a slave I2C device.
- Returns
- number of bytes read. If different from quantity, something bad happened.
- Parameters
-
| address | 7-bit I2C address |
| acceptBuffer | buffer pointer to fill |
| quantity | anticipated length of read |
Definition at line 72 of file LT_Wire.cpp.
◆ requestFrom() [4/4]
| uint8_t LT_TwoWire::requestFrom |
( |
int |
address, |
|
|
uint8_t * |
acceptBuffer, |
|
|
int |
quantity, |
|
|
int |
sendStop |
|
) |
| |
Read from a slave I2C device.
- Returns
- number of bytes read. If different from quantity, something bad happened.
- Parameters
-
| address | 7-bit I2C address |
| acceptBuffer | buffer pointer to fill |
| quantity | anticipated length of read |
| sendStop | whether to STOP or anticipate a repeated START |
Definition at line 77 of file LT_Wire.cpp.
◆ LT_TwoWire()
| LT_TwoWire::LT_TwoWire |
( |
| ) |
|
The documentation for this class was generated from the following files: