Definition at line 61 of file LT_SMBusPec.h.
|
| | LT_SMBusPec () |
| |
| | LT_SMBusPec (uint32_t speed) |
| |
| virtual | ~LT_SMBusPec () |
| |
| LT_I2CBus * | i2cbus (void) |
| |
| void | i2cbus (LT_I2CBus *i2cbus) |
| |
| void | writeByte (uint8_t address, uint8_t command, uint8_t data) |
| | SMBus write byte command. More...
|
| |
| void | writeBytes (uint8_t *addresses, uint8_t *commands, uint8_t *data, uint8_t no_addresses) |
| | SMBus write byte command for a list of addresses. More...
|
| |
| uint8_t | readByte (uint8_t address, uint8_t command) |
| | SMBus read byte command. More...
|
| |
| void | writeWord (uint8_t address, uint8_t command, uint16_t data) |
| | SMBus write word command. More...
|
| |
| uint16_t | readWord (uint8_t address, uint8_t command) |
| | SMBus read word command. More...
|
| |
| void | writeBlock (uint8_t address, uint8_t command, uint8_t *block, uint16_t block_size) |
| | SMBus write block command. More...
|
| |
| uint8_t | writeReadBlock (uint8_t address, uint8_t command, uint8_t *block_out, uint16_t block_out_size, uint8_t *block_in, uint16_t block_in_size) |
| | SMBus write then read block command. More...
|
| |
| uint8_t | readBlock (uint8_t address, uint8_t command, uint8_t *block, uint16_t block_size) |
| | SMBus read block command. More...
|
| |
| void | sendByte (uint8_t address, uint8_t command) |
| | SMBus send byte command. More...
|
| |
| uint8_t | readAlert (void) |
| | Perform ARA. More...
|
| |
| uint8_t | waitForAck (uint8_t address, uint8_t command) |
| | Read with the address and command in loop until ack, then issue stop. More...
|
| |
| uint8_t * | probe (uint8_t command) |
| | SMBus bus probe. More...
|
| |
| uint8_t * | probeUnique (uint8_t command) |
| | SMBus bus probe. More...
|
| |
| virtual | ~LT_SMBus () |
| |
| bool | pecEnabled (void) |
| | Check if PEC is enabled. More...
|
| |
| void | pecClear (void) |
| | Clear the pec value so it can start a new calculation. More...
|
| |
| void | pecAdd (uint8_t byte_value) |
| | Add a byte to the pec calculation. More...
|
| |
| uint8_t | pecGet (void) |
| | Get the current pec result. More...
|
| |
| bool | checkCRC (uint8_t *data) |
| | Check CRC of block data organized as 31 data bytes plus CRC. More...
|
| |
| uint8_t | getCRC (uint8_t *data) |
| | Get CRC of block data organized as 31 bytes pluse CRC. More...
|
| |
| uint8_t | calculate (uint8_t *data, uint8_t begining_value, uint8_t start_index, uint8_t length) |
| | Helper function for pec. More...
|
| |