![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
PMBusRail communication. For Multiphase Rails. More...
PMBusRail communication. For Multiphase Rails.
Definition at line 72 of file LT_PMBusRail.h.
Public Member Functions | |
| LT_PMBusRail (LT_PMBus *pmbus, uint8_t railAddress, tRailDef **railDef) | |
| Construct a LT_PMBus. More... | |
| ~LT_PMBusRail () | |
| void | changePMBus (LT_PMBus *pmbus) |
| Change the pmbus. More... | |
| uint8_t | getAddress () |
| Get ther rail address. More... | |
| bool | isController () |
| Ask if devices is a PSM controller. More... | |
| uint8_t | getNoPages () |
| Get the number of pages in the rail. More... | |
| bool | isMultiphase () |
| Ask if the rail is multiphase. More... | |
| uint32_t | getCapabilities () |
| Get a list of capabilities. More... | |
| uint32_t | hasCapability (uint32_t capability) |
| Ask if the rail has the given capability. More... | |
| void | merge (LT_PMBusRail *rail) |
| Merge a rail into this one. No delete of incomming rail. More... | |
| void | setVout (float voltage) |
| Set the output voltage of a polyphase rail. More... | |
| float | readVin (bool polling) |
| Read the input voltage of a polyphase rail. More... | |
| float | readVout (bool polling) |
| Read the output voltage of a polyphase rail. More... | |
| float | readIin (bool polling) |
| Read the input current of a polyphase rail. More... | |
| float | readIout (bool polling) |
| Read the output current of a polyphase rail. More... | |
| float | readPin (bool polling) |
| Read the input power of a polyphase rail. More... | |
| float | readPout (bool polling) |
| Read the output power of a polyphase rail. More... | |
| float | readExternalTemperature (bool polling) |
| Read the external temperature of a polyphase rail. More... | |
| float | readInternalTemperature (bool polling) |
| Read the internal temperature of a polyphase rail. More... | |
| float | readEfficiency (bool polling) |
| Read the efficiency (calculated) More... | |
| float | readDutyCycle (bool polling) |
| Read the average duty cycle. More... | |
| float | readPhaseBalance (bool polling) |
| Read the phase balance (calculated) More... | |
| float | readTransient (bool polling) |
| Read the transient. More... | |
| uint16_t | readStatusWord () |
| Read the status word of a polyphase rail. More... | |
| uint16_t | readMfrSpecialId () |
| Read the special of a polyphase rail. More... | |
| void | clearFaults () |
| Clear faults of polyphase rail. More... | |
| void | sequenceOn () |
| Sequence on a polyphase rail. More... | |
| void | immediateOff () |
| Turn off a polyphase rail. More... | |
| void | sequenceOff () |
| Sequence off a polyphase rail. More... | |
| void | marginHigh () |
| Margin high polyphase rail. More... | |
| void | marginLow () |
| Margin low polyphase rail. More... | |
| void | marginOff () |
| Margin off polyphase rail. More... | |
Protected Attributes | |
| tRailDef ** | railDef_ |
| void LT_PMBusRail::changePMBus | ( | LT_PMBus * | pmbus | ) |
Change the pmbus.
Definition at line 93 of file LT_PMBusRail.cpp.
| void LT_PMBusRail::clearFaults | ( | ) |
| uint8_t LT_PMBusRail::getAddress | ( | ) |
Get ther rail address.
Definition at line 98 of file LT_PMBusRail.cpp.
| uint32_t LT_PMBusRail::getCapabilities | ( | ) |
Get a list of capabilities.
Definition at line 127 of file LT_PMBusRail.cpp.
| uint8_t LT_PMBusRail::getNoPages | ( | ) |
Get the number of pages in the rail.
Definition at line 109 of file LT_PMBusRail.cpp.
| uint32_t LT_PMBusRail::hasCapability | ( | uint32_t | capability | ) |
Ask if the rail has the given capability.
Definition at line 132 of file LT_PMBusRail.cpp.
| void LT_PMBusRail::immediateOff | ( | ) |
| bool LT_PMBusRail::isController | ( | ) |
Ask if devices is a PSM controller.
Definition at line 103 of file LT_PMBusRail.cpp.
| bool LT_PMBusRail::isMultiphase | ( | ) |
Ask if the rail is multiphase.
Definition at line 122 of file LT_PMBusRail.cpp.
| void LT_PMBusRail::marginHigh | ( | ) |
| void LT_PMBusRail::marginLow | ( | ) |
| void LT_PMBusRail::marginOff | ( | ) |
| void LT_PMBusRail::merge | ( | LT_PMBusRail * | rail | ) |
Merge a rail into this one. No delete of incomming rail.
| rail | Rail to merge |
Definition at line 71 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readDutyCycle | ( | bool | polling | ) |
Read the average duty cycle.
| polling | true for polling |
Definition at line 385 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readEfficiency | ( | bool | polling | ) |
Read the efficiency (calculated)
| polling | true for polling |
Definition at line 338 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readExternalTemperature | ( | bool | polling | ) |
Read the external temperature of a polyphase rail.
| polling | true for polling |
Definition at line 279 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readIin | ( | bool | polling | ) |
Read the input current of a polyphase rail.
| polling | true for polling |
Definition at line 181 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readInternalTemperature | ( | bool | polling | ) |
Read the internal temperature of a polyphase rail.
| polling | true for polling |
Definition at line 306 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readIout | ( | bool | polling | ) |
Read the output current of a polyphase rail.
| polling | true for polling |
Definition at line 207 of file LT_PMBusRail.cpp.
| uint16_t LT_PMBusRail::readMfrSpecialId | ( | ) |
| float LT_PMBusRail::readPhaseBalance | ( | bool | polling | ) |
Read the phase balance (calculated)
| polling | true for polling |
Definition at line 410 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readPin | ( | bool | polling | ) |
Read the input power of a polyphase rail.
| polling | true for polling |
Definition at line 232 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readPout | ( | bool | polling | ) |
Read the output power of a polyphase rail.
| polling | true for polling |
Definition at line 254 of file LT_PMBusRail.cpp.
| uint16_t LT_PMBusRail::readStatusWord | ( | ) |
Read the status word of a polyphase rail.
Definition at line 550 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readTransient | ( | bool | polling | ) |
Read the transient.
| polling | true for polling |
Definition at line 440 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readVin | ( | bool | polling | ) |
Read the input voltage of a polyphase rail.
| polling | true for polling |
Definition at line 154 of file LT_PMBusRail.cpp.
| float LT_PMBusRail::readVout | ( | bool | polling | ) |
Read the output voltage of a polyphase rail.
| polling | true for polling |
Definition at line 167 of file LT_PMBusRail.cpp.
| void LT_PMBusRail::sequenceOff | ( | ) |
| void LT_PMBusRail::sequenceOn | ( | ) |
| void LT_PMBusRail::setVout | ( | float | voltage | ) |
Set the output voltage of a polyphase rail.
| voltage | Rail voltage |
Definition at line 142 of file LT_PMBusRail.cpp.
Construct a LT_PMBus.
A list of addresses with pages that make up the rail. NULL terminated.
| pmbus | SMBus for communication. Use the PEC or non-PEC version. |
| railAddress | The rail address. |
Definition at line 64 of file LT_PMBusRail.cpp.
| LT_PMBusRail::~LT_PMBusRail | ( | ) |
Definition at line 81 of file LT_PMBusRail.cpp.
|
protected |
Definition at line 81 of file LT_PMBusRail.h.