![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Definition at line 56 of file LT_EEDataFaultLog.h.
Public Member Functions | |
| LT_EEDataFaultLog (LT_PMBus *pmbus) | |
| void | getNvmBlock (uint8_t address, uint16_t offset, uint16_t numWords, uint8_t command, uint8_t *data) |
Public Member Functions inherited from LT_FaultLog | |
| LT_FaultLog (LT_PMBus *pmbus) | |
| virtual | ~LT_FaultLog () |
| bool | hasFaultLog (uint8_t address) |
| void | enableFaultLog (uint8_t address) |
| void | disableFaultLog (uint8_t address) |
| void | clearFaultLog (uint8_t address) |
| virtual void | read (uint8_t address)=0 |
| virtual void | print (Print *printer)=0 |
| virtual uint8_t * | getBinary ()=0 |
| virtual uint16_t | getBinarySize ()=0 |
| virtual void | dumpBinary (Print *printer=0)=0 |
| virtual void | release ()=0 |
| void | dumpBin (Print *printer, uint8_t *log, uint8_t size) |
| uint64_t | getSharedTime200us (FaultLogTimeStamp time_stamp) |
| float | getTimeInMs (FaultLogTimeStamp time_stamp) |
| uint8_t | getRawByteVal (RawByte value) |
| uint16_t | getRawWordVal (RawWord value) |
| uint16_t | getRawWordReverseVal (RawWordReverse value) |
| uint16_t | getLin5_11WordVal (Lin5_11Word value) |
| uint16_t | getLin5_11WordReverseVal (Lin5_11WordReverse value) |
| uint16_t | getLin16WordVal (Lin16Word value) |
| uint16_t | getLin16WordReverseVal (Lin16WordReverse value) |
Additional Inherited Members | |
Protected Member Functions inherited from LT_FaultLog | |
| uint8_t | readMfrStatusByte (uint8_t address) |
| uint8_t | readMfrFaultLogStatusByte (uint8_t address) |
Protected Attributes inherited from LT_FaultLog | |
| LT_PMBus * | pmbus_ |
|
virtual |
Implements LT_FaultLog.
Definition at line 65 of file LT_EEDataFaultLog.h.
| LT_EEDataFaultLog::LT_EEDataFaultLog | ( | LT_PMBus * | pmbus | ) |
Definition at line 60 of file LT_EEDataFaultLog.h.