![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
class that handles LTC3887 fault logs. More...
class that handles LTC3887 fault logs.
contains structs for interpreting the data read from the part.
Definition at line 61 of file LT_3887FaultLog.h.
Data Structures | |
| struct | FaultLogLtc3887 |
| struct | FaultLogPreambleLtc3887 |
| struct | FaultLogReadLoopLtc3887 |
| struct | FaultLogTelemetrySummaryLtc3887 |
Public Member Functions | |
| LT_3887FaultLog (LT_PMBus *pmbus) | |
| Constructor. More... | |
| void | print (Print *printer=0) |
| Pretty prints this part's fault log to a Print inheriting object, or Serial if none specified. More... | |
| uint8_t * | getBinary () |
| Get binary of the fault log or NULL if no log. More... | |
| uint16_t | getBinarySize () |
| Get size of binary data. More... | |
| void | dumpBinary (Print *printer=0) |
| Dumps binary of the fault log to a Print inheriting object, or Serial if none specified. More... | |
| void | read (uint8_t address) |
| Reads the fault log from the specified address, reserves memory to hold the data. More... | |
| struct FaultLogLtc3887 * | get () |
| void | release () |
| Frees the memory reserved for the fault log. More... | |
Public Member Functions inherited from LT_EEDataFaultLog | |
| LT_EEDataFaultLog (LT_PMBus *pmbus) | |
| void | getNvmBlock (uint8_t address, uint16_t offset, uint16_t numWords, uint8_t command, uint8_t *data) |
Public Member Functions inherited from LT_FaultLog | |
| LT_FaultLog (LT_PMBus *pmbus) | |
| virtual | ~LT_FaultLog () |
| bool | hasFaultLog (uint8_t address) |
| void | enableFaultLog (uint8_t address) |
| void | disableFaultLog (uint8_t address) |
| void | clearFaultLog (uint8_t address) |
| void | dumpBin (Print *printer, uint8_t *log, uint8_t size) |
| uint64_t | getSharedTime200us (FaultLogTimeStamp time_stamp) |
| float | getTimeInMs (FaultLogTimeStamp time_stamp) |
| uint8_t | getRawByteVal (RawByte value) |
| uint16_t | getRawWordVal (RawWord value) |
| uint16_t | getRawWordReverseVal (RawWordReverse value) |
| uint16_t | getLin5_11WordVal (Lin5_11Word value) |
| uint16_t | getLin5_11WordReverseVal (Lin5_11WordReverse value) |
| uint16_t | getLin16WordVal (Lin16Word value) |
| uint16_t | getLin16WordReverseVal (Lin16WordReverse value) |
Protected Attributes | |
| FaultLogLtc3887 * | faultLog3887 |
Protected Attributes inherited from LT_FaultLog | |
| LT_PMBus * | pmbus_ |
Additional Inherited Members | |
Protected Member Functions inherited from LT_FaultLog | |
| uint8_t | readMfrStatusByte (uint8_t address) |
| uint8_t | readMfrFaultLogStatusByte (uint8_t address) |
|
virtual |
Dumps binary of the fault log to a Print inheriting object, or Serial if none specified.
| printer | Print inheriting object to print the binary to. |
Implements LT_FaultLog.
Definition at line 108 of file LT_3887FaultLog.cpp.
| struct FaultLogLtc3887* LT_3887FaultLog::get | ( | ) |
Definition at line 156 of file LT_3887FaultLog.h.
|
virtual |
Get binary of the fault log or NULL if no log.
Implements LT_FaultLog.
Definition at line 98 of file LT_3887FaultLog.cpp.
|
virtual |
Get size of binary data.
Implements LT_FaultLog.
Definition at line 103 of file LT_3887FaultLog.cpp.
|
virtual |
Pretty prints this part's fault log to a Print inheriting object, or Serial if none specified.
| printer | Print inheriting object to print the fault log to. |
Implements LT_FaultLog.
Definition at line 113 of file LT_3887FaultLog.cpp.
|
virtual |
Reads the fault log from the specified address, reserves memory to hold the data.
| address | the address to read the fault log from. |
Implements LT_FaultLog.
Definition at line 75 of file LT_3887FaultLog.cpp.
|
virtual |
Frees the memory reserved for the fault log.
Implements LT_FaultLog.
Definition at line 92 of file LT_3887FaultLog.cpp.
| LT_3887FaultLog::LT_3887FaultLog | ( | LT_PMBus * | pmbus | ) |
Constructor.
| pmbus | pmbus object reference for this fault log handler to use. |
Definition at line 61 of file LT_3887FaultLog.cpp.
|
protected |
Definition at line 129 of file LT_3887FaultLog.h.