![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
The EasySMU_IOpanel class provides an interface between the EasySMU and a touchscreen. More...
The EasySMU_IOpanel class provides an interface between the EasySMU and a touchscreen.
User Guide
Schematic
Top-Level Linduino Firmware for EasySMU
EasySMU Class Reference
EasySMU_IOpanel Class Reference
EasySMU Webpage
Definition at line 221 of file EasySMU_IOpanel.h.
Public Member Functions | |
| void | Init () |
| Initialize the IO panel, including drawing buttons, etc. More... | |
| int | CheckButton () |
| check if a button is pressed More... | |
| void | DisplaySMULabel () |
| Draw the SMU labels. The selected channel will be green. More... | |
| void | DisplayVoltageSourceSetting (int16_t channel, float flt_old, float flt_new) |
| Draw the voltage source setting for a single channel. More... | |
| void | DisplayMeasuredVoltage (int16_t channel, float flt_old, float flt_new) |
| Draw the measured voltage for a single channel. More... | |
| void | DisplayCurrentSourceSetting (int16_t channel, float flt_old, float flt_new, int8_t source_both_sink) |
| Draw the current source setting for a single channel. More... | |
| void | DisplayMeasuredCurrent (int16_t channel, float flt_old, float flt_new) |
| Draw the measured current for a single channel. More... | |
| void | DisplayTemperatureOfIadc (int16_t channel, float flt_old, float flt_new) |
| Draw the measured temperature from the current ADC. Presently, not used as it clutters up the screen. More... | |
| void | DisplayTemperatureOfVadc (int16_t channel, float flt_old, float flt_new) |
| Draw the measured temperature from the voltage ADC. Presently, not used as it clutters up the screen. More... | |
Data Fields | |
| Adafruit_ILI9341 | lcd = Adafruit_ILI9341(TFT_CS, TFT_DC) |
| Adafruit_FT6206 | touchp = Adafruit_FT6206() |
| uint32_t | start_button_pressed_ |
| keep track of when the button was pressed to later calculate the duration it has been held More... | |
| uint32_t | duration_button_pressed_ |
| stores a value corresponding to how long the button has been pressed More... | |
| int | button_pressed_ |
| stores the value of the button pressed (from enum) More... | |
| int | SMUselected_ |
| stores which SMU channel is selected on the TFT display More... | |
| uint8_t | enabled_ |
| indicates if the TFT is enabled. More... | |
| int16_t EasySMU_IOpanel::CheckButton | ( | ) |
check if a button is pressed
Definition at line 177 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::DisplayCurrentSourceSetting | ( | int16_t | channel, |
| float | flt_old, | ||
| float | flt_new, | ||
| int8_t | source_both_sink | ||
| ) |
Draw the current source setting for a single channel.
| flt_old | the old value to be overwitten in the background color |
| flt_new | the new value to be drawn in the foreground color |
| source_both_sink | If source only mode is set, a '+' will be drawn in front. If sink only mode is set, a '-' will be drawn in front. |
Definition at line 440 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::DisplayMeasuredCurrent | ( | int16_t | channel, |
| float | flt_old, | ||
| float | flt_new | ||
| ) |
Draw the measured current for a single channel.
| flt_old | the old value to be overwitten in the background color |
| flt_new | the new value to be drawn in the foreground color |
Definition at line 475 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::DisplayMeasuredVoltage | ( | int16_t | channel, |
| float | flt_old, | ||
| float | flt_new | ||
| ) |
Draw the measured voltage for a single channel.
| flt_old | the old value to be overwitten in the background color |
| flt_new | the new value to be drawn in the foreground color |
Definition at line 348 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::DisplaySMULabel | ( | ) |
Draw the SMU labels. The selected channel will be green.
Definition at line 280 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::DisplayTemperatureOfIadc | ( | int16_t | channel, |
| float | flt_old, | ||
| float | flt_new | ||
| ) |
Draw the measured temperature from the current ADC. Presently, not used as it clutters up the screen.
| flt_old | the old value to be overwitten in the background color |
| flt_new | the new value to be drawn in the foreground color |
Definition at line 376 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::DisplayTemperatureOfVadc | ( | int16_t | channel, |
| float | flt_old, | ||
| float | flt_new | ||
| ) |
Draw the measured temperature from the voltage ADC. Presently, not used as it clutters up the screen.
| flt_old | the old value to be overwitten in the background color |
| flt_new | the new value to be drawn in the foreground color |
Definition at line 403 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::DisplayVoltageSourceSetting | ( | int16_t | channel, |
| float | flt_old, | ||
| float | flt_new | ||
| ) |
Draw the voltage source setting for a single channel.
| channel | channel to draw |
| flt_old | the old value to be overwitten in the background color |
| flt_new | the new value to be drawn in the foreground color |
Definition at line 318 of file EasySMU_IOpanel.cpp.
| void EasySMU_IOpanel::Init | ( | ) |
Initialize the IO panel, including drawing buttons, etc.
Definition at line 106 of file EasySMU_IOpanel.cpp.
| int EasySMU_IOpanel::button_pressed_ |
stores the value of the button pressed (from enum)
Definition at line 265 of file EasySMU_IOpanel.h.
| uint32_t EasySMU_IOpanel::duration_button_pressed_ |
stores a value corresponding to how long the button has been pressed
Definition at line 261 of file EasySMU_IOpanel.h.
| uint8_t EasySMU_IOpanel::enabled_ |
indicates if the TFT is enabled.
1=enabled, 0=disabled. (TFT may be disabled to reduce noise in the SMU output caused by SPI communication.)
Definition at line 267 of file EasySMU_IOpanel.h.
| Adafruit_ILI9341 EasySMU_IOpanel::lcd = Adafruit_ILI9341(TFT_CS, TFT_DC) |
Definition at line 247 of file EasySMU_IOpanel.h.
| int EasySMU_IOpanel::SMUselected_ |
stores which SMU channel is selected on the TFT display
Definition at line 266 of file EasySMU_IOpanel.h.
| uint32_t EasySMU_IOpanel::start_button_pressed_ |
keep track of when the button was pressed to later calculate the duration it has been held
Definition at line 260 of file EasySMU_IOpanel.h.
| Adafruit_FT6206 EasySMU_IOpanel::touchp = Adafruit_FT6206() |
Definition at line 250 of file EasySMU_IOpanel.h.