![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Definition at line 118 of file Adafruit_ILI9341.h.
Public Member Functions | |
| Adafruit_ILI9341 (int8_t _CS, int8_t _DC, int8_t _MOSI, int8_t _SCLK, int8_t _RST, int8_t _MISO) | |
| Adafruit_ILI9341 (int8_t _CS, int8_t _DC, int8_t _RST=-1) | |
| void | begin (void) |
| void | setAddrWindow (uint16_t x0, uint16_t y0, uint16_t x1, uint16_t y1) |
| void | pushColor (uint16_t color) |
| void | fillScreen (uint16_t color) |
| void | drawPixel (int16_t x, int16_t y, uint16_t color) |
| void | drawFastVLine (int16_t x, int16_t y, int16_t h, uint16_t color) |
| void | drawFastHLine (int16_t x, int16_t y, int16_t w, uint16_t color) |
| void | fillRect (int16_t x, int16_t y, int16_t w, int16_t h, uint16_t color) |
| void | setRotation (uint8_t r) |
| void | invertDisplay (boolean i) |
| uint16_t | color565 (uint8_t r, uint8_t g, uint8_t b) |
| uint8_t | readdata (void) |
| uint8_t | readcommand8 (uint8_t reg, uint8_t index=0) |
| void | spiwrite (uint8_t) |
| void | writecommand (uint8_t c) |
| void | writedata (uint8_t d) |
| void | commandList (uint8_t *addr) |
| uint8_t | spiread (void) |
Public Member Functions inherited from Adafruit_GFX | |
| Adafruit_GFX (int16_t w, int16_t h) | |
| virtual void | drawLine (int16_t x0, int16_t y0, int16_t x1, int16_t y1, uint16_t color) |
| virtual void | drawFastVLine (int16_t x, int16_t y, int16_t h, uint16_t color) |
| virtual void | drawFastHLine (int16_t x, int16_t y, int16_t w, uint16_t color) |
| virtual void | drawRect (int16_t x, int16_t y, int16_t w, int16_t h, uint16_t color) |
| virtual void | fillRect (int16_t x, int16_t y, int16_t w, int16_t h, uint16_t color) |
| virtual void | fillScreen (uint16_t color) |
| virtual void | invertDisplay (boolean i) |
| void | drawCircle (int16_t x0, int16_t y0, int16_t r, uint16_t color) |
| void | drawCircleHelper (int16_t x0, int16_t y0, int16_t r, uint8_t cornername, uint16_t color) |
| void | fillCircle (int16_t x0, int16_t y0, int16_t r, uint16_t color) |
| void | fillCircleHelper (int16_t x0, int16_t y0, int16_t r, uint8_t cornername, int16_t delta, uint16_t color) |
| void | drawTriangle (int16_t x0, int16_t y0, int16_t x1, int16_t y1, int16_t x2, int16_t y2, uint16_t color) |
| void | fillTriangle (int16_t x0, int16_t y0, int16_t x1, int16_t y1, int16_t x2, int16_t y2, uint16_t color) |
| void | drawRoundRect (int16_t x0, int16_t y0, int16_t w, int16_t h, int16_t radius, uint16_t color) |
| void | fillRoundRect (int16_t x0, int16_t y0, int16_t w, int16_t h, int16_t radius, uint16_t color) |
| void | drawBitmap (int16_t x, int16_t y, const uint8_t *bitmap, int16_t w, int16_t h, uint16_t color) |
| void | drawBitmap (int16_t x, int16_t y, const uint8_t *bitmap, int16_t w, int16_t h, uint16_t color, uint16_t bg) |
| void | drawBitmap (int16_t x, int16_t y, uint8_t *bitmap, int16_t w, int16_t h, uint16_t color) |
| void | drawBitmap (int16_t x, int16_t y, uint8_t *bitmap, int16_t w, int16_t h, uint16_t color, uint16_t bg) |
| void | drawXBitmap (int16_t x, int16_t y, const uint8_t *bitmap, int16_t w, int16_t h, uint16_t color) |
| void | drawChar (int16_t x, int16_t y, unsigned char c, uint16_t color, uint16_t bg, uint8_t size) |
| void | setCursor (int16_t x, int16_t y) |
| void | setTextColor (uint16_t c) |
| void | setTextColor (uint16_t c, uint16_t bg) |
| void | setTextSize (uint8_t s) |
| void | setTextWrap (boolean w) |
| void | setRotation (uint8_t r) |
| void | cp437 (boolean x=true) |
| void | setFont (const GFXfont *f=NULL) |
| void | getTextBounds (char *string, int16_t x, int16_t y, int16_t *x1, int16_t *y1, uint16_t *w, uint16_t *h) |
| void | getTextBounds (const __FlashStringHelper *s, int16_t x, int16_t y, int16_t *x1, int16_t *y1, uint16_t *w, uint16_t *h) |
| virtual void | write (uint8_t) |
| int16_t | height (void) const |
| int16_t | width (void) const |
| uint8_t | getRotation (void) const |
| int16_t | getCursorX (void) const |
| int16_t | getCursorY (void) const |
Additional Inherited Members | |
Protected Attributes inherited from Adafruit_GFX | |
| const int16_t | WIDTH |
| const int16_t | HEIGHT |
| int16_t | _width |
| int16_t | _height |
| int16_t | cursor_x |
| int16_t | cursor_y |
| uint16_t | textcolor |
| uint16_t | textbgcolor |
| uint8_t | textsize |
| uint8_t | rotation |
| boolean | wrap |
| boolean | _cp437 |
| GFXfont * | gfxFont |
| void Adafruit_ILI9341::begin | ( | void | ) |
Definition at line 219 of file Adafruit_ILI9341.cpp.
| uint16_t Adafruit_ILI9341::color565 | ( | uint8_t | r, |
| uint8_t | g, | ||
| uint8_t | b | ||
| ) |
Definition at line 599 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::commandList | ( | uint8_t * | addr | ) |
Definition at line 191 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::drawFastHLine | ( | int16_t | x, |
| int16_t | y, | ||
| int16_t | w, | ||
| uint16_t | color | ||
| ) |
Definition at line 521 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::drawFastVLine | ( | int16_t | x, |
| int16_t | y, | ||
| int16_t | h, | ||
| uint16_t | color | ||
| ) |
Definition at line 482 of file Adafruit_ILI9341.cpp.
|
virtual |
Implements Adafruit_GFX.
Definition at line 453 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::fillRect | ( | int16_t | x, |
| int16_t | y, | ||
| int16_t | w, | ||
| int16_t | h, | ||
| uint16_t | color | ||
| ) |
Definition at line 558 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::fillScreen | ( | uint16_t | color | ) |
Definition at line 552 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::invertDisplay | ( | boolean | i | ) |
Definition at line 646 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::pushColor | ( | uint16_t | color | ) |
Definition at line 429 of file Adafruit_ILI9341.cpp.
| uint8_t Adafruit_ILI9341::readcommand8 | ( | uint8_t | reg, |
| uint8_t | index = 0 |
||
| ) |
Definition at line 708 of file Adafruit_ILI9341.cpp.
| uint8_t Adafruit_ILI9341::readdata | ( | void | ) |
Definition at line 697 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::setAddrWindow | ( | uint16_t | x0, |
| uint16_t | y0, | ||
| uint16_t | x1, | ||
| uint16_t | y1 | ||
| ) |
Definition at line 409 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::setRotation | ( | uint8_t | r | ) |
Definition at line 613 of file Adafruit_ILI9341.cpp.
| uint8_t Adafruit_ILI9341::spiread | ( | void | ) |
Definition at line 657 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::spiwrite | ( | uint8_t | c | ) |
Definition at line 79 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::writecommand | ( | uint8_t | c | ) |
Definition at line 140 of file Adafruit_ILI9341.cpp.
| void Adafruit_ILI9341::writedata | ( | uint8_t | d | ) |
Definition at line 161 of file Adafruit_ILI9341.cpp.
| Adafruit_ILI9341::Adafruit_ILI9341 | ( | int8_t | _CS, |
| int8_t | _DC, | ||
| int8_t | _MOSI, | ||
| int8_t | _SCLK, | ||
| int8_t | _RST, | ||
| int8_t | _MISO | ||
| ) |
Definition at line 55 of file Adafruit_ILI9341.cpp.
| Adafruit_ILI9341::Adafruit_ILI9341 | ( | int8_t | _CS, |
| int8_t | _DC, | ||
| int8_t | _RST = -1 |
||
| ) |
Definition at line 70 of file Adafruit_ILI9341.cpp.