![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Definition at line 108 of file Adafruit_GFX.h.
Public Member Functions | |
| Adafruit_GFX_Button (void) | |
| void | initButton (Adafruit_GFX *gfx, int16_t x, int16_t y, uint8_t w, uint8_t h, uint16_t outline, uint16_t fill, uint16_t textcolor, char *label, uint8_t textsize) |
| void | drawButton (boolean inverted=false) |
| boolean | contains (int16_t x, int16_t y) |
| void | press (boolean p) |
| boolean | isPressed () |
| boolean | justPressed () |
| boolean | justReleased () |
| boolean Adafruit_GFX_Button::contains | ( | int16_t | x, |
| int16_t | y | ||
| ) |
Definition at line 1087 of file Adafruit_GFX.cpp.
| void Adafruit_GFX_Button::drawButton | ( | boolean | inverted = false | ) |
Definition at line 1061 of file Adafruit_GFX.cpp.
| void Adafruit_GFX_Button::initButton | ( | Adafruit_GFX * | gfx, |
| int16_t | x, | ||
| int16_t | y, | ||
| uint8_t | w, | ||
| uint8_t | h, | ||
| uint16_t | outline, | ||
| uint16_t | fill, | ||
| uint16_t | textcolor, | ||
| char * | label, | ||
| uint8_t | textsize | ||
| ) |
Definition at line 1043 of file Adafruit_GFX.cpp.
| boolean Adafruit_GFX_Button::isPressed | ( | ) |
Definition at line 1100 of file Adafruit_GFX.cpp.
| boolean Adafruit_GFX_Button::justPressed | ( | ) |
Definition at line 1104 of file Adafruit_GFX.cpp.
| boolean Adafruit_GFX_Button::justReleased | ( | ) |
Definition at line 1108 of file Adafruit_GFX.cpp.
| void Adafruit_GFX_Button::press | ( | boolean | p | ) |
Definition at line 1094 of file Adafruit_GFX.cpp.
| Adafruit_GFX_Button::Adafruit_GFX_Button | ( | void | ) |
Definition at line 1038 of file Adafruit_GFX.cpp.