![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Definition at line 61 of file Adafruit_FT6206.h.
Public Member Functions | |
| Adafruit_FT6206 (void) | |
| Instantiates a new FT6206 class. More... | |
| boolean | begin (uint8_t thresh=FT6206_DEFAULT_THRESSHOLD) |
| Setups the HW. More... | |
| void | writeRegister8 (uint8_t reg, uint8_t val) |
| uint8_t | readRegister8 (uint8_t reg) |
| void | readData (uint16_t *x, uint16_t *y) |
| void | autoCalibrate (void) |
| boolean | touched (void) |
| TS_Point | getPoint (void) |
| void Adafruit_FT6206::autoCalibrate | ( | void | ) |
Definition at line 74 of file Adafruit_FT6206.cpp.
| boolean Adafruit_FT6206::begin | ( | uint8_t | thresh = FT6206_DEFAULT_THRESSHOLD | ) |
Setups the HW.
Definition at line 48 of file Adafruit_FT6206.cpp.
| TS_Point Adafruit_FT6206::getPoint | ( | void | ) |
Definition at line 184 of file Adafruit_FT6206.cpp.
| void Adafruit_FT6206::readData | ( | uint16_t * | x, |
| uint16_t * | y | ||
| ) |
Definition at line 112 of file Adafruit_FT6206.cpp.
| uint8_t Adafruit_FT6206::readRegister8 | ( | uint8_t | reg | ) |
Definition at line 193 of file Adafruit_FT6206.cpp.
| boolean Adafruit_FT6206::touched | ( | void | ) |
Definition at line 102 of file Adafruit_FT6206.cpp.
| void Adafruit_FT6206::writeRegister8 | ( | uint8_t | reg, |
| uint8_t | val | ||
| ) |
Definition at line 211 of file Adafruit_FT6206.cpp.
| Adafruit_FT6206::Adafruit_FT6206 | ( | void | ) |
Instantiates a new FT6206 class.
Definition at line 38 of file Adafruit_FT6206.cpp.