![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Functions | |
| static void | print_title () |
| static void | print_prompt () |
| static void | setup () |
| static void | loop () |
Macros | |
| #define | EEPROM_PAGE_SIZE 16 |
| #define | EEPROM_DATA_SIZE 256 |
Variables | |
| static uint8_t | i2c_address = 0xA0 |
| unsigned char | id_string_size = 50 |
| static uint16_t | eeprom_address = 0x00 |
| byte | terminator = 0x0a |
| byte | read_count = id_string_size |
| static int | int_data |
| long | long_data |
| static float | float_data |
| unsigned char | user_command |
|
static |
Definition at line 145 of file Serial_EEPROM_Test.ino.
|
static |
Definition at line 97 of file Serial_EEPROM_Test.ino.
|
static |
Definition at line 77 of file Serial_EEPROM_Test.ino.
|
static |
Definition at line 136 of file Serial_EEPROM_Test.ino.
| #define EEPROM_DATA_SIZE 256 |
Definition at line 55 of file Serial_EEPROM_Test.ino.
| #define EEPROM_PAGE_SIZE 16 |
Definition at line 54 of file Serial_EEPROM_Test.ino.
|
static |
Definition at line 67 of file Serial_EEPROM_Test.ino.
|
static |
Definition at line 72 of file Serial_EEPROM_Test.ino.
|
static |
Definition at line 65 of file Serial_EEPROM_Test.ino.
| unsigned char id_string_size = 50 |
Definition at line 66 of file Serial_EEPROM_Test.ino.
|
static |
Definition at line 70 of file Serial_EEPROM_Test.ino.
| long long_data |
Definition at line 71 of file Serial_EEPROM_Test.ino.
| byte read_count = id_string_size |
Definition at line 69 of file Serial_EEPROM_Test.ino.
| byte terminator = 0x0a |
Definition at line 68 of file Serial_EEPROM_Test.ino.
| unsigned char user_command |
Definition at line 75 of file Serial_EEPROM_Test.ino.