![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Code for datasheet application - Margining a power supply with the LTC2645 Quad 12-/10-/8-Bit PWM to VOUT DACs with 10ppm/C Reference. More...
Code for datasheet application - Margining a power supply with the LTC2645 Quad 12-/10-/8-Bit PWM to VOUT DACs with 10ppm/C Reference.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a precision voltage source (null box) and a precision voltmeter (to monitor voltage source). No external power supply is required. Ensure JP1 is installed in the default position from the factory. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2645
http://www.linear.com/product/LTC2645
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file Margining.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| 16-bit PWM Pin More... | |
| static void | print_prompt () |
| static void | init_16_bit_PWM () |
| Initializes Pin 9 and 10 for 16-bit PWM. More... | |
| static void | pwm_16_bit (uint8_t pin, uint16_t duty) |
| Sets duty cycle for 16-bit PWM. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static void | print_prompt (int16_t selected_dac) |
| Prints main menu. More... | |
Variables | |
| const uint8_t | DAC_A = 9 |
| const uint8_t | DAC_B = 10 |
| 16-bit PWM Pin More... | |
|
static |
Initializes Pin 9 and 10 for 16-bit PWM.
Definition at line 173 of file Margining.ino.
|
static |
Repeats Linduino loop.
Definition at line 96 of file Margining.ino.
|
static |
|
static |
Prints main menu.
Definition at line 157 of file Margining.ino.
|
static |
16-bit PWM Pin
Prints the title block when program first starts.
Definition at line 141 of file Margining.ino.
|
static |
Sets duty cycle for 16-bit PWM.
Definition at line 205 of file Margining.ino.
|
static |
Initialize Linduino.
Definition at line 82 of file Margining.ino.
| const uint8_t DAC_A = 9 |
Definition at line 72 of file Margining.ino.
| const uint8_t DAC_B = 10 |
16-bit PWM Pin
Definition at line 73 of file Margining.ino.