![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LT_SPI: Routines to communicate with ATmega328P's hardware SPI port. More...
LT_SPI: Routines to communicate with ATmega328P's hardware SPI port.
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Library Header File for LT_SPI: Routines to communicate with ATmega328P's hardware SPI port.
Definition in file LT_SPI.h.
Go to the source code of this file.
Functions | |
| void | spi_transfer_byte (uint8_t cs_pin, uint8_t tx, uint8_t *rx) |
| Reads and sends a byte. More... | |
| void | spi_transfer_word (uint8_t cs_pin, uint16_t tx, uint16_t *rx) |
| Reads and sends a word. More... | |
| void | spi_transfer_block (uint8_t cs_pin, uint8_t *tx, uint8_t *rx, uint8_t length) |
| Reads and sends a byte array. More... | |
| void | quikeval_SPI_connect () |
| Connect SPI pins to QuikEval connector through the Linduino MUX. This will disconnect I2C. More... | |
| void | quikeval_SPI_init () |
| Configure the SPI port for 4Mhz SCK. More... | |
| void | spi_enable (uint8_t spi_clock_divider) |
| Setup the processor for hardware SPI communication. More... | |
| void | spi_disable () |
| Disable the SPI hardware port. More... | |
| void | spi_write (int8_t data) |
| Write a data byte using the SPI hardware. More... | |
| int8_t | spi_read (int8_t data) |
| Read and write a data byte using the SPI hardware. More... | |
| void quikeval_SPI_connect | ( | ) |
Connect SPI pins to QuikEval connector through the Linduino MUX. This will disconnect I2C.
Definition at line 138 of file LT_SPI.cpp.
| void quikeval_SPI_init | ( | ) |
Configure the SPI port for 4Mhz SCK.
This function or spi_enable() must be called before using the other SPI routines.
Definition at line 151 of file LT_SPI.cpp.
| void spi_disable | ( | ) |
Disable the SPI hardware port.
Definition at line 170 of file LT_SPI.cpp.
| void spi_enable | ( | uint8_t | spi_clock_divider | ) |
Setup the processor for hardware SPI communication.
Must be called before using the other SPI routines. Alternatively, call quikeval_SPI_connect(), which automatically calls this function.
| spi_clock_divider | Configures SCK frequency. Use constant defined in header file. |
Definition at line 160 of file LT_SPI.cpp.
| int8_t spi_read | ( | int8_t | data | ) |
Read and write a data byte using the SPI hardware.
Read and write a data byte using the SPI hardware.
| data | The data byte to be written |
Definition at line 189 of file LT_SPI.cpp.
| void spi_transfer_block | ( | uint8_t | cs_pin, |
| uint8_t * | tx, | ||
| uint8_t * | rx, | ||
| uint8_t | length | ||
| ) |
Reads and sends a byte array.
| cs_pin | Chip select pin |
| tx | Byte array to be transmitted |
| rx | Byte array to be received |
| length | Length of array |
Definition at line 125 of file LT_SPI.cpp.
| void spi_transfer_byte | ( | uint8_t | cs_pin, |
| uint8_t | tx, | ||
| uint8_t * | rx | ||
| ) |
Reads and sends a byte.
| cs_pin | Chip select pin |
| tx | Byte to be transmitted |
| rx | Byte to be received |
Definition at line 87 of file LT_SPI.cpp.
| void spi_transfer_word | ( | uint8_t | cs_pin, |
| uint16_t | tx, | ||
| uint16_t * | rx | ||
| ) |
Reads and sends a word.
| cs_pin | Chip select pin |
| tx | Byte to be transmitted |
| rx | Byte to be received |
Definition at line 98 of file LT_SPI.cpp.
| void spi_write | ( | int8_t | data | ) |
Write a data byte using the SPI hardware.
| data | Byte to be written to SPI port |
Definition at line 176 of file LT_SPI.cpp.