![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LT_I2C: Routines to communicate with ATmega328P's hardware I2C port. More...
LT_I2C: Routines to communicate with ATmega328P's hardware I2C port.
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Library Header File for LT_I2C: Routines to communicate with ATmega328P's hardware I2C port.
Definition in file LT_I2C.h.
Go to the source code of this file.
Functions | |
| int8_t | i2c_read_byte (uint8_t address, uint8_t *value) |
| Read a byte, store in "value". More... | |
| int8_t | i2c_write_byte (uint8_t address, uint8_t value) |
| Write "value" byte to device at "address". More... | |
| int8_t | i2c_read_byte_data (uint8_t address, uint8_t command, uint8_t *value) |
| Read a byte of data at register specified by "command", store in "value". More... | |
| int8_t | i2c_write_byte_data (uint8_t address, uint8_t command, uint8_t value) |
| Write a byte of data to register specified by "command". More... | |
| int8_t | i2c_read_word_data (uint8_t address, uint8_t command, uint16_t *value) |
| Read a 16-bit word of data from register specified by "command". More... | |
| int8_t | i2c_write_word_data (uint8_t address, uint8_t command, uint16_t value) |
| Write a 16-bit word of data to register specified by "command". More... | |
| int8_t | i2c_read_block_data (uint8_t address, uint8_t command, uint8_t length, uint8_t *values) |
| Read a block of data, starting at register specified by "command" and ending at (command + length - 1) More... | |
| int8_t | i2c_read_block_data (uint8_t address, uint8_t length, uint8_t *values) |
| Read a block of data, no command byte, reads length number of bytes and stores it in values. More... | |
| int8_t | i2c_write_block_data (uint8_t address, uint8_t command, uint8_t length, uint8_t *values) |
| Write a block of data, starting at register specified by "command" and ending at (command + length - 1) More... | |
| int8_t | i2c_two_byte_command_read_block (uint8_t address, uint16_t command, uint8_t length, uint8_t *values) |
| Write a two command bytes, then receive a block of data. More... | |
| void | quikeval_I2C_init (void) |
| Initializes Linduino I2C port. More... | |
| void | quikeval_I2C_connect (void) |
| Switch MUX to connect I2C pins to QuikEval connector. More... | |
| void | i2c_enable (void) |
| i2c_enable or quikeval_I2C_init must be called before using any of the other I2C routines. More... | |
| int8_t | i2c_start () |
| Write start bit to the hardware I2C port. More... | |
| int8_t | i2c_repeated_start () |
| Write a repeat start bit to the hardware I2C port. More... | |
| void | i2c_stop () |
| Write stop bit to the hardware I2C port. More... | |
| int8_t | i2c_write (uint8_t data) |
| Send a data byte to hardware I2C port. More... | |
| uint8_t | i2c_read (int8_t ack) |
| Read a data byte from the hardware I2C port. More... | |
| int8_t | i2c_poll (uint8_t i2c_address) |
| Poll the I2C port and look for an acknowledge. More... | |
Macros | |
HARDWARE I2C PRESCALER VALUES | |
| #define | HARDWARE_I2C_PRESCALER_1 0 |
| #define | HARDWARE_I2C_PRESCALER_4 1 |
| #define | HARDWARE_I2C_PRESCALER_16 2 |
| #define | HARDWARE_I2C_PRESCALER_64 3 |
I2C READ and WRITE BITS | |
Eighth bit (LSB) of I2C address indicates a "read" or "write". (The first seven bits are the 7-bit I2C address.) | |
| #define | I2C_READ_BIT 0x01 |
| #define | I2C_WRITE_BIT 0x00 |
STATUS BITS | |
| #define | STATUS_START 0x08 |
| #define | STATUS_REPEATED_START 0x10 |
| #define | STATUS_ADDRESS_WRITE_ACK 0x18 |
| #define | STATUS_ADDRESS_WRITE_NACK 0x20 |
| #define | STATUS_WRITE_ACK 0x28 |
| #define | STATUS_WRITE_NACK 0x30 |
| #define | STATUS_ARBITRATION_LOST 0x38 |
| #define | STATUS_ADDRESS_READ_ACK 0x40 |
| #define | STATUS_ADDRESS_READ_NACK 0x48 |
| #define | STATUS_READ_ACK 0x50 |
| #define | STATUS_READ_NACK 0x58 |
TIMEOUT AND DELAY IN US | |
| #define | HW_I2C_DELAY 1 |
| #define | HW_I2C_TIMEOUT 20000 |
ACK OR NACK PARAMETER PASSED TO I2C_READ | |
| #define | WITH_ACK 0 |
| Use with i2c_read(WITH_ACK) to read with an acknowledge. More... | |
| #define | WITH_NACK 1 |
| Use with i2c_read(WITH_NACK) to read without an acknowledge. More... | |
OPTIONAL I2C Address MACRO | |
| #define | I2C_8ADDR(address) (address >> 1) |
| Use to convert an 8-bit I2C address to 7 bits. More... | |
| void i2c_enable | ( | void | ) |
i2c_enable or quikeval_I2C_init must be called before using any of the other I2C routines.
Definition at line 414 of file LT_I2C.cpp.
| int8_t i2c_poll | ( | uint8_t | i2c_address | ) |
Poll the I2C port and look for an acknowledge.
| i2c_address | i2c_address is the address of the slave being polled. |
Definition at line 526 of file LT_I2C.cpp.
| uint8_t i2c_read | ( | int8_t | ack | ) |
Read a data byte from the hardware I2C port.
If ack is 0 then an acknowledge (ACK) is generated, else a NACK is generated.
| ack | If ACK is 0 then an acknowledge is generated, else a NACK is generated. |
Definition at line 491 of file LT_I2C.cpp.
| int8_t i2c_read_block_data | ( | uint8_t | address, |
| uint8_t | command, | ||
| uint8_t | length, | ||
| uint8_t * | values | ||
| ) |
Read a block of data, starting at register specified by "command" and ending at (command + length - 1)
| address | 7-bit I2C address |
| command | Command byte |
| length | Length of array |
| values | Byte array to be read |
Definition at line 244 of file LT_I2C.cpp.
| int8_t i2c_read_block_data | ( | uint8_t | address, |
| uint8_t | length, | ||
| uint8_t * | values | ||
| ) |
Read a block of data, no command byte, reads length number of bytes and stores it in values.
| address | 7-bit I2C address |
| length | Length of array |
| values | Byte array to be read |
Definition at line 291 of file LT_I2C.cpp.
| int8_t i2c_read_byte | ( | uint8_t | address, |
| uint8_t * | value | ||
| ) |
Read a byte, store in "value".
Read a byte, store in "value".
Wire.endTransmission() returns 0, 1, 2, 3, or 4. To maintain consistency with our Legacy LT_I2C library, a zero(false) or a non-zero(true) is tested. 0 .. success 1 .. length to long for buffer 2 .. address send, NACK received 3 .. data send, NACK received 4 .. other twi error (lost bus arbitration, bus error, ..)
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
| address | 7-bit I2C address |
| value | Byte to be read |
Definition at line 93 of file LT_I2C.cpp.
| int8_t i2c_read_byte_data | ( | uint8_t | address, |
| uint8_t | command, | ||
| uint8_t * | value | ||
| ) |
Read a byte of data at register specified by "command", store in "value".
| address | 7-bit I2C address |
| command | Command byte |
| value | Byte to be read |
Definition at line 124 of file LT_I2C.cpp.
| int8_t i2c_read_word_data | ( | uint8_t | address, |
| uint8_t | command, | ||
| uint16_t * | value | ||
| ) |
Read a 16-bit word of data from register specified by "command".
| address | 7-bit I2C address |
| command | Command byte |
| value | Word to be read |
Definition at line 172 of file LT_I2C.cpp.
| int8_t i2c_repeated_start | ( | ) |
Write a repeat start bit to the hardware I2C port.
Definition at line 444 of file LT_I2C.cpp.
| int8_t i2c_start | ( | ) |
Write start bit to the hardware I2C port.
Definition at line 425 of file LT_I2C.cpp.
| void i2c_stop | ( | ) |
Write stop bit to the hardware I2C port.
Definition at line 462 of file LT_I2C.cpp.
| int8_t i2c_two_byte_command_read_block | ( | uint8_t | address, |
| uint16_t | command, | ||
| uint8_t | length, | ||
| uint8_t * | values | ||
| ) |
Write a two command bytes, then receive a block of data.
| address | 7-bit I2C address |
| command | Command word |
| length | Length of array |
| values | Byte array to be read |
Definition at line 345 of file LT_I2C.cpp.
| int8_t i2c_write | ( | uint8_t | data | ) |
Send a data byte to hardware I2C port.
| data | byte that will be written to hardware I2C port. |
Definition at line 470 of file LT_I2C.cpp.
| int8_t i2c_write_block_data | ( | uint8_t | address, |
| uint8_t | command, | ||
| uint8_t | length, | ||
| uint8_t * | values | ||
| ) |
Write a block of data, starting at register specified by "command" and ending at (command + length - 1)
| address | 7-bit I2C address |
| command | Command byte |
| length | Length of array |
| values | Byte array to be written |
Definition at line 321 of file LT_I2C.cpp.
| int8_t i2c_write_byte | ( | uint8_t | address, |
| uint8_t | value | ||
| ) |
Write "value" byte to device at "address".
| address | 7-bit I2C address |
| value | Byte to be written |
Definition at line 109 of file LT_I2C.cpp.
| int8_t i2c_write_byte_data | ( | uint8_t | address, |
| uint8_t | command, | ||
| uint8_t | value | ||
| ) |
Write a byte of data to register specified by "command".
| address | 7-bit I2C address |
| command | Command byte |
| value | Byte to be written |
Definition at line 155 of file LT_I2C.cpp.
| int8_t i2c_write_word_data | ( | uint8_t | address, |
| uint8_t | command, | ||
| uint16_t | value | ||
| ) |
Write a 16-bit word of data to register specified by "command".
| address | 7-bit I2C address |
| command | Command byte |
| value | Word to be written |
Definition at line 216 of file LT_I2C.cpp.
| void quikeval_I2C_connect | ( | void | ) |
Switch MUX to connect I2C pins to QuikEval connector.
This will disconnect SPI pins.
Definition at line 401 of file LT_I2C.cpp.
| void quikeval_I2C_init | ( | void | ) |
Initializes Linduino I2C port.
Before communicating to the I2C port through the QuikEval connector, you must also run quikeval_I2C_connect to connect the I2C port to the QuikEval connector through the QuikEval MUX (and disconnect SPI).
Definition at line 394 of file LT_I2C.cpp.
| #define WITH_ACK 0 |