LTC6953: Ultra-Low Jitter, JESD204B Clock Distributor with Eleven Programmable Outputs.
More...
LTC6953: Ultra-Low Jitter, JESD204B Clock Distributor with Eleven Programmable Outputs.
SPI DATA FORMAT (MSB First):
Write Sequence:
Byte #1 Byte #2
MOSI: A6 A5 A4 A3 A2 A1 A0 W D7 D6 D5 D4 D3 D2 D1 D0
MISO: X X X X X X X X X X X X X X X X
Read Sequence:
Byte #1 Byte #2
MOSI: A6 A5 A4 A3 A2 A1 A0 R X X X X X X X X
MISO: X X X X X X X X D7 D6 D5 D4 D3 D2 D1 D0
W : SPI Write (0)
R : SPI Read (1)
Ax : Address
Dx : Data Bits
X : Don't carehttp://www.linear.com/product/LTC6953
http://www.linear.com/product/LTC6953#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
- Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
- Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
- Neither the name of Analog Devices, Inc. nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
- The use of this software may or may not infringe the patent rights of one or more patent holders. This license does not release you from the requirement that you obtain separate licenses from these patent holders to use this software.
- Use of the software either in source or binary form, must be run on or directly connected to an Analog Devices Inc. component.
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC6953: Ultra-Low Jitter, JESD204B Clock Distributor with Eleven Programmable Outputs
Definition in file LTC6953.h.
|
| uint8_t | LTC6953_read (uint8_t cs, int8_t address) |
| | LTC6953 Read Single Address reads 8 bit Data field to LTC6953. More...
|
| |
| long | LTC6953_read_field (uint8_t cs, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| | LTC6953 Read Single Field For SPI FIELDS located in 1 or multiple address location reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More...
|
| |
| long | get_LTC6953_SPI_FIELD (uint8_t cs, uint8_t f) |
| | Gets the LTC6953 SPI field value calls function LTC6953_read_field, which reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More...
|
| |
| void | LTC6953_write (uint8_t cs, uint8_t address, uint8_t Data) |
| | LTC6953 Write Single Address writes 8 bit Data field to LTC6953. More...
|
| |
| uint8_t | LTC6953_write_field (uint8_t cs, long field_data, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| | LTC6953 Write Single Field For SPI FIELDS in 1 or multiple address locations reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More...
|
| |
| void | set_LTC6953_SPI_FIELD (uint8_t cs, uint8_t f, long field_data) |
| | Sets the LTC6953 SPI field value calls function LTC6953_read_field, which reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More...
|
| |
| void | set_LTC6953_REGS_lkup_tbl (uint8_t lkup_tbl_row) |
| | Writes values to ALL LTC6953 RW addresses from a look-up table. More...
|
| |
| void | LTC6953_init () |
| | Initializes the SPI MAP arrays The values set in initialization are used for all the LTC6953 SPI/WRITE and read functions (set_LTC6953_SPI_FIELD, get_LTC6953_SPI_FIELD, LTC6953_read, LTC6953_write, etc, etc) More...
|
| |
| uint8_t | get_LTC6953_REGSIZE () |
| | returns # of addresses in parts register map (array size) More...
|
| |
| uint8_t | get_LTC6953_SPI_FIELD_NUMBITS (uint8_t f) |
| | returns the number of bits for a given field name in the SPI map More...
|
| |
| uint8_t | get_LTC6953_SPI_FIELD_RW (uint8_t f) |
| | returns if the given field name is (0)read/write or (1)read_only field More...
|
| |
| int8_t | discover_demo_board_local (char *demo_name) |
| | Read the ID string from the EEPROM and determine if any demo board is connected. More...
|
| |
|
| #define | LTC6953_CS QUIKEVAL_CS |
| | Define the SPI CS pin. More...
|
| |
| #define | LTC6953_ADEL0 1 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL1 2 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL2 3 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL3 4 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL4 5 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL5 6 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL6 7 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL7 8 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL8 9 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL9 10 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_ADEL10 11 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL0 12 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL1 13 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL2 14 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL3 15 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL4 16 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL5 17 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL6 18 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL7 19 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL8 20 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL9 21 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_DDEL10 22 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_EZMD 23 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_FILTV 24 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_INVSTAT 25 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD0 26 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD1 27 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD2 28 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD3 29 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD4 30 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD5 31 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD6 32 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD7 33 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD8 34 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD9 35 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MD10 36 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE0 37 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE1 38 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE2 39 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE3 40 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE4 41 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE5 42 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE6 43 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE7 44 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE8 45 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE9 46 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MODE10 47 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP0 48 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP1 49 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP2 50 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP3 51 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP4 52 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP5 53 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP6 54 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP7 55 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP8 56 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP9 57 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_MP10 58 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV0 59 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV1 60 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV2 61 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV3 62 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV4 63 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV5 64 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV6 65 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV7 66 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV8 67 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV9 68 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_OINV10 69 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PART 70 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PDALL 71 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PDVCOPK 72 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD10 73 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD9 74 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD8 75 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD7 76 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD6 77 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD5 78 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD4 79 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD3 80 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD2 81 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD1 82 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_PD0 83 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_POR 84 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_REV 85 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SYSCT 86 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQMD 87 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SSRQ 88 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN0 89 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN1 90 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN2 91 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN3 92 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN4 93 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN5 94 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN6 95 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN7 96 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN8 97 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN9 98 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_SRQEN10 99 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_TEMPO 100 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_nVCOOK 101 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_VCOOK 102 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_x 103 |
| | for spi_map array, defines location for field specific information used to create the spi map More...
|
| |
| #define | LTC6953_NUM_REGADDR 57 |
| | Defines number of LTC6953 SPI registers, used in spi_map array. More...
|
| |
| #define | LTC6953_NUM_REGFIELD 103 |
| | Defines number of LTC6953 SPI fields, used in spi_map array. More...
|
| |
| #define | ADDRx 0 |
| | used for 2nd dim of 2d spi_map array More...
|
| |
| #define | DxMSB 1 |
| | used for 2nd dim of 2d spi_map array More...
|
| |
| #define | NUMBITS 2 |
| | used for 2nd dim of 2d spi_map array More...
|
| |
| #define | R_ONLY 3 |
| | used for 2nd dim of 2d spi_map array More...
|
| |