![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC6811-1 Multicell Battery Monitor. More...
Library for LTC6811-1 Multicell Battery Monitor.
Definition in file LTC6811.cpp.
Go to the source code of this file.
Functions | |
| void | LTC6811_init_reg_limits (uint8_t total_ic, cell_asic *ic) |
| Initialize the Register limits. More... | |
| void | LTC6811_wrcfg (uint8_t total_ic, cell_asic *ic) |
| Write the LTC6811 configuration register. More... | |
| int8_t | LTC6811_rdcfg (uint8_t total_ic, cell_asic *ic) |
| Reads configuration registers of a LTC6811. More... | |
| void | LTC6811_adcv (uint8_t MD, uint8_t DCP, uint8_t CH) |
| Starts cell voltage conversion. More... | |
| void | LTC6811_adax (uint8_t MD, uint8_t CHG) |
| Start a GPIO and Vref2 Conversion. More... | |
| void | LTC6811_adstat (uint8_t MD, uint8_t CHST) |
| Start a Status ADC Conversion. More... | |
| void | LTC6811_adcvax (uint8_t MD, uint8_t DCP) |
| Starts cell voltage and GPIO 1&2 conversion. More... | |
| void | LTC6811_adcvsc (uint8_t MD, uint8_t DCP) |
| Starts cell voltage and SOC conversion. More... | |
| uint8_t | LTC6811_rdcv (uint8_t reg, uint8_t total_ic, cell_asic *ic) |
| Reads and parses the LTC6811 cell voltage registers. More... | |
| int8_t | LTC6811_rdaux (uint8_t reg, uint8_t total_ic, cell_asic *ic) |
| Reads and parses the LTC6811 auxiliary registers. More... | |
| int8_t | LTC6811_rdstat (uint8_t reg, uint8_t total_ic, cell_asic *ic) |
| Reads and parses the LTC6811 stat registers. More... | |
| uint8_t | LTC6811_pladc () |
| Sends the poll ADC command. More... | |
| uint32_t | LTC6811_pollAdc () |
| This function will block operation until the ADC has finished it's conversion. More... | |
| void | LTC6811_clrcell () |
| Clears the LTC6811 cell voltage registers. More... | |
| void | LTC6811_clraux () |
| Clears the LTC6811 Auxiliary registers. More... | |
| void | LTC6811_clrstat () |
| Clears the LTC6811 Stat registers. More... | |
| void | LTC6811_diagn () |
| Starts the Mux Decoder diagnostic self test Running this command will start the Mux Decoder Diagnostic Self Test. More... | |
| void | LTC6811_cvst (uint8_t MD, uint8_t ST) |
| Starts cell voltage self test conversion. More... | |
| void | LTC6811_axst (uint8_t MD, uint8_t ST) |
| Start an Auxiliary Register Self Test Conversion. More... | |
| void | LTC6811_statst (uint8_t MD, uint8_t ST) |
| Start a Status Register Self Test Conversion. More... | |
| void | LTC6811_adol (uint8_t MD, uint8_t DCP) |
| Starts cell voltage overlap conversion. More... | |
| void | LTC6811_adaxd (uint8_t MD, uint8_t CHG) |
| Start an GPIO Redundancy test. More... | |
| void | LTC6811_adstatd (uint8_t MD, uint8_t CHST) |
| Start a Status register redundancy test Conversion. More... | |
| int16_t | LTC6811_run_cell_adc_st (uint8_t adc_reg, uint8_t total_ic, cell_asic *ic, uint8_t md, bool adcopt) |
| Helper function that runs the ADC Self Tests. More... | |
| uint16_t | LTC6811_run_adc_overlap (uint8_t total_ic, cell_asic *ic) |
| Helper Function that runs the ADC Overlap test. More... | |
| int16_t | LTC6811_run_adc_redundancy_st (uint8_t adc_mode, uint8_t adc_reg, uint8_t total_ic, cell_asic *ic) |
| Helper function that runs the ADC Digital Redundancy commands and checks output for errors. More... | |
| void | LTC6811_adow (uint8_t MD, uint8_t PUP, uint8_t CH, uint8_t DCP) |
| Start an open wire Conversion. More... | |
| void | LTC6811_run_openwire_single (uint8_t total_ic, cell_asic *ic) |
| Helper function that runs the data sheet open wire algorithm for single cell detection. More... | |
| void | LTC6811_run_openwire_multi (uint8_t total_ic, cell_asic *ic) |
| Helper function that runs open wire for multiple cell and two consecutive cells detection. More... | |
| void | LTC6811_set_discharge (int Cell, uint8_t total_ic, cell_asic *ic) |
| Helper function to set discharge bit in CFG register. More... | |
| void | LTC6811_clear_discharge (uint8_t total_ic, cell_asic *ic) |
| Clears all of the DCC bits in the configuration registers. More... | |
| void | LTC6811_wrpwm (uint8_t total_ic, uint8_t pwmReg, cell_asic *ic) |
| Write the LTC6811 PWM register. More... | |
| int8_t | LTC6811_rdpwm (uint8_t total_ic, uint8_t pwmReg, cell_asic *ic) |
| Reads pwm registers of a LTC6811 daisy chain. More... | |
| void | LTC6811_wrsctrl (uint8_t total_ic, uint8_t sctrl_reg, cell_asic *ic) |
| Write the LTC6811 Sctrl register. More... | |
| int8_t | LTC6811_rdsctrl (uint8_t total_ic, uint8_t sctrl_reg, cell_asic *ic) |
| Reads sctrl registers of a LTC6811 daisy chain. More... | |
| void | LTC6811_stsctrl () |
| Start Sctrl data communication This command will start the sctrl pulse communication over the spins. More... | |
| void | LTC6811_clrsctrl () |
| Clears the LTC6811 Sctrl registers. More... | |
| void | LTC6811_wrcomm (uint8_t total_ic, cell_asic *ic) |
| Writes to the LTC6811 COMM register. More... | |
| int8_t | LTC6811_rdcomm (uint8_t total_ic, cell_asic *ic) |
| Reads comm registers of a LTC6811 daisy chain. More... | |
| void | LTC6811_stcomm (uint8_t len) |
| Issues a stcomm command and clocks data out of the COMM register. More... | |
| void | LTC6811_check_pec (uint8_t total_ic, uint8_t reg, cell_asic *ic) |
| Helper Function that counts overall PEC errors and register/IC PEC errors. More... | |
| void | LTC6811_reset_crc_count (uint8_t total_ic, cell_asic *ic) |
| Helper Function that resets the PEC error counters. More... | |
| void | LTC6811_init_cfg (uint8_t total_ic, cell_asic *ic) |
| Helper Function to initialize the CFGR data structures. More... | |
| void | LTC6811_set_cfgr (uint8_t nIC, cell_asic *ic, bool refon, bool adcopt, bool gpio[5], bool dcc[12], bool dcto[4], uint16_t uv, uint16_t ov) |
| Helper function to set appropriate bits in CFGR register based on bit function. More... | |
| void | LTC6811_set_cfgr_refon (uint8_t nIC, cell_asic *ic, bool refon) |
| Helper function to turn the refon bit HIGH or LOW. More... | |
| void | LTC6811_set_cfgr_adcopt (uint8_t nIC, cell_asic *ic, bool adcopt) |
| Helper function to turn the ADCOPT bit HIGH or LOW. More... | |
| void | LTC6811_set_cfgr_gpio (uint8_t nIC, cell_asic *ic, bool gpio[5]) |
| void | LTC6811_set_cfgr_dis (uint8_t nIC, cell_asic *ic, bool dcc[12]) |
| void | LTC6811_set_cfgr_dcto (uint8_t nIC, cell_asic *ic, bool dcto[4]) |
| void | LTC6811_set_cfgr_uv (uint8_t nIC, cell_asic *ic, uint16_t uv) |
| Helper function to set uv field in CFGRA register. More... | |
| void | LTC6811_set_cfgr_ov (uint8_t nIC, cell_asic *ic, uint16_t ov) |
| Helper function to set ov field in CFGRA register. More... | |
| void LTC6811_adax | ( | uint8_t | MD, |
| uint8_t | CHG | ||
| ) |
Start a GPIO and Vref2 Conversion.
| MD | ADC Conversion Mode |
| CHG | Sets which GPIO channels are converted |
Definition at line 113 of file LTC6811.cpp.
| void LTC6811_adaxd | ( | uint8_t | MD, |
| uint8_t | CHG | ||
| ) |
Start an GPIO Redundancy test.
| MD | ADC Conversion Mode |
| CHG | Sets which GPIO channels are converted |
Definition at line 268 of file LTC6811.cpp.
| void LTC6811_adcv | ( | uint8_t | MD, |
| uint8_t | DCP, | ||
| uint8_t | CH | ||
| ) |
Starts cell voltage conversion.
| MD | ADC Conversion Mode |
| DCP | Controls if Discharge is permitted during conversion |
| CH | Sets which Cell channels are converted |
Definition at line 104 of file LTC6811.cpp.
| void LTC6811_adcvax | ( | uint8_t | MD, |
| uint8_t | DCP | ||
| ) |
Starts cell voltage and GPIO 1&2 conversion.
| MD | ADC Conversion Mode |
| DCP | Controls if Discharge is permitted during conversion |
Definition at line 129 of file LTC6811.cpp.
| void LTC6811_adcvsc | ( | uint8_t | MD, |
| uint8_t | DCP | ||
| ) |
Starts cell voltage and SOC conversion.
| MD | ADC Conversion Mode |
| DCP | Controls if Discharge is permitted during conversion |
Definition at line 137 of file LTC6811.cpp.
| void LTC6811_adol | ( | uint8_t | MD, |
| uint8_t | DCP | ||
| ) |
Starts cell voltage overlap conversion.
| MD | ADC Conversion Mode |
| DCP | Discharge permitted during conversion |
Definition at line 260 of file LTC6811.cpp.
| void LTC6811_adow | ( | uint8_t | MD, |
| uint8_t | PUP, | ||
| uint8_t | CH, | ||
| uint8_t | DCP | ||
| ) |
Start an open wire Conversion.
| MD | ADC Mode |
| PUP | Discharge Permit |
| CH | Cell selection |
| DCP | Discharge Permit |
Definition at line 319 of file LTC6811.cpp.
| void LTC6811_adstat | ( | uint8_t | MD, |
| uint8_t | CHST | ||
| ) |
Start a Status ADC Conversion.
| MD | ADC Conversion Mode |
| CHST | Sets which Stat channels are converted |
Definition at line 121 of file LTC6811.cpp.
| void LTC6811_adstatd | ( | uint8_t | MD, |
| uint8_t | CHST | ||
| ) |
Start a Status register redundancy test Conversion.
| MD | ADC Conversion Mode |
| CHST | Sets which Status channels are converted |
Definition at line 276 of file LTC6811.cpp.
| void LTC6811_axst | ( | uint8_t | MD, |
| uint8_t | ST | ||
| ) |
Start an Auxiliary Register Self Test Conversion.
| MD | ADC Conversion Mode |
| ST | Sets if self test 1 or 2 is run |
Definition at line 244 of file LTC6811.cpp.
| void LTC6811_check_pec | ( | uint8_t | total_ic, |
| uint8_t | reg, | ||
| cell_asic * | ic | ||
| ) |
Helper Function that counts overall PEC errors and register/IC PEC errors.
| total_ic | Number of ICs in the system |
| reg | Type of register |
| ic | A two dimensional array that will store the data |
Definition at line 458 of file LTC6811.cpp.
| void LTC6811_clear_discharge | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Clears all of the DCC bits in the configuration registers.
| total_ic | Number of ICs in the daisy chain |
| ic | A two dimensional array that will store the data |
Definition at line 368 of file LTC6811.cpp.
| void LTC6811_clraux | ( | ) |
| void LTC6811_clrcell | ( | ) |
| void LTC6811_clrsctrl | ( | ) |
| void LTC6811_clrstat | ( | ) |
| void LTC6811_cvst | ( | uint8_t | MD, |
| uint8_t | ST | ||
| ) |
Starts cell voltage self test conversion.
| MD | ADC Conversion Mode |
| ST | Sets if self test 1 or 2 is run |
Definition at line 236 of file LTC6811.cpp.
| void LTC6811_diagn | ( | ) |
Starts the Mux Decoder diagnostic self test Running this command will start the Mux Decoder Diagnostic Self Test.
This test takes roughly 1ms to complete. The MUXFAIL bit will be updated. The bit will be set to 1 for a failure and 0 if the test has been passed.
Definition at line 230 of file LTC6811.cpp.
| void LTC6811_init_cfg | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Helper Function to initialize the CFGR data structures.
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 475 of file LTC6811.cpp.
| void LTC6811_init_reg_limits | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Initialize the Register limits.
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 66 of file LTC6811.cpp.
| uint8_t LTC6811_pladc | ( | ) |
Sends the poll ADC command.
Definition at line 191 of file LTC6811.cpp.
| uint32_t LTC6811_pollAdc | ( | ) |
This function will block operation until the ADC has finished it's conversion.
Definition at line 197 of file LTC6811.cpp.
| int8_t LTC6811_rdaux | ( | uint8_t | reg, |
| uint8_t | nIC, | ||
| cell_asic * | ic | ||
| ) |
Reads and parses the LTC6811 auxiliary registers.
| reg | Controls which GPIO voltage register is read back |
| total_ic | The number of ICs in the daisy chain |
| ic | A two dimensional array of the parsed gpio voltage codes |
Definition at line 164 of file LTC6811.cpp.
| int8_t LTC6811_rdcfg | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Reads configuration registers of a LTC6811.
| total_ic | Number of ICs |
| ic | A two dimensional array that the function stores the read configuration data |
Definition at line 94 of file LTC6811.cpp.
| int8_t LTC6811_rdcomm | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Reads comm registers of a LTC6811 daisy chain.
| total_ic | Number of ICs in the daisy chain |
| ic | Two dimensional array that the function stores the read comm data. |
Definition at line 442 of file LTC6811.cpp.
| uint8_t LTC6811_rdcv | ( | uint8_t | reg, |
| uint8_t | total_ic, | ||
| cell_asic * | ic | ||
| ) |
Reads and parses the LTC6811 cell voltage registers.
| reg | Controls which cell voltage register is read back. |
| total_ic | The number of ICs in the daisy chain |
| ic | Array of the parsed cell codes from lowest to highest. |
Definition at line 149 of file LTC6811.cpp.
| int8_t LTC6811_rdpwm | ( | uint8_t | total_ic, |
| uint8_t | pwmReg, | ||
| cell_asic * | ic | ||
| ) |
Reads pwm registers of a LTC6811 daisy chain.
| total_ic | Number of ICs |
| pwmReg | Select register |
| ic | A two dimensional array that the function stores the read pwm data |
Definition at line 384 of file LTC6811.cpp.
| int8_t LTC6811_rdsctrl | ( | uint8_t | total_ic, |
| uint8_t | sctrl_reg, | ||
| cell_asic * | ic | ||
| ) |
Reads sctrl registers of a LTC6811 daisy chain.
| total_ic | Number of ICs in the daisy chain |
| sctrl_reg | Select register |
| ic | A two dimensional array that the function stores the read data |
Definition at line 404 of file LTC6811.cpp.
| int8_t LTC6811_rdstat | ( | uint8_t | reg, |
| uint8_t | total_ic, | ||
| cell_asic * | ic | ||
| ) |
Reads and parses the LTC6811 stat registers.
| reg | Determines which Stat register is read back. |
| total_ic | The number of ICs in the system |
| ic | Array of the parsed Stat codes |
Definition at line 180 of file LTC6811.cpp.
| void LTC6811_reset_crc_count | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Helper Function that resets the PEC error counters.
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 467 of file LTC6811.cpp.
| uint16_t LTC6811_run_adc_overlap | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Helper Function that runs the ADC Overlap test.
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 297 of file LTC6811.cpp.
| int16_t LTC6811_run_adc_redundancy_st | ( | uint8_t | adc_mode, |
| uint8_t | adc_reg, | ||
| uint8_t | total_ic, | ||
| cell_asic * | ic | ||
| ) |
Helper function that runs the ADC Digital Redundancy commands and checks output for errors.
| adc_mode | ADC Mode |
| adc_reg | Type of register |
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 307 of file LTC6811.cpp.
| int16_t LTC6811_run_cell_adc_st | ( | uint8_t | adc_reg, |
| uint8_t | total_ic, | ||
| cell_asic * | ic, | ||
| uint8_t | md, | ||
| bool | adcopt | ||
| ) |
Helper function that runs the ADC Self Tests.
| adc_reg | Type of register |
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
| md | ADC Mode |
| adcopt | The adcopt bit in the configuration register |
Definition at line 284 of file LTC6811.cpp.
| void LTC6811_run_openwire_multi | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Helper function that runs open wire for multiple cell and two consecutive cells detection.
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 337 of file LTC6811.cpp.
| void LTC6811_run_openwire_single | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Helper function that runs the data sheet open wire algorithm for single cell detection.
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 329 of file LTC6811.cpp.
| void LTC6811_set_cfgr | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| bool | refon, | ||
| bool | adcopt, | ||
| bool | gpio[5], | ||
| bool | dcc[12], | ||
| bool | dcto[4], | ||
| uint16_t | uv, | ||
| uint16_t | ov | ||
| ) |
Helper function to set appropriate bits in CFGR register based on bit function.
| nIC | Current IC |
| ic | A two dimensional array that will store the data |
| refon | The REFON bit |
| adcopt | The ADCOPT bit |
| gpio | The GPIO bits |
| dcc | The DCC bits |
| dcto | The Dcto bits |
| uv | The UV value |
| ov | The OV value |
Definition at line 483 of file LTC6811.cpp.
| void LTC6811_set_cfgr_adcopt | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| bool | adcopt | ||
| ) |
Helper function to turn the ADCOPT bit HIGH or LOW.
| nIC | Current IC |
| ic | A two dimensional array that will store the data |
| adcopt | The ADCOPT bit |
Definition at line 504 of file LTC6811.cpp.
| void LTC6811_set_cfgr_dcto | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| bool | dcto[4] | ||
| ) |
Definition at line 522 of file LTC6811.cpp.
| void LTC6811_set_cfgr_dis | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| bool | dcc[12] | ||
| ) |
Definition at line 516 of file LTC6811.cpp.
| void LTC6811_set_cfgr_gpio | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| bool | gpio[5] | ||
| ) |
Definition at line 510 of file LTC6811.cpp.
| void LTC6811_set_cfgr_ov | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| uint16_t | ov | ||
| ) |
Helper function to set ov field in CFGRA register.
| nIC | Current IC |
| ic | A two dimensional array that will store the data |
| ov | The OV value |
Definition at line 534 of file LTC6811.cpp.
| void LTC6811_set_cfgr_refon | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| bool | refon | ||
| ) |
Helper function to turn the refon bit HIGH or LOW.
| nIC | Current IC |
| ic | A two dimensional array that will store the data |
| refon | The REFON bit |
Definition at line 498 of file LTC6811.cpp.
| void LTC6811_set_cfgr_uv | ( | uint8_t | nIC, |
| cell_asic * | ic, | ||
| uint16_t | uv | ||
| ) |
Helper function to set uv field in CFGRA register.
| nIC | Current IC |
| ic | A two dimensional array that will store the data |
| uv | The UV value |
Definition at line 528 of file LTC6811.cpp.
| void LTC6811_set_discharge | ( | int | Cell, |
| uint8_t | total_ic, | ||
| cell_asic * | ic | ||
| ) |
Helper function to set discharge bit in CFG register.
| Cell | The cell to be discharged |
| total_ic | Number of ICs in the system |
| ic | A two dimensional array that will store the data |
Definition at line 345 of file LTC6811.cpp.
| void LTC6811_statst | ( | uint8_t | MD, |
| uint8_t | ST | ||
| ) |
Start a Status Register Self Test Conversion.
| MD | ADC Conversion Mode |
| ST | Sets if self test 1 or 2 is run |
Definition at line 252 of file LTC6811.cpp.
| void LTC6811_stcomm | ( | uint8_t | len | ) |
Issues a stcomm command and clocks data out of the COMM register.
| len | Length of data to be transmitted |
Definition at line 452 of file LTC6811.cpp.
| void LTC6811_stsctrl | ( | ) |
Start Sctrl data communication This command will start the sctrl pulse communication over the spins.
Definition at line 418 of file LTC6811.cpp.
| void LTC6811_wrcfg | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Write the LTC6811 configuration register.
| total_ic | The number of ICs being written |
| ic | A two dimensional array of the configuration data that will be written |
Definition at line 86 of file LTC6811.cpp.
| void LTC6811_wrcomm | ( | uint8_t | total_ic, |
| cell_asic * | ic | ||
| ) |
Writes to the LTC6811 COMM register.
| total_ic | Number of ICs in the daisy chain |
| ic | A two dimensional array of the comm data that will be written |
Definition at line 434 of file LTC6811.cpp.
| void LTC6811_wrpwm | ( | uint8_t | total_ic, |
| uint8_t | pwmReg, | ||
| cell_asic * | ic | ||
| ) |
Write the LTC6811 PWM register.
| total_ic | Number of ICs |
| pwmReg | Select register |
| ic | A two dimensional array that the function stores the data in. |
Definition at line 374 of file LTC6811.cpp.
| void LTC6811_wrsctrl | ( | uint8_t | total_ic, |
| uint8_t | sctrl_reg, | ||
| cell_asic * | ic | ||
| ) |
Write the LTC6811 Sctrl register.
| total_ic | Number of ICs in the daisy chain |
| sctrl_reg | Select register |
| ic | A two dimensional array of the data that will be written |
Definition at line 395 of file LTC6811.cpp.