![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC6803-2 Multicell Battery Monitor. More...
Library for LTC6803-2 Multicell Battery Monitor.
Definition in file LTC68032.cpp.
Go to the source code of this file.
Functions | |
| void | LTC6803_initialize () |
| Initializes the SPI port. More... | |
| void | LTC6803_wrcfg (uint8_t total_ic, uint8_t config[][6]) |
| Function that writes configuration of LTC6803-1/-3. More... | |
| int8_t | LTC6803_rdcfg (uint8_t total_ic, uint8_t r_config[][7]) |
| Function that reads configuration of LTC6803-2/-3. More... | |
| void | LTC6803_stcvad () |
| Function that starts Cell Voltage measurement. More... | |
| void | LTC6803_sttmpad () |
| Function that Temp channel voltage measurement. More... | |
| int8_t | LTC6803_rdtmp (uint8_t total_ic, uint16_t temp_codes[][3]) |
| Function that reads Temp Voltage registers. More... | |
| uint8_t | LTC6803_rdcv (uint8_t total_ic, uint16_t cell_codes[][12]) |
| Function that reads Cell Voltage registers. More... | |
| uint8_t | pec8_calc (uint8_t len, uint8_t *data) |
| Function that calculates PEC byte. More... | |
| void | spi_write_array (uint8_t len, uint8_t data[]) |
| Writes an array of bytes out of the SPI port. More... | |
| void | spi_write_read (uint8_t tx_Data[], uint8_t tx_len, uint8_t *rx_data, uint8_t rx_len) |
| Writes and read a set number of bytes using the SPI port. More... | |
| void LTC6803_initialize | ( | ) |
| int8_t LTC6803_rdcfg | ( | uint8_t | total_ic, |
| uint8_t | r_config[][7] | ||
| ) |
Function that reads configuration of LTC6803-2/-3.
Function that reads configuration of LTC6803-2/-4.
Function that reads configuration of LTC6803-1/-3.
| total_ic | total_ic number of LTC6803 ICs in stack |
| r_config | The Function will put the read config register data into this array |
Definition at line 130 of file LTC68032.cpp.
| uint8_t LTC6803_rdcv | ( | uint8_t | total_ic, |
| uint16_t | cell_codes[][12] | ||
| ) |
Function that reads Cell Voltage registers.
| total_ic | total_ic number of LTC6803 ICs in stack |
| cell_codes | The Function will put the parsed measured cell voltages into this array |
Definition at line 249 of file LTC68032.cpp.
| int8_t LTC6803_rdtmp | ( | uint8_t | total_ic, |
| uint16_t | temp_codes[][3] | ||
| ) |
Function that reads Temp Voltage registers.
| total_ic | total_ic number of LTC6803 ICs in stack |
| temp_codes | The Function will put the parsed measured Temp voltages into this array |
Definition at line 202 of file LTC68032.cpp.
| void LTC6803_stcvad | ( | ) |
Function that starts Cell Voltage measurement.
Function to start Cell Voltage measurement.
Definition at line 181 of file LTC68032.cpp.
| void LTC6803_sttmpad | ( | ) |
Function that Temp channel voltage measurement.
Function to start Temp channel voltage measurement.
Definition at line 191 of file LTC68032.cpp.
| void LTC6803_wrcfg | ( | uint8_t | total_ic, |
| uint8_t | config[][6] | ||
| ) |
Function that writes configuration of LTC6803-1/-3.
Function that writes configuration of LTC6803-2/-4.
| total_ic | total_ic number of LTC6803 ICs in stack |
| config | The function will write the 6803 CFGR register with data in the config array |
Definition at line 90 of file LTC68032.cpp.
| uint8_t pec8_calc | ( | uint8_t | len, |
| uint8_t * | data | ||
| ) |
Function that calculates PEC byte.
| len | the length of the data array |
| data | data array |
Definition at line 297 of file LTC68032.cpp.
| void spi_write_array | ( | uint8_t | len, |
| uint8_t | data[] | ||
| ) |
Writes an array of bytes out of the SPI port.
Definition at line 341 of file LTC68032.cpp.
| void spi_write_read | ( | uint8_t | tx_Data[], |
| uint8_t | tx_len, | ||
| uint8_t * | rx_data, | ||
| uint8_t | rx_len | ||
| ) |
Writes and read a set number of bytes using the SPI port.
Definition at line 353 of file LTC68032.cpp.