![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC6603: Dual, Matched, High Frequency Bandpass/Lowpass Filters. More...
LTC6603: Dual, Matched, High Frequency Bandpass/Lowpass Filters.
The LTC6603 is a dual, matched, programmable bandpass or lowpass filter
and differential driver. The selectivity of the LTC6603, combined with its
phase matching and dynamic range, make it ideal for filtering in RFID
systems. With two degree phase matching between channels, the LTC6603 can
be used in applications requiring highly matched filters, such as
transceiver I and Q channels. Gain programmability, and the fully
differential inputs and outputs, simplify implementation in most systems.
SPI DATA FORMAT (MSB First):
Byte #1 Byte #2
Data In : GAIN0 GAIN1 LPF0 LPF1 NOFUNC0 NOFUNC1 SHDN OUT GAIN0 GAIN1 LPF0 LPF1 NOFUNC0 NOFUNC1 SHDN OUT
|---- GAIN, BW CONTROL WORD FOR #2 ----| |---- GAIN, BW CONTROL WORD FOR #1 ----|
GAINx : Gain Control Bits
LPFx : Lowpass Cutoff Frequency Bits
NOFUNCx : Highpass Cutoff Frequency Bits
SHDN : Shutdown Bit
OUT : General Purpose Output Pinhttp://www.analog.com/en/products/amplifiers/adc-drivers/fully-differential-amplifiers/ltc6603.html
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
The views and conclusions contained in the software and documentation are those of the authors and should not be interpreted as representing official policies, either expressed or implied, of Linear Technology Corp.
The Linear Technology Linduino is not affiliated with the official Arduino team. However, the Linduino is only possible because of the Arduino team's commitment to the open-source community. Please, visit http://www.arduino.cc and http://store.arduino.cc , and consider a purchase that will help fund their ongoing work.
Header for LTC6603: Dual Matched, High Frequency Bandpass/Lowpass Filters
Definition in file LTC6603.h.
Go to the source code of this file.
Macros | |
| #define | LTC6603_FREQ_MIN 12 |
| Define external frequency range. More... | |
| #define | LTC6603_FREQ_MAX 80 |
| 80 Mhz More... | |
| #define | LTC6603_CS QUIKEVAL_CS |
| Define the SPI CS pin. More... | |
LTC6603 gain configuration bits. | |
Refer to Table 1 in Data Sheet | |
| #define | LTC6603_GAIN_0dB 0x00 |
| #define | LTC6603_GAIN_6dB 0x80 |
| #define | LTC6603_GAIN_12dB 0x40 |
| #define | LTC6603_GAIN_24dB 0xC0 |
| #define | LTC6603_GAIN_MASK 0x3F |
LTC6603 lowpass cutoff frequency configuration bits. | |
Refer to Table 2 and 3 for Bandwidth | |
| #define | LTC6603_LPF0 0x00 |
| #define | LTC6603_LPF1 0x20 |
| #define | LTC6603_LPF2 0x10 |
| #define | LTC6603_LPF3 0x30 |
| #define | LTC6603_LPF_MASK 0xCF |
LTC6603 Highpass cutoff frequency configuration bits. | |
Refer to Table 2 and 3 for Bandwidth | |
| #define | LTC6603_NOFUNC0 0x00 |
| #define | LTC6603_NOFUNC1 0x08 |
| #define | LTC6603_NOFUNC2 0x04 |
| #define | LTC6603_NOFUNC3 0x0C |
| #define | LTC6603_NOFUNC_MASK 0xF3 |
LTC6603 shutdown/powerup and GPO configuration bits. | |
| #define | LTC6603_SHDN 0x02 |
| Shuts down LTC6603. More... | |
| #define | LTC6603_PRUP 0x00 |
| Turns on LTC6603. More... | |
| #define | LTC6603_ONOFF_MASK 0xFD |
| #define | LTC6603_GPO_HIGH 0x01 |
| Sets the general purpose. More... | |
| #define | LTC6603_GPO_LOW 0x00 |
| #define | LTC6603_GPO_MASK 0xFE |
| void | LTC6603_write (uint8_t cs, uint8_t *tx, uint8_t length) |
| Sends Data to the LTC6603. More... | |
| void LTC6603_write | ( | uint8_t | cs, |
| uint8_t * | tx, | ||
| uint8_t | length | ||
| ) |
Sends Data to the LTC6603.
| cs | Chip Select pin |
| tx | Byte array to be transmitted |
| length | Length of array |
Definition at line 89 of file LTC6603.cpp.
| #define LTC6603_CS QUIKEVAL_CS |
| #define LTC6603_FREQ_MIN 12 |