![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Copyright 2018(c) Analog Devices, Inc. More...
Copyright 2018(c) Analog Devices, Inc.
LTC5566: Dual Programmable Gain Downconverting Mixer
The LTC5566 dual programmable gain downconverting mixer
is ideal for diversity and MIMO receivers that require precise
gain setting. Each channel incorporates an active mixer and a
digital IF VGA with 15.5dB gain control range. The IF gain of
each channel is programmed in 0.5dB steps through the SPI.
SPI DATA FORMAT (MSB First):
Byte #1 Byte #2
Data In : RP2 RT2[1] RT2[0] IF2[4] IF2[3] IF2[2] IF2[1] IF2[0] RP1 RT1[1] RT1[0] IF1[4] IF1[3] IF1[2] IF1[1] IF1[0]
|---- ATT, TUNE, POWER CONTROL WORD FOR MIXER 2 ---| |---- ATT, TUNE, POWER CONTROL WORD FOR MIXER 1 ---|
RPx : Reduced Power Mode Bit
RTx : RF Input Tune Control Bits
IFx : IF Attenuation Control Bitshttp://www.linear.com/product/LTC5566
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC5566: Dual Programmable Gain Downconverting Mixer
Definition in file LTC5566.h.
Go to the source code of this file.
Functions | |
| void | LTC5566_write (uint8_t cs, uint16_t tx, uint16_t *rx) |
| Writes to the LTC5566 twice and reads back the last two bytes to make sure the LTC5566 was loaded properly. More... | |
| uint8_t | LTC5566_dupl_settings () |
| Function to duplicate settings for both LTC5566 channels. More... | |
| uint16_t | LTC5566_diff_settings () |
| Function to apply unique settings for each LTC5566 channel. More... | |
| uint8_t | LTC5566_get_power_mode (char *prompt) |
| Function to get data from user for power mode. More... | |
| uint8_t | LTC5566_get_tune_mode (char *prompt) |
| Function to get data from user for RF input tune mode. More... | |
| uint8_t | LTC5566_get_att (char *prompt) |
| Function to get data from user for IF attenuation. More... | |
| void | LTC5566_decode_output (uint8_t output) |
| Decode the register value read from the LTC5555. More... | |
Macros | |
| #define | LTC5566_CS QUIKEVAL_CS |
| Define the SPI CS pin. More... | |
LTC5566 reduced power mode configuration bit. | |
| #define | LTC5566_FULL_POWER 0x00 |
| #define | LTC5566_REDUCED_POWER 0x80 |
LTC5566 shutdown/powerup and GPO configuration bits. | |
| #define | LTC5566_RF_TUNE_00 0x00 |
| #define | LTC5566_RF_TUNE_01 0x20 |
| #define | LTC5566_RF_TUNE_10 0x40 |
| #define | LTC5566_RF_TUNE_11 0x60 |
| void LTC5566_decode_output | ( | uint8_t | output | ) |
Decode the register value read from the LTC5555.
| output | Raw output from the LTC5566 to decode |
Definition at line 372 of file LTC5566.cpp.
| uint16_t LTC5566_diff_settings | ( | ) |
Function to apply unique settings for each LTC5566 channel.
Definition at line 143 of file LTC5566.cpp.
| uint8_t LTC5566_dupl_settings | ( | ) |
Function to duplicate settings for both LTC5566 channels.
Definition at line 95 of file LTC5566.cpp.
| uint8_t LTC5566_get_att | ( | char * | prompt | ) |
Function to get data from user for IF attenuation.
| prompt | Prompt to ask for the desired attenuation |
Definition at line 319 of file LTC5566.cpp.
| uint8_t LTC5566_get_power_mode | ( | char * | prompt | ) |
Function to get data from user for power mode.
| prompt | Prompt to ask for the desired power mode |
Definition at line 221 of file LTC5566.cpp.
| uint8_t LTC5566_get_tune_mode | ( | char * | prompt | ) |
Function to get data from user for RF input tune mode.
| prompt | Prompt to ask for the desired RF tune mode |
Definition at line 265 of file LTC5566.cpp.
| void LTC5566_write | ( | uint8_t | cs, |
| uint16_t | tx, | ||
| uint16_t * | rx | ||
| ) |
Writes to the LTC5566 twice and reads back the last two bytes to make sure the LTC5566 was loaded properly.
| tx | Chip Select pin |
| rx | Word to be transmitted Output pointer |
Definition at line 88 of file LTC5566.cpp.
| #define LTC5566_CS QUIKEVAL_CS |