![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC5556: Dual Programmable Downconverting Mixer with IF DVGAs. More...
Library for LTC5556: Dual Programmable Downconverting Mixer with IF DVGAs.
Definition in file LTC5556.cpp.
Go to the source code of this file.
Functions | |
| void | LTC5556_write (uint8_t cs, uint16_t tx, uint16_t *rx) |
| Writes to the LTC5556 twice and reads back the last byte to make sure the LTC5556 was loaded properly. More... | |
| uint8_t | LTC5556_dupl_settings () |
| Function to duplicate settings for both LTC5556 channels. More... | |
| uint16_t | LTC5556_diff_settings () |
| Function to apply unique settings for each LTC5556 channel. More... | |
| uint8_t | LTC5556_get_power_mode (char *prompt) |
| Function to get data from user for power mode. More... | |
| uint8_t | LTC5556_get_att (char *prompt) |
| Get attenuation value from user. More... | |
| void | LTC5556_decode_output (uint8_t output_register) |
| Decode the register value read from the LTC5556. More... | |
Variables | |
| uint8_t | mixer_1_value |
| Global Variables. More... | |
| uint8_t | mixer_2_value |
| uint16_t | register_value |
| uint16_t | full_output |
| uint8_t | mixer_1_output |
| uint8_t | mixer_2_output |
| void LTC5556_decode_output | ( | uint8_t | output | ) |
Decode the register value read from the LTC5556.
| output_register | Raw output from the LTC5556 to decode |
Definition at line 293 of file LTC5556.cpp.
| uint16_t LTC5556_diff_settings | ( | ) |
Function to apply unique settings for each LTC5556 channel.
Definition at line 136 of file LTC5556.cpp.
| uint8_t LTC5556_dupl_settings | ( | ) |
Function to duplicate settings for both LTC5556 channels.
Definition at line 97 of file LTC5556.cpp.
| uint8_t LTC5556_get_att | ( | char * | prompt | ) |
Get attenuation value from user.
| prompt | Prompt to ask for the desired attenuation |
Definition at line 240 of file LTC5556.cpp.
| uint8_t LTC5556_get_power_mode | ( | char * | prompt | ) |
Function to get data from user for power mode.
| prompt | Prompt to ask for the desired power mode |
Definition at line 196 of file LTC5556.cpp.
| void LTC5556_write | ( | uint8_t | cs, |
| uint16_t | tx, | ||
| uint16_t * | rx | ||
| ) |
Writes to the LTC5556 twice and reads back the last byte to make sure the LTC5556 was loaded properly.
| tx | Chip Select pin |
| rx | Word to be transmitted Output pointer |
Definition at line 90 of file LTC5556.cpp.
| uint16_t full_output |
Definition at line 80 of file LTC5556.cpp.
| uint8_t mixer_1_output |
Definition at line 83 of file LTC5556.cpp.
| uint8_t mixer_1_value |
Global Variables.
Definition at line 71 of file LTC5556.cpp.
| uint8_t mixer_2_output |
Definition at line 86 of file LTC5556.cpp.
| uint8_t mixer_2_value |
Definition at line 74 of file LTC5556.cpp.
| uint16_t register_value |
Definition at line 77 of file LTC5556.cpp.