![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC4282: High Current Hot Swap Controller with I2C Compatible Monitoring and EEPROM. More...
LTC4282: High Current Hot Swap Controller with I2C Compatible Monitoring and EEPROM.
The LTC4282 Hot Swap controller allows a board to be safely inserted and removed from a live backplane.
Using one or more external N-channel pass transistors, board supply voltage and inrush current is ramped up at an adjustable rate.
An I2C interface and onboard ADC allows for monitoring of board current, voltage, power, energy and fault status.
I2C DATA FORMAT (MSB FIRST):
Data Out:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
Data In:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK Repeat Start SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK
Byte #4 Byte #5
MSB LSB
D15 D14 D13 D12 D11 D10 D9 D8 MACK D7 D6 D5 D4 D3 D2 D1 D0 MNACK STOP
START : I2C Start
Repeat Start: I2c Repeat Start
STOP : I2C Stop
SAx : I2C Address
SACK : I2C Slave Generated Acknowledge (Active Low)
MACK : I2C Master Generated Acknowledge (Active Low)
MNACK : I2c Master Generated Not Acknowledge
W : I2C Write (0)
R : I2C Read (1)
Cx : Command Code
Dx : Data Bits
X : Don't care
Example Code:
Read Voltage and Current
static uint8_t CTRLREG_LSB = LTC4282_VIN_MODE_12_V;
static uint8_t ILIM_ADJUST = (LTC4282_ILIM_ADJUST_25_V_0|LTC4282_FOLDBACK_MODE_12_V_0|LTC4282_ADC_VSOURCE|LTC4282_ADC_GPIO2_MODE)& ~LTC4282_ADC_16_BIT;
resistor = .1; // Resistor Value On Demo Board
ack |= LTC4282_read_16_bits(LTC4282_I2C_ADDRESS, LTC4282_VSOURCE_MSB_REG, &voltage_code); //!< Read Voltage Code From VSOURCE Register
vsource = LTC4282_code_to_voltage(voltage_code, voltage_fullscale); //!< Convert Voltage Code to Current Source Voltage
ack |= LTC4282_read_16_bits(LTC4282_I2C_ADDRESS, LTC4282_CURRENT_MSB_REG, t_code); // Reads the voltage code across sense resistor
current = LTC4282_code_to_current(current_code, resistor); // Calculates current from current code, resistor value.
ack |= LTC4282_read_16_bits(LTC4282_I2C_ADDRESS, LTC4282_VOLTAGE_MSB_REG, &voltage_code); // Reads voltage voltage code
VIN = LTC4282_VIN_code_to_voltage(voltage_code); // Calculates VIN voltage from VIN code and lsbhttp://www.linear.com/product/LTC4282
http://www.linear.com/product/LTC4282#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC4282: High Current Hot Swap Controller with I2C Compatible Monitoring and EEPROM
Definition in file LTC4282.h.
Go to the source code of this file.
Data Structures | |
| union | LT_union_int64_8bytes |
Functions | |
| int8_t | LTC4282_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC4282. More... | |
| int8_t | LTC4282_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write an 16-bit code to the LTC4282. More... | |
| int8_t | LTC4282_write_32_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t code) |
| Write an 32-bit code to the LTC4282. More... | |
| int8_t | LTC4282_write_48_bits (uint8_t i2c_address, uint8_t adc_command, uint64_t code) |
| Write an 48-bit code to the LTC4282. More... | |
| int8_t | LTC4282_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Read an 8-bit code from the LTC4282. More... | |
| int8_t | LTC4282_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Read a 16-bit code from the LTC4282. More... | |
| int8_t | LTC4282_read_32_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t *adc_code) |
| Read a 32-bit code from the LTC4282. More... | |
| int8_t | LTC4282_read_48_bits (uint8_t i2c_address, uint8_t adc_command, uint64_t *adc_code) |
| Read a 48-bit code from the LTC4282. More... | |
| float | LTC4282_code_to_VGPIO (uint16_t code) |
| Convert ADC code to VGPIO. More... | |
| float | LTC4282_code_to_voltage (uint16_t code, float fullscaleVoltage) |
| Convert ADC code to voltage. More... | |
| float | LTC4282_code_to_current (uint16_t code, float resistor) |
| Convert ADC code to current. More... | |
| float | LTC4282_code_to_power (uint16_t code, float fullscaleVoltage, float resistor) |
| Convert ADC code to power. More... | |
| float | LTC4282_code_to_energy (uint64_t code, float fullscaleVoltage, float resistor, float tConv) |
| Convert ADC code to energy. More... | |
| float | LTC4282_code_to_coulombs (uint64_t code, float resistor, float tConv) |
| Convert ADC code to coulombs. More... | |
| float | LTC4282_code_to_avg_power (uint64_t code, float energy, float tConv) |
| Convert ADC code to average power. More... | |
| float | LTC4282_code_to_avg_current (uint64_t code, float coulombs, float tConv) |
| Convert ADC code to average current. More... | |
| float | LTC4282_code_to_GPIO_alarm (uint8_t code) |
| Convert ADC code to GPIO alarm voltage. More... | |
| float | LTC4282_code_to_volt_alarm (uint8_t code, float fullscaleVoltage) |
| Convert ADC code to alarm voltage. More... | |
| float | LTC4282_code_to_current_alarm (uint8_t code, float resistor) |
| Convert ADC code to alarm current. More... | |
| float | LTC4282_code_to_power_alarm (uint8_t code, float fullscaleVoltage, float resistor) |
| Convert ADC code to alarm power. More... | |
| uint8_t | LTC4282_VGPIO_to_code_alarm (float vgpio) |
| Convert GPIO voltage to alarm code. More... | |
| uint8_t | LTC4282_volt_to_code_alarm (float volt, float fullscaleVoltage) |
| Convert voltage to alarm code. More... | |
| uint8_t | LTC4282_current_to_code_alarm (float current, float resistor) |
| Convert current to alarm code. More... | |
| uint8_t | LTC4282_power_to_code_alarm (float power, float resistor, float fullscaleVoltage) |
| Convert power to alarm code. More... | |
Macros | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
LTC4282 I2C Address | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Use table to select address
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_I2C_ADDRESS 0x4A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_I2C_MASS_WRITE 0x5F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_I2C_ALERT_RESPONSE 0x19 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Registers | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_CONTROL_MSB_REG 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_CONTROL_LSB_REG 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ALERT_MSB_REG 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ALERT_LSB_REG 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FAULT_LOG_REG 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ADC_ALERT_LOG_REG 0x05 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FET_BAD_FAULT_TIME_REG 0x06 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO_CONFIG_REG 0x07 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_ALARM_MIN_REG 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_ALARM_MAX_REG 0x09 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_ALARM_MIN_REG 0x0A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_ALARM_MAX_REG 0x0B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_ALARM_MIN_REG 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_ALARM_MAX_REG 0x0D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_ALARM_MIN_REG 0x0E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_ALARM_MAX_REG 0x0F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_CLK_DEC_REG 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_REG 0x11 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_METER_MSB5_REG 0x12 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_METER_MSB4_REG 0x13 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_METER_MSB3_REG 0x14 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_METER_MSB2_REG 0x15 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_METER_MSB1_REG 0x16 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_METER_LSB_REG 0x17 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_TICK_COUNTER_MSB3_REG 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_TICK_COUNTER_MSB2_REG 0x19 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_TICK_COUNTER_MSB1_REG 0x1A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_TICK_COUNTER_LSB_REG 0x1B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ALERT_CONTROL_REG 0x1C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ADC_CONTROL_REG 0x1D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_STATUS_MSB_REG 0x1E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_STATUS_LSB_REG 0x1F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_CONTROL_MSB_REG 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_CONTROL_LSB_REG 0x21 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_ALERT_MSB_REG 0x22 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_ALERT_LSB_REG 0x23 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_FAULT_REG 0x24 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_ADC_ALERT_LOG_REG 0x25 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_FET_BAD_FAULT_TIME_REG 0x26 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_GPIO_CONFIG_REG 0x27 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_VSOURCE_ALARM_MIN_REG 0x28 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_VSOURCE_ALARM_MAX_REG 0x29 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_VGPIO_ALARM_MIN_REG 0x2A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_VGPIO_ALARM_MAX_REG 0x2B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_VSENSE_ALARM_MIN_REG 0x2C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_VSENSE_ALARM_MAX_REG 0x2D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_POWER_ALARM_MIN_REG 0x2E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_POWER_ALARM_MAX_REG 0x2F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_CLK_DEC_REG 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_ILIM_ADJUST_REG 0x31 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_MSB_REG 0x34 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_LSB_REG 0x35 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_MIN_MSB_REG 0x36 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_MIN_LSB_REG 0x37 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_MAX_MSB_REG 0x38 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_MAX_LSB_REG 0x39 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_MSB_REG 0x3A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_LSB_REG 0x3B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_MIN_MSB_REG 0x3C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_MIN_LSB_REG 0x3D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_MAX_MSB_REG 0x3E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_MAX_LSB_REG 0x3F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_MSB_REG 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_LSB_REG 0x41 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_MIN_MSB_REG 0x42 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_MIN_LSB_REG 0x43 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_MAX_MSB_REG 0x44 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_MAX_LSB_REG 0x45 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_MSB_REG 0x46 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_LSB_REG 0x47 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_MIN_MSB_REG 0x48 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_MIN_LSB_REG 0x49 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_MAX_MSB_REG 0x4A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_MAX_LSB_REG 0x4B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_SPARE_MSB3_REG 0x4C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_SPARE_MSB2_REG 0x4D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_SPARE_MSB1_REG 0x4E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EE_SPARE_LSB_REG 0x4F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Command Codes | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ON_FAULT_MASK 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ON_DELAY 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ON_ENB 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_MASS_WRITE 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FET_ON 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OC_AUTORETRY 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_UV_AUTORETRY 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OV_AUTORETRY 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FB_MODE_EXTERNAL 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FB_MODE_5 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FB_MODE_10 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FB_MODE_15 0xC0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_UV_MODE_EXTERNAL 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_UV_MODE_5 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_UV_MODE_10 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_UV_MODE_15 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OV_MODE_EXTERNAL 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OV_MODE_5 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OV_MODE_10 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OV_MODE_15 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VIN_MODE_3_V_3 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VIN_MODE_5_V 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VIN_MODE_12_V 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VIN_MODE_24_V 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_EEPROM_DONE_ALERT 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FET_BAD_FAULT_ALERT 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FET_SHORT_ALERT 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ON_ALERT 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_PB_ALERT 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OC_ALERT 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_UV_ALERT 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OV_ALERT 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_ALARM_HIGH 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_POWER_ALARM_LOW 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_ALARM_HIGH 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSENSE_ALARM_LOW 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_ALARM_HIGH 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VSOURCE_ALARM_LOW 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_ALARM_HIGH 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VGPIO_ALARM_LOW 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO3_PD 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO2_PD 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO1_CONFIG_POWER_GOOD 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO1_CONFIG_POWER_BAD 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO1_CONFIG_OUTPUT 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO1_CONFIG_INPUT 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO1_OUTPUT 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ADC_CONV_ALERT 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_STRESS_TO_GPIO2 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_METER_OF_ALERT 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_COULOMB_METER 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_TICK_OUT 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_INT_CLK_OUT 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_12_V_5 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_15_V_6 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_18_V_7 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_21_V_8 0x60 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_25_V_0 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_28_V_1 0xA0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_31_V_2 0xC0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_34_V_3 0xE0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FOLDBACK_MODE_3_V_3 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FOLDBACK_MODE_5_V_0 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FOLDBACK_MODE_12_V_0 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FOLDBACK_MODE_24_V_0 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ADC_VSOURCE 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ADC_GPIO2_MODE 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ADC_16_BIT 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ENABLE_ALERT_GENERATED 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ENABLE_ALERT_PD 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_DISABLE_ALERT_GENERATED 0x7F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_DISABLE_ALERT_PD 0xBF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_REBOOT 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ENABLE_METER_RESET 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ENABLE_METER_HALT 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ENABLE_FAULT_LOG 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GATEUP 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ADC_HALT 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_DISABLE_METER_RESET 0xBF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_DISABLE_METER_HALT 0xDF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_DISABLE_FAULT_LOG 0xFB | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Register MASKS | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FB_MODE_MASK 0xC0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| LTC4282 Register MASKS. More... | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_UV_MODE_MASK 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_OV_MODE_MASK 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_VIN_MODE_MASK 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_ILIM_ADJUST_MASK 0xE0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_FOLDBACK_MASK 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC4282_GPIO1_CONFIG_MASK 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Variables | |
LTC4282 LSB's | |
| const float | LTC4282_ADC_FS = 40E-3 |
| LTC4282 LSB's. More... | |
| const float | LTC4282_VSOURCE_24V_FS = 33.28 |
| const float | LTC4282_VSOURCE_12V_FS = 16.64 |
| const float | LTC4282_VSOURCE_5V_FS = 8.32 |
| const float | LTC4282_VSOURCE_3V3_FS = 5.547 |
| const float | LTC4282_GPIO_FS = 1.28 |
| float LTC4282_code_to_avg_current | ( | uint64_t | code, |
| float | coulombs, | ||
| float | tConv | ||
| ) |
Convert ADC code to average current.
| code | Code to be converted to average power |
| coulombs | Energy value |
| tConv | Conversion Time |
Definition at line 224 of file LTC4282.cpp.
| float LTC4282_code_to_avg_power | ( | uint64_t | code, |
| float | energy, | ||
| float | tConv | ||
| ) |
Convert ADC code to average power.
| code | Code to be converted to average power |
| energy | Energy value |
| tConv | Conversion Time |
Definition at line 216 of file LTC4282.cpp.
| float LTC4282_code_to_coulombs | ( | uint64_t | code, |
| float | resistor, | ||
| float | tConv | ||
| ) |
Convert ADC code to coulombs.
| code | Code to be converted to Coulombs |
| resistor | Sense Resistor Value |
| tConv | Conversion Time |
Definition at line 208 of file LTC4282.cpp.
| float LTC4282_code_to_current | ( | uint16_t | code, |
| float | resistor | ||
| ) |
Convert ADC code to current.
| code | Code to be converted to current |
| resistor | Sense Resistor Value |
Definition at line 185 of file LTC4282.cpp.
| float LTC4282_code_to_current_alarm | ( | uint8_t | code, |
| float | resistor | ||
| ) |
Convert ADC code to alarm current.
| code | Code to be converted to current |
| resistor | Sense Resistor Value |
Definition at line 248 of file LTC4282.cpp.
| float LTC4282_code_to_energy | ( | uint64_t | code, |
| float | fullscaleVoltage, | ||
| float | resistor, | ||
| float | tConv | ||
| ) |
Convert ADC code to energy.
| code | Code to be converted to energy |
| fullscaleVoltage | Fullscale VSOURCE Voltage |
| resistor | Sense Resistor Value |
| tConv | Conversion Time |
Definition at line 200 of file LTC4282.cpp.
| float LTC4282_code_to_GPIO_alarm | ( | uint8_t | code | ) |
Convert ADC code to GPIO alarm voltage.
| code | Code to be converted to voltage |
Definition at line 232 of file LTC4282.cpp.
| float LTC4282_code_to_power | ( | uint16_t | code, |
| float | fullscaleVoltage, | ||
| float | resistor | ||
| ) |
Convert ADC code to power.
| code | Code to be converted to power |
| fullscaleVoltage | Fullscale VSOURCE Voltage |
| resistor | Sense Resistor Value |
Definition at line 193 of file LTC4282.cpp.
| float LTC4282_code_to_power_alarm | ( | uint8_t | code, |
| float | fullscaleVoltage, | ||
| float | resistor | ||
| ) |
Convert ADC code to alarm power.
| code | Code to be converted to power |
| fullscaleVoltage | Fullscale VSOURCE voltage |
| resistor | Sense Resistor Value |
Definition at line 256 of file LTC4282.cpp.
| float LTC4282_code_to_VGPIO | ( | uint16_t | code | ) |
Convert ADC code to VGPIO.
| code | Code to be converted to voltage |
Definition at line 168 of file LTC4282.cpp.
| float LTC4282_code_to_volt_alarm | ( | uint8_t | code, |
| float | fullscaleVoltage | ||
| ) |
Convert ADC code to alarm voltage.
| code | Code to be converted to voltage |
| fullscaleVoltage | Fullscale VSOURCE voltage |
Definition at line 240 of file LTC4282.cpp.
| float LTC4282_code_to_voltage | ( | uint16_t | code, |
| float | fullscaleVoltage | ||
| ) |
Convert ADC code to voltage.
| code | Code to be converted to voltage |
| fullscaleVoltage | Fullscale VSOURCE Voltage |
Definition at line 177 of file LTC4282.cpp.
| uint8_t LTC4282_current_to_code_alarm | ( | float | current, |
| float | resistor | ||
| ) |
Convert current to alarm code.
| current | Current value to be converted to alarm code |
| resistor | Sense Resistor Value |
Definition at line 280 of file LTC4282.cpp.
| uint8_t LTC4282_power_to_code_alarm | ( | float | power, |
| float | resistor, | ||
| float | fullscaleVoltage | ||
| ) |
Convert power to alarm code.
| power | Power value to be converted to alarm code |
| resistor | Sense Resistor Value |
| fullscaleVoltage | Fullsvale voltage value to convert voltage into alarm code |
Definition at line 288 of file LTC4282.cpp.
| int8_t LTC4282_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Read an 8-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the register |
Definition at line 120 of file LTC4282.cpp.
| int8_t LTC4282_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Read a 16-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the |
Definition at line 129 of file LTC4282.cpp.
| int8_t LTC4282_read_32_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t * | adc_code | ||
| ) |
Read a 32-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the |
Definition at line 140 of file LTC4282.cpp.
| int8_t LTC4282_read_48_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint64_t * | adc_code | ||
| ) |
Read a 48-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the |
Definition at line 154 of file LTC4282.cpp.
| uint8_t LTC4282_VGPIO_to_code_alarm | ( | float | vgpio | ) |
Convert GPIO voltage to alarm code.
| vgpio | VGPIO voltage to be converted to alarm code |
Definition at line 264 of file LTC4282.cpp.
| uint8_t LTC4282_volt_to_code_alarm | ( | float | volt, |
| float | fullscaleVoltage | ||
| ) |
Convert voltage to alarm code.
| volt | Voltage to be converted to alarm code |
| fullscaleVoltage | Fullscale voltage value to convert voltage into alarm code |
Definition at line 272 of file LTC4282.cpp.
| int8_t LTC4282_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 69 of file LTC4282.cpp.
| int8_t LTC4282_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write an 16-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 81 of file LTC4282.cpp.
| int8_t LTC4282_write_32_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t | code | ||
| ) |
Write an 32-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 91 of file LTC4282.cpp.
| int8_t LTC4282_write_48_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint64_t | code | ||
| ) |
Write an 48-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 105 of file LTC4282.cpp.