![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC4282: High Current Hot Swap Controller with I2C Compatible Monitoring and EEPROM. More...
Library for LTC4282: High Current Hot Swap Controller with I2C Compatible Monitoring and EEPROM.
Definition in file LTC4282.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTC4282_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC4282. More... | |
| int8_t | LTC4282_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write an 16-bit code to the LTC4282. More... | |
| int8_t | LTC4282_write_32_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t code) |
| Write an 32-bit code to the LTC4282. More... | |
| int8_t | LTC4282_write_48_bits (uint8_t i2c_address, uint8_t adc_command, uint64_t code) |
| Write an 48-bit code to the LTC4282. More... | |
| int8_t | LTC4282_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Read an 8-bit code from the LTC4282. More... | |
| int8_t | LTC4282_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Read a 16-bit code from the LTC4282. More... | |
| int8_t | LTC4282_read_32_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t *adc_code) |
| Read a 32-bit code from the LTC4282. More... | |
| int8_t | LTC4282_read_48_bits (uint8_t i2c_address, uint8_t adc_command, uint64_t *adc_code) |
| Read a 48-bit code from the LTC4282. More... | |
| float | LTC4282_code_to_VGPIO (uint16_t code) |
| Convert ADC code to VGPIO. More... | |
| float | LTC4282_code_to_voltage (uint16_t code, float fullscaleVoltage) |
| Convert ADC code to voltage. More... | |
| float | LTC4282_code_to_current (uint16_t code, float resistor) |
| Convert ADC code to current. More... | |
| float | LTC4282_code_to_power (uint16_t code, float fullscaleVoltage, float resistor) |
| Convert ADC code to power. More... | |
| float | LTC4282_code_to_energy (uint64_t code, float fullscaleVoltage, float resistor, float tConv) |
| Convert ADC code to energy. More... | |
| float | LTC4282_code_to_coulombs (uint64_t code, float resistor, float tConv) |
| Convert ADC code to coulombs. More... | |
| float | LTC4282_code_to_avg_power (uint64_t code, float energy, float tConv) |
| Convert ADC code to average power. More... | |
| float | LTC4282_code_to_avg_current (uint64_t code, float coulombs, float tConv) |
| Convert ADC code to average current. More... | |
| float | LTC4282_code_to_GPIO_alarm (uint8_t code) |
| Convert ADC code to GPIO alarm voltage. More... | |
| float | LTC4282_code_to_volt_alarm (uint8_t code, float fullscaleVoltage) |
| Convert ADC code to alarm voltage. More... | |
| float | LTC4282_code_to_current_alarm (uint8_t code, float resistor) |
| Convert ADC code to alarm current. More... | |
| float | LTC4282_code_to_power_alarm (uint8_t code, float fullscaleVoltage, float resistor) |
| Convert ADC code to alarm power. More... | |
| uint8_t | LTC4282_VGPIO_to_code_alarm (float vgpio) |
| Convert GPIO voltage to alarm code. More... | |
| uint8_t | LTC4282_volt_to_code_alarm (float volt, float fullscaleVoltage) |
| Convert voltage to alarm code. More... | |
| uint8_t | LTC4282_current_to_code_alarm (float current, float resistor) |
| Convert current to alarm code. More... | |
| uint8_t | LTC4282_power_to_code_alarm (float power, float resistor, float fullscaleVoltage) |
| Convert power to alarm code. More... | |
| float LTC4282_code_to_avg_current | ( | uint64_t | code, |
| float | coulombs, | ||
| float | tConv | ||
| ) |
Convert ADC code to average current.
| code | Code to be converted to average power |
| coulombs | Energy value |
| tConv | Conversion Time |
Definition at line 224 of file LTC4282.cpp.
| float LTC4282_code_to_avg_power | ( | uint64_t | code, |
| float | energy, | ||
| float | tConv | ||
| ) |
Convert ADC code to average power.
| code | Code to be converted to average power |
| energy | Energy value |
| tConv | Conversion Time |
Definition at line 216 of file LTC4282.cpp.
| float LTC4282_code_to_coulombs | ( | uint64_t | code, |
| float | resistor, | ||
| float | tConv | ||
| ) |
Convert ADC code to coulombs.
| code | Code to be converted to Coulombs |
| resistor | Sense Resistor Value |
| tConv | Conversion Time |
Definition at line 208 of file LTC4282.cpp.
| float LTC4282_code_to_current | ( | uint16_t | code, |
| float | resistor | ||
| ) |
Convert ADC code to current.
| code | Code to be converted to current |
| resistor | Sense Resistor Value |
Definition at line 185 of file LTC4282.cpp.
| float LTC4282_code_to_current_alarm | ( | uint8_t | code, |
| float | resistor | ||
| ) |
Convert ADC code to alarm current.
| code | Code to be converted to current |
| resistor | Sense Resistor Value |
Definition at line 248 of file LTC4282.cpp.
| float LTC4282_code_to_energy | ( | uint64_t | code, |
| float | fullscaleVoltage, | ||
| float | resistor, | ||
| float | tConv | ||
| ) |
Convert ADC code to energy.
| code | Code to be converted to energy |
| fullscaleVoltage | Fullscale VSOURCE Voltage |
| resistor | Sense Resistor Value |
| tConv | Conversion Time |
Definition at line 200 of file LTC4282.cpp.
| float LTC4282_code_to_GPIO_alarm | ( | uint8_t | code | ) |
Convert ADC code to GPIO alarm voltage.
| code | Code to be converted to voltage |
Definition at line 232 of file LTC4282.cpp.
| float LTC4282_code_to_power | ( | uint16_t | code, |
| float | fullscaleVoltage, | ||
| float | resistor | ||
| ) |
Convert ADC code to power.
| code | Code to be converted to power |
| fullscaleVoltage | Fullscale VSOURCE Voltage |
| resistor | Sense Resistor Value |
Definition at line 193 of file LTC4282.cpp.
| float LTC4282_code_to_power_alarm | ( | uint8_t | code, |
| float | fullscaleVoltage, | ||
| float | resistor | ||
| ) |
Convert ADC code to alarm power.
| code | Code to be converted to power |
| fullscaleVoltage | Fullscale VSOURCE voltage |
| resistor | Sense Resistor Value |
Definition at line 256 of file LTC4282.cpp.
| float LTC4282_code_to_VGPIO | ( | uint16_t | code | ) |
Convert ADC code to VGPIO.
| code | Code to be converted to voltage |
Definition at line 168 of file LTC4282.cpp.
| float LTC4282_code_to_volt_alarm | ( | uint8_t | code, |
| float | fullscaleVoltage | ||
| ) |
Convert ADC code to alarm voltage.
| code | Code to be converted to voltage |
| fullscaleVoltage | Fullscale VSOURCE voltage |
Definition at line 240 of file LTC4282.cpp.
| float LTC4282_code_to_voltage | ( | uint16_t | code, |
| float | fullscaleVoltage | ||
| ) |
Convert ADC code to voltage.
| code | Code to be converted to voltage |
| fullscaleVoltage | Fullscale VSOURCE Voltage |
Definition at line 177 of file LTC4282.cpp.
| uint8_t LTC4282_current_to_code_alarm | ( | float | current, |
| float | resistor | ||
| ) |
Convert current to alarm code.
| current | Current value to be converted to alarm code |
| resistor | Sense Resistor Value |
Definition at line 280 of file LTC4282.cpp.
| uint8_t LTC4282_power_to_code_alarm | ( | float | power, |
| float | resistor, | ||
| float | fullscaleVoltage | ||
| ) |
Convert power to alarm code.
| power | Power value to be converted to alarm code |
| resistor | Sense Resistor Value |
| fullscaleVoltage | Fullsvale voltage value to convert voltage into alarm code |
Definition at line 288 of file LTC4282.cpp.
| int8_t LTC4282_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Read an 8-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the register |
Definition at line 120 of file LTC4282.cpp.
| int8_t LTC4282_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Read a 16-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the |
Definition at line 129 of file LTC4282.cpp.
| int8_t LTC4282_read_32_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t * | adc_code | ||
| ) |
Read a 32-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the |
Definition at line 140 of file LTC4282.cpp.
| int8_t LTC4282_read_48_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint64_t * | adc_code | ||
| ) |
Read a 48-bit code from the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| adc_code | Value that will be read from the |
Definition at line 154 of file LTC4282.cpp.
| uint8_t LTC4282_VGPIO_to_code_alarm | ( | float | vgpio | ) |
Convert GPIO voltage to alarm code.
| vgpio | VGPIO voltage to be converted to alarm code |
Definition at line 264 of file LTC4282.cpp.
| uint8_t LTC4282_volt_to_code_alarm | ( | float | volt, |
| float | fullscaleVoltage | ||
| ) |
Convert voltage to alarm code.
| volt | Voltage to be converted to alarm code |
| fullscaleVoltage | Fullscale voltage value to convert voltage into alarm code |
Definition at line 272 of file LTC4282.cpp.
| int8_t LTC4282_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 69 of file LTC4282.cpp.
| int8_t LTC4282_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write an 16-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 81 of file LTC4282.cpp.
| int8_t LTC4282_write_32_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t | code | ||
| ) |
Write an 32-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 91 of file LTC4282.cpp.
| int8_t LTC4282_write_48_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint64_t | code | ||
| ) |
Write an 48-bit code to the LTC4282.
| i2c_address | Register address for the LTC4282 |
| adc_command | The "command byte" for the LTC4282 |
| code | Value that will be written to the register |
Definition at line 105 of file LTC4282.cpp.