![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC4261: Negative Voltage Hot Swap Controllers with ADC and I2C Monitoring. More...
Library for LTC4261: Negative Voltage Hot Swap Controllers with ADC and I2C Monitoring.
Definition in file LTC4261.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTC4261_write (uint8_t i2c_address, uint8_t command, uint8_t code) |
| Write an 8-bit code to the LTC4261. More... | |
| int8_t | LTC4261_read (uint8_t i2c_address, uint8_t command, uint8_t *code) |
| Reads an 8-bit adc_code from LTC4261. More... | |
| int8_t | LTC4261_read_10_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 10-bit adc_code from LTC4261. More... | |
| int8_t | LTC4261_ARA (uint8_t alert_response_address, uint8_t *i2c_address) |
| SMBus Alert Response Protocol: Sends an alert response command and releases /ALERT pin. More... | |
| float | LTC4261_ADIN_code_to_voltage (uint16_t adc_code, float LTC4261_ADIN_lsb, float resistor_divider_ratio) |
| Calculate the LTC4261 ADIN voltage. More... | |
| float | LTC4261_code_to_current (uint16_t adc_code, float resistor, float LTC4261_DELTA_SENSE_lsb) |
| Calculate the LTC4261 current with a sense resistor. More... | |
| float LTC4261_ADIN_code_to_voltage | ( | uint16_t | adc_code, |
| float | LTC4261_ADIN_lsb, | ||
| float | resistor_divider_ratio | ||
| ) |
Calculate the LTC4261 ADIN voltage.
| adc_code | The ADC value |
| LTC4261_ADIN_lsb | ADIN lsb weight |
| resistor_divider_ratio | the ratio that the voltages have been divided down |
Definition at line 110 of file LTC4261.cpp.
| int8_t LTC4261_ARA | ( | uint8_t | alert_response_address, |
| uint8_t * | i2c_address | ||
| ) |
SMBus Alert Response Protocol: Sends an alert response command and releases /ALERT pin.
LTC4261 responds with its address
| alert_response_address | the Alert Response Address on the I2C bus |
| i2c_address | the address of the alert source |
Definition at line 102 of file LTC4261.cpp.
| float LTC4261_code_to_current | ( | uint16_t | adc_code, |
| float | resistor, | ||
| float | LTC4261_DELTA_SENSE_lsb | ||
| ) |
Calculate the LTC4261 current with a sense resistor.
| adc_code | The ADC value |
| resistor | The resistor value |
| LTC4261_DELTA_SENSE_lsb | Delta sense lsb weight |
Definition at line 119 of file LTC4261.cpp.
| int8_t LTC4261_read | ( | uint8_t | i2c_address, |
| uint8_t | command, | ||
| uint8_t * | code | ||
| ) |
Reads an 8-bit adc_code from LTC4261.
| i2c_address | I2C Address for the LTC4261 |
| command | The "command byte" for the LTC4261 that corresponds to register address |
| code | Value that will be read from the register |
Definition at line 82 of file LTC4261.cpp.
| int8_t LTC4261_read_10_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 10-bit adc_code from LTC4261.
| i2c_address | I2C Address for the LTC4261 |
| adc_command | The "command byte" for the LTC4261 that corresponds to register address |
| adc_code | Value that will be read from the register. |
Definition at line 91 of file LTC4261.cpp.
| int8_t LTC4261_write | ( | uint8_t | i2c_address, |
| uint8_t | command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC4261.
| i2c_address | I2C Address for the LTC4261 |
| command | The "command byte" for the LTC4261 that corresponds to register address |
| code | Value that will be written to the register |
Definition at line 73 of file LTC4261.cpp.