Go to the source code of this file.
|
| void | ltc2970_gpio_up (LT_SMBus *smbus, uint8_t ltc2970_i2c_address, int gpio_number) |
| | Set GPIO_n high. More...
|
| |
| void | ltc2970_gpio_down (LT_SMBus *smbus, uint8_t ltc2970_i2c_address, int gpio_number) |
| | Set GPIO_n low. More...
|
| |
| void | ltc2970_dac_disconnect (LT_SMBus *smbus, uint8_t ltc2970_i2c_address, int dac_number) |
| | Disconnect a DAC from its channel. More...
|
| |
| void | ltc2970_hard_connect_dac (LT_SMBus *smbus, uint8_t ltc2970_i2c_address, int dac_number, uint8_t dac_value_8) |
| | Unceremoniously connect DAC0 to the control node set DAC to a hard value no attempt to equalize voltages. More...
|
| |
| int | ltc2970_soft_connect_dac (LT_SMBus *smbus, uint8_t ltc2970_i2c_address, int dac_number) |
| | soft-connect DACn to its controlled node More...
|
| |
| void | ltc2970_servo_to_adc_val (LT_SMBus *smbus, uint8_t ltc2970_i2c_address, int channel_number, uint16_t code) |
| | Servo once to a given ADC value. More...
|
| |
| void | ltc2970_print_die_temp (LT_SMBus *smbus, uint8_t ltc2970_i2c_address) |
| | Prints die temperature on the LTC2970. More...
|
| |
| void | ltc2970_read_faults (LT_SMBus *smbus, uint8_t ltc2970_i2c_address) |
| | Read FAULT, FAULT_LA, and FAULT_LA_INDEX registers print the results. More...
|
| |
◆ ltc2970_dac_disconnect()
| void ltc2970_dac_disconnect |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address, |
|
|
int |
dac_number |
|
) |
| |
Disconnect a DAC from its channel.
- Returns
- void
Definition at line 51 of file LTC2970.cpp.
◆ ltc2970_gpio_down()
| void ltc2970_gpio_down |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address, |
|
|
int |
gpio_number |
|
) |
| |
Set GPIO_n low.
- Returns
- void
Definition at line 28 of file LTC2970.cpp.
◆ ltc2970_gpio_up()
| void ltc2970_gpio_up |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address, |
|
|
int |
gpio_number |
|
) |
| |
Set GPIO_n high.
- Returns
- void
Definition at line 5 of file LTC2970.cpp.
◆ ltc2970_hard_connect_dac()
| void ltc2970_hard_connect_dac |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address, |
|
|
int |
dac_number, |
|
|
uint8_t |
dac_value_8 |
|
) |
| |
Unceremoniously connect DAC0 to the control node set DAC to a hard value no attempt to equalize voltages.
Unceremoniously connect DAC0 to the control node no attempt to equalize voltages.
- Returns
- void
Definition at line 82 of file LTC2970.cpp.
◆ ltc2970_print_die_temp()
| void ltc2970_print_die_temp |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address |
|
) |
| |
Prints die temperature on the LTC2970.
- Returns
- void
Definition at line 265 of file LTC2970.cpp.
◆ ltc2970_read_faults()
| void ltc2970_read_faults |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address |
|
) |
| |
Read FAULT, FAULT_LA, and FAULT_LA_INDEX registers print the results.
- Returns
- void
Definition at line 289 of file LTC2970.cpp.
◆ ltc2970_servo_to_adc_val()
| void ltc2970_servo_to_adc_val |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address, |
|
|
int |
channel_number, |
|
|
uint16_t |
code |
|
) |
| |
Servo once to a given ADC value.
- Returns
- void
Definition at line 227 of file LTC2970.cpp.
◆ ltc2970_soft_connect_dac()
| int ltc2970_soft_connect_dac |
( |
LT_SMBus * |
smbus, |
|
|
uint8_t |
ltc2970_i2c_address, |
|
|
int |
dac_number |
|
) |
| |
soft-connect DACn to its controlled node
- Returns
- int
Definition at line 114 of file LTC2970.cpp.