![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2944: Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement. More...
LTC2944: Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement.
The LTC®2944 measures battery charge state, battery voltage,
battery current and its own temperature in portable
product applications. The wide input voltage range allows
use with multicell batteries up to 60V. A precision coulomb
counter integrates current through a sense resistor between
the battery’s positive terminal and the load or charger.
Voltage, current and temperature are measured with an
internal 14-bit No Latency ΔΣ™ ADC. The measurements
are stored in internal registers accessible via the onboard
I2C/SMBus Interface.
I2C DATA FORMAT (MSB FIRST):
Data Out:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
Data In:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK Repeat Start SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK
Byte #4 Byte #5
MSB LSB
D15 D14 D13 D12 D11 D10 D9 D8 MACK D7 D6 D5 D4 D3 D2 D1 D0 MNACK STOP
START : I2C Start
Repeat Start: I2c Repeat Start
STOP : I2C Stop
SAx : I2C Address
SACK : I2C Slave Generated Acknowledge (Active Low)
MACK : I2C Master Generated Acknowledge (Active Low)
MNACK : I2c Master Generated Not Acknowledge
W : I2C Write (0)
R : I2C Read (1)
Cx : Command Code
Dx : Data Bits
X : Don't care
Example Code:
Read charge, current, and voltage.
adc_command = LTC2944_SENSE_MONITOR | LTC2944_AUTOMATIC_MODE; // Builds commands to set LTC2944 to automatic mode
ack |= LTC2944_write(LTC2944_I2C_ADDRESS, LTC2944_CONTROL_REG, adc_command); // Sets the LTC2944 to automatic mode
resistor = .1; // Resistor Value On Demo Board
ack |= LTC2944_read_16_bits(LTC2944_I2C_ADDRESS, LTC2944_CHARGE_MSB_REG, &charge_code); // Reads the ADC registers that contains charge value
charge = LTC2944_code_to_coulombs(charge_code, resistor, prescalarValue); // Calculates charge from charge code, resistor and prescalar
ack |= LTC2944_read_16_bits(LTC2944_I2C_ADDRESS, LTC2944_CURRENT_MSB_REG, ¤t_code); // Reads the voltage code across sense resistor
current = LTC2944_code_to_current(current_code, resistor); // Calculates current from current code, resistor value.
ack |= LTC2944_read_16_bits(LTC2944_I2C_ADDRESS, LTC2944_VOLTAGE_MSB_REG, &voltage_code); // Reads voltage voltage code
VIN = LTC2944_VIN_code_to_voltage(voltage_code); // Calculates VIN voltage from VIN code and lsbHeader for LTC2944: Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement
Definition in file LTC2944.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2944_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC2944. More... | |
| int8_t | LTC2944_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write a 16-bit code to the LTC2944. More... | |
| int8_t | LTC2944_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Reads an 8-bit adc_code from LTC2944. More... | |
| int8_t | LTC2944_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 16-bit adc_code from LTC2944. More... | |
| float | LTC2944_code_to_coulombs (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2944 charge in Coulombs. More... | |
| float | LTC2944_code_to_mAh (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2944 charge in mAh. More... | |
| float | LTC2944_code_to_voltage (uint16_t adc_code) |
| Calculate the LTC2944 SENSE+ voltage. More... | |
| float | LTC2944_code_to_current (uint16_t adc_code, float resistor) |
| Calculate the LTC2944 current with a sense resistor. More... | |
| float | LTC2944_code_to_kelvin_temperature (uint16_t adc_code) |
| Calculate the LTC2944 temperature. More... | |
| float | LTC2944_code_to_celcius_temperature (uint16_t adc_code) |
| Calculate the LTC2944 temperature. More... | |
Macros | |||||||||||||||||||||||||||||||||||||||||||||||||||
LTC2944 I2C Address | |||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_I2C_ADDRESS 0x64 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_I2C_ALERT_RESPONSE 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||
Registers | |||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_STATUS_REG 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CONTROL_REG 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_ACCUM_CHARGE_MSB_REG 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_ACCUM_CHARGE_LSB_REG 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CHARGE_THRESH_HIGH_MSB_REG 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CHARGE_THRESH_HIGH_LSB_REG 0x05 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CHARGE_THRESH_LOW_MSB_REG 0x06 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CHARGE_THRESH_LOW_LSB_REG 0x07 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_VOLTAGE_MSB_REG 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_VOLTAGE_LSB_REG 0x09 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_VOLTAGE_THRESH_HIGH_MSB_REG 0x0A | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_VOLTAGE_THRESH_HIGH_LSB_REG 0x0B | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_VOLTAGE_THRESH_LOW_MSB_REG 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_VOLTAGE_THRESH_LOW_LSB_REG 0x0D | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CURRENT_MSB_REG 0x0E | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CURRENT_LSB_REG 0x0F | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CURRENT_THRESH_HIGH_MSB_REG 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CURRENT_THRESH_HIGH_LSB_REG 0x11 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CURRENT_THRESH_LOW_MSB_REG 0x12 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CURRENT_THRESH_LOW_LSB_REG 0x13 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_TEMPERATURE_MSB_REG 0x14 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_TEMPERATURE_LSB_REG 0x15 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_TEMPERATURE_THRESH_HIGH_REG 0x16 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_TEMPERATURE_THRESH_LOW_REG 0x17 | ||||||||||||||||||||||||||||||||||||||||||||||||||
Command Codes | |||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_AUTOMATIC_MODE 0xC0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_SCAN_MODE 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_MANUAL_MODE 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_SLEEP_MODE 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_1 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_4 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_16 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_64 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_256 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_1024 0x28 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_4096 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_PRESCALAR_M_4096_2 0x31 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_ALERT_MODE 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_CHARGE_COMPLETE_MODE 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_DISABLE_ALCC_PIN 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2944_SHUTDOWN_MODE 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||
Variables | |
Conversion Constants | |
| const float | LTC2944_CHARGE_lsb = 0.34E-3 |
| const float | LTC2944_VOLTAGE_lsb = 4.32E-3 |
| const float | LTC2944_CURRENT_lsb = 31.25E-6 |
| const float | LTC2944_TEMPERATURE_lsb = 0.25 |
| const float | LTC2944_FULLSCALE_VOLTAGE = 70.8 |
| const float | LTC2944_FULLSCALE_CURRENT = 64E-3 |
| const float | LTC2944_FULLSCALE_TEMPERATURE = 510 |
| float LTC2944_code_to_celcius_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2944 temperature.
| adc_code | The RAW ADC value |
Definition at line 161 of file LTC2944.cpp.
| float LTC2944_code_to_coulombs | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2944 charge in Coulombs.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 120 of file LTC2944.cpp.
| float LTC2944_code_to_current | ( | uint16_t | adc_code, |
| float | resistor | ||
| ) |
Calculate the LTC2944 current with a sense resistor.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
Definition at line 145 of file LTC2944.cpp.
| float LTC2944_code_to_kelvin_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2944 temperature.
| adc_code | The RAW ADC value |
Definition at line 153 of file LTC2944.cpp.
| float LTC2944_code_to_mAh | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2944 charge in mAh.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 129 of file LTC2944.cpp.
| float LTC2944_code_to_voltage | ( | uint16_t | adc_code | ) |
Calculate the LTC2944 SENSE+ voltage.
| adc_code | The RAW ADC value |
Definition at line 137 of file LTC2944.cpp.
| int8_t LTC2944_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Reads an 8-bit adc_code from LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| adc_code | Value that will be read from the register. |
Definition at line 98 of file LTC2944.cpp.
| int8_t LTC2944_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 16-bit adc_code from LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| adc_code | Value that will be read from the register. |
Definition at line 109 of file LTC2944.cpp.
| int8_t LTC2944_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| code | Value that will be written to the register. |
Definition at line 77 of file LTC2944.cpp.
| int8_t LTC2944_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write a 16-bit code to the LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| code | Value that will be written to the register. |
Definition at line 88 of file LTC2944.cpp.