![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2943: Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement. More...
LTC2943: Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement.
LTC2943-1: Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement.
The LTC2943 measures battery charge state, battery voltage,
battery current and its own temperature in portable
product applications. The wide input voltage range allows
use with multicell batteries up to 20V. A precision coulomb
counter integrates current through a sense resistor between
the battery’s positive terminal and the load or charger.
Voltage, current and temperature are measured with an
internal 14-bit No Latency ΔΣ™ ADC. The measurements
are stored in internal registers accessible via the onboard
I2C/SMBus Interface.
I2C DATA FORMAT (MSB FIRST):
Data Out:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
Data In:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK Repeat Start SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK
Byte #4 Byte #5
MSB LSB
D15 D14 D13 D12 D11 D10 D9 D8 MACK D7 D6 D5 D4 D3 D2 D1 D0 MNACK STOP
START : I2C Start
Repeat Start: I2c Repeat Start
STOP : I2C Stop
SAx : I2C Address
SACK : I2C Slave Generated Acknowledge (Active Low)
MACK : I2C Master Generated Acknowledge (Active Low)
MNACK : I2c Master Generated Not Acknowledge
W : I2C Write (0)
R : I2C Read (1)
Cx : Command Code
Dx : Data Bits
X : Don't care
Example Code:
Read charge, current, and voltage.
adc_command = LTC2943_SENSE_MONITOR | LTC2943_AUTOMATIC_MODE; // Builds commands to set LTC2943 to automatic mode
ack |= LTC2943_write(LTC2943_I2C_ADDRESS, LTC2943_CONTROL_REG, adc_command); // Sets the LTC2943 to automatic mode
resistor = .1; // Resistor Value On Demo Board
ack |= LTC2943_read_16_bits(LTC2943_I2C_ADDRESS, LTC2943_CHARGE_MSB_REG, &charge_code); // Reads the ADC registers that contains charge value
charge = LTC2943_code_to_coulombs(charge_code, resistor, prescalarValue); // Calculates charge from charge code, resistor and prescalar
ack |= LTC2943_read_16_bits(LTC2943_I2C_ADDRESS, LTC2943_CURRENT_MSB_REG, ¤t_code); // Reads the voltage code across sense resistor
current = LTC2943_code_to_current(current_code, resistor); // Calculates current from current code, resistor value.
ack |= LTC2943_read_16_bits(LTC2943_I2C_ADDRESS, LTC2943_VOLTAGE_MSB_REG, &voltage_code); // Reads voltage voltage code
VIN = LTC2943_VIN_code_to_voltage(voltage_code); // Calculates VIN voltage from VIN code and lsbhttp://www.linear.com/product/LTC2943 http://www.linear.com/product/LTC2943-1
http://www.linear.com/product/LTC2943#demoboards http://www.linear.com/product/LTC2943-1#demoboards
Header for LTC2943: Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement
Definition in file LTC2943.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2943_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC2943. More... | |
| int8_t | LTC2943_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write a 16-bit code to the LTC2943. More... | |
| int8_t | LTC2943_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Reads an 8-bit adc_code from LTC2943. More... | |
| int8_t | LTC2943_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 16-bit adc_code from LTC2943. More... | |
| float | LTC2943_code_to_coulombs (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2943 charge in Coulombs. More... | |
| float | LTC2943_code_to_mAh (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2943 charge in mAh. More... | |
| float | LTC2943_code_to_voltage (uint16_t adc_code) |
| Calculate the LTC2943 SENSE+ voltage. More... | |
| float | LTC2943_code_to_current (uint16_t adc_code, float resistor) |
| Calculate the LTC2943 current with a sense resistor. More... | |
| float | LTC2943_code_to_kelvin_temperature (uint16_t adc_code) |
| Calculate the LTC2943 temperature. More... | |
| float | LTC2943_code_to_celcius_temperature (uint16_t adc_code) |
| Calculate the LTC2943 temperature. More... | |
Macros | |||||||||||||||||||||||||||||||||||||||||||||||||||
LTC2943 I2C Address | |||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_I2C_ADDRESS 0x64 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_I2C_ALERT_RESPONSE 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||
Registers | |||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_STATUS_REG 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CONTROL_REG 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_ACCUM_CHARGE_MSB_REG 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_ACCUM_CHARGE_LSB_REG 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CHARGE_THRESH_HIGH_MSB_REG 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CHARGE_THRESH_HIGH_LSB_REG 0x05 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CHARGE_THRESH_LOW_MSB_REG 0x06 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CHARGE_THRESH_LOW_LSB_REG 0x07 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_VOLTAGE_MSB_REG 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_VOLTAGE_LSB_REG 0x09 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_VOLTAGE_THRESH_HIGH_MSB_REG 0x0A | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_VOLTAGE_THRESH_HIGH_LSB_REG 0x0B | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_VOLTAGE_THRESH_LOW_MSB_REG 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_VOLTAGE_THRESH_LOW_LSB_REG 0x0D | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CURRENT_MSB_REG 0x0E | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CURRENT_LSB_REG 0x0F | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CURRENT_THRESH_HIGH_MSB_REG 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CURRENT_THRESH_HIGH_LSB_REG 0x11 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CURRENT_THRESH_LOW_MSB_REG 0x12 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CURRENT_THRESH_LOW_LSB_REG 0x13 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_TEMPERATURE_MSB_REG 0x14 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_TEMPERATURE_LSB_REG 0x15 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_TEMPERATURE_THRESH_HIGH_REG 0x16 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_TEMPERATURE_THRESH_LOW_REG 0x17 | ||||||||||||||||||||||||||||||||||||||||||||||||||
Command Codes | |||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_AUTOMATIC_MODE 0xC0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_SCAN_MODE 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_MANUAL_MODE 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_SLEEP_MODE 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_1 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_4 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_16 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_64 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_256 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_1024 0x28 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_4096 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_PRESCALAR_M_4096_2 0x31 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_ALERT_MODE 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_CHARGE_COMPLETE_MODE 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_DISABLE_ALCC_PIN 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2943_SHUTDOWN_MODE 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||
Variables | |||||||||||||||||
Conversion Constants | |||||||||||||||||
| |||||||||||||||||
| const float | LTC2943_CHARGE_lsb = 0.34E-3 | ||||||||||||||||
| const float | LTC2943_VOLTAGE_lsb = 1.44E-3 | ||||||||||||||||
| const float | LTC2943_CURRENT_lsb = 29.3E-6 | ||||||||||||||||
| const float | LTC2943_TEMPERATURE_lsb = 0.25 | ||||||||||||||||
| const float | LTC2943_FULLSCALE_VOLTAGE = 23.6 | ||||||||||||||||
| const float | LTC2943_FULLSCALE_CURRENT = 60E-3 | ||||||||||||||||
| const float | LTC2943_FULLSCALE_TEMPERATURE = 510 | ||||||||||||||||
| float LTC2943_code_to_celcius_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2943 temperature.
| adc_code | The RAW ADC value |
Definition at line 164 of file LTC2943.cpp.
| float LTC2943_code_to_coulombs | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2943 charge in Coulombs.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 123 of file LTC2943.cpp.
| float LTC2943_code_to_current | ( | uint16_t | adc_code, |
| float | resistor | ||
| ) |
Calculate the LTC2943 current with a sense resistor.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
Definition at line 148 of file LTC2943.cpp.
| float LTC2943_code_to_kelvin_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2943 temperature.
| adc_code | The RAW ADC value |
Definition at line 156 of file LTC2943.cpp.
| float LTC2943_code_to_mAh | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2943 charge in mAh.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 132 of file LTC2943.cpp.
| float LTC2943_code_to_voltage | ( | uint16_t | adc_code | ) |
Calculate the LTC2943 SENSE+ voltage.
| adc_code | The RAW ADC value |
Definition at line 140 of file LTC2943.cpp.
| int8_t LTC2943_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Reads an 8-bit adc_code from LTC2943.
| i2c_address | Register address for the LTC2943 |
| adc_command | The "command byte" for the LTC2943 |
| adc_code | Value that will be read from the register. |
Definition at line 101 of file LTC2943.cpp.
| int8_t LTC2943_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 16-bit adc_code from LTC2943.
| i2c_address | Register address for the LTC2943 |
| adc_command | The "command byte" for the LTC2943 |
| adc_code | Value that will be read from the register. |
Definition at line 112 of file LTC2943.cpp.
| int8_t LTC2943_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC2943.
| i2c_address | Register address for the LTC2943 |
| adc_command | The "command byte" for the LTC2943 |
| code | Value that will be written to the register. |
Definition at line 80 of file LTC2943.cpp.
| int8_t LTC2943_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write a 16-bit code to the LTC2943.
| i2c_address | Register address for the LTC2943 |
| adc_command | The "command byte" for the LTC2943 |
| code | Value that will be written to the register. |
Definition at line 91 of file LTC2943.cpp.