![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC24XX General Library: Functions and defines for all SINC4 Delta Sigma ADCs. More...
LTC24XX General Library: Functions and defines for all SINC4 Delta Sigma ADCs.
LTC2442 / LTC2444 / LTC2445 / LTC2448 / LTC2449 (Are there don't care bits in the low channel counts?
SPI DATA FORMAT (MSB First):
Byte #1 Byte #2
Data Out : !EOC DMY SIG D28 D27 D26 D25 D24 D23 D22 D21 D20 D19 D18 D17 D16
Data In : 1 0 EN SGL OS S2 S1 S0 OSR3 OSR2 OSR1 OSR1 SPD X X X
Byte #3 Byte #4
D15 D14 D13 D12 D11 D10 D9 D8 D7 D6 D5 D4 *D3 *D2 *D1 *D0
X X X X X X X X X X X X X X X X
!EOC : End of Conversion Bit (Active Low)
DMY : Dummy Bit (Always 0)
SIG : Sign Bit (1-data positive, 0-data negative)
Dx : Data Bits
*Dx : Data Bits Below lsb
EN : Enable Bit (0-keep previous mode, 1-change mode)
SGL : Enable Single-Ended Bit (0-differential, 1-single-ended)
OS : ODD/Sign Bit
Sx : Address Select Bit
0SRX : Over Sampling Rate Bits
SPD : Double Output Rate Select Bit (0-Normal rate, auto-calibration on, 2x rate, auto_calibration off)
Command Byte #1
1 0 EN SGL OS S2 S1 S0 Comments
1 0 0 X X X X X Keep Previous Mode
1 0 1 0 X X X X Differential Mode
1 0 1 1 X X X X Single-Ended Mode
| Coversion Rate | RMS | ENOB | OSR | Latency
Command Byte #2 |Internal | External | Noise | | |
| 9MHz | 10.24MHz | | | |
OSR3 OSR2 OSR1 OSR1 SPD | Clock | Clock | | | |
0 0 0 0 0 Keep Previous Speed/Resolution
0 0 0 1 0 3.52kHz 4kHz 23uV 17 64 none
0 0 1 0 0 1.76kHz 2kHz 3.5uV 20.1 128 none
0 0 1 1 0 880Hz 1kHz 2uV 21.3 256 none
0 1 0 0 0 440Hz 500Hz 1.4uV 21.8 512 none
0 1 0 1 0 220Hz 250Hz 1uV 22.4 1024 none
0 1 1 0 0 110Hz 125Hz 750nV 22.9 2048 none
0 1 1 1 0 55Hz 62.5Hz 510nV 23.4 4096 none
1 0 0 0 0 27.5Hz 31.25Hz 375nV 24 8192 none
1 0 0 1 0 13.75Hz 15.625Hz 250nV 24.4 16384 none
1 1 1 1 0 6.87kHz 7.8125Hz 200nV 24.6 32768 none
0 0 0 0 1 Keep Previous Speed/Resolution
OSR3 OSR2 OSR1 OSR1 1 2X Mode *all clock speeds double
Example Code:
Read Channel 0 in Single-Ended with OSR of 65536
uint16_t miso_timeout = 1000;
adc_command = LTC2449_CH0 | LTC2449_OSR_32768 | LTC2449_SPEED_2X; // Build ADC command for channel 0
// OSR = 32768*2 = 65536
if(LTC2449_EOC_timeout(LTC2449_CS, miso_timeout)) // Check for EOC
return; // Exit if timeout is reached
LTC2449_read(LTC2449_CS, adc_command, &adc_code); // Throws out last reading
if(LTC2449_EOC_timeout(LTC2449_CS, miso_timeout)) // Check for EOC
return; // Exit if timeout is reached
LTC2449_read(LTC2449_CS, adc_command, &adc_code); // Obtains the current reading and stores to adc_code variable
// Convert adc_code to voltage
adc_voltage = LTC2449_code_to_voltage(adc_code, LTC2449_lsb, LTC2449_offset_code);http://www.linear.com/product/LTC2449
http://www.linear.com/product/LTC2449#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2449: 24-Bit, 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution
Definition in file LTC24XX_general.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC24XX_EOC_timeout (uint8_t cs, uint16_t miso_timeout) |
| Checks for EOC with a specified timeout. More... | |
| void | LTC24XX_SPI_32bit_data (uint8_t cs, int32_t *adc_code) |
| Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result. More... | |
| void | LTC24XX_SPI_8bit_command_32bit_data (uint8_t cs, uint8_t adc_command, int32_t *adc_code) |
| Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result. More... | |
| void | LTC24XX_SPI_16bit_command_32bit_data (uint8_t cs, uint8_t adc_command_high, uint8_t adc_command_low, int32_t *adc_code) |
| Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result. More... | |
| void | LTC24XX_SPI_2ch_ping_pong_32bit_data (uint8_t cs, uint8_t *adc_channel, int32_t *code) |
| Reads from LTC24XX two channel "Ping-Pong" ADC, placing the channel information in the adc_channel parameter and returning the 32 bit result with the channel bit cleared so the data format matches the rest of the family. More... | |
| void | LTC24XX_SPI_24bit_data (uint8_t cs, int32_t *adc_code) |
| Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result. More... | |
| void | LTC24XX_SPI_8bit_command_24bit_data (uint8_t cs, uint8_t adc_command, int32_t *adc_code) |
| Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result. More... | |
| void | LTC24XX_SPI_16bit_command_24bit_data (uint8_t cs, uint8_t adc_command_high, uint8_t adc_command_low, int32_t *adc_code) |
| Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result. More... | |
| void | LTC24XX_SPI_8bit_command_16bit_data (uint8_t cs, uint8_t adc_command, int32_t *adc_code) |
| Reads from LTC24XX ADC that accepts a 8 bit configuration and returns a 16 bit result. More... | |
| void | LTC24XX_SPI_2ch_ping_pong_24bit_data (uint8_t cs, uint8_t *adc_channel, int32_t *code) |
| Reads from LTC24XX two channel "Ping-Pong" ADC, placing the channel information in the adc_channel parameter and returning the 32 bit result with the channel bit cleared so the data format matches the rest of the family. More... | |
| int8_t | LTC24XX_I2C_32bit_data (uint8_t i2c_address, int32_t *adc_code, uint16_t eoc_timeout) |
| Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result. More... | |
| int8_t | LTC24XX_I2C_8bit_command_32bit_data (uint8_t i2c_address, uint8_t adc_command, int32_t *adc_code, uint16_t eoc_timeout) |
| Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result. More... | |
| int8_t | LTC24XX_I2C_16bit_command_32bit_data (uint8_t i2c_address, uint8_t adc_command_high, uint8_t adc_command_low, int32_t *adc_code, uint16_t eoc_timeout) |
| Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result. More... | |
| int8_t | LTC24XX_I2C_24bit_data (uint8_t i2c_address, int32_t *adc_code, uint16_t eoc_timeout) |
| Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result. More... | |
| int8_t | LTC24XX_I2C_8bit_command_24bit_data (uint8_t i2c_address, uint8_t adc_command, int32_t *adc_code, uint16_t eoc_timeout) |
| Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result. More... | |
| int8_t | LTC24XX_I2C_16bit_command_24bit_data (uint8_t i2c_address, uint8_t adc_command_high, uint8_t adc_command_low, int32_t *adc_code, uint16_t eoc_timeout) |
| Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result. More... | |
| float | LTC24XX_SE_code_to_voltage (int32_t adc_code, float vref) |
| Calculates the voltage corresponding to an ADC code, given the reference voltage. More... | |
| float | LTC24XX_diff_code_to_voltage (int32_t adc_code, float vref) |
| Calculates the voltage corresponding to an ADC code, given the reference voltage. More... | |
| float | LTC24XX_diff_code_to_calibrated_voltage (int32_t adc_code, float LTC24XX_lsb, int32_t LTC24XX_offset_code) |
| Calculates the voltage corresponding to an ADC code, given lsb weight (in volts) and the calibrated ADC offset code (zero code that is subtracted from adc_code). More... | |
| void | LTC24XX_calibrate_voltage (int32_t zero_code, int32_t fs_code, float zero_voltage, float fs_voltage, float *LTC24XX_lsb, int32_t *LTC24XX_offset_code) |
| Calculate the lsb weight and offset code given a full-scale code and a measured zero-code. More... | |
Macros | |
| #define | LTC24XX_CS QUIKEVAL_CS |
| Define the SPI CS pin. More... | |
Mode Configuration for High Speed Family | |
In 2X Mode, A non offset binary 0 can be produced. This is corrected in the differential code to voltage functions. To disable this correction, uncomment The following #define. | |
| #define | LTC24XX_HS_MULTI_KEEP_PREVIOUS_MODE 0x80 |
| #define | LTC24XX_HS_MULTI_KEEP_PREVIOUS_SPEED_RESOLUTION 0x00 |
| #define | LTC24XX_HS_MULTI_SPEED_1X 0x00 |
| #define | LTC24XX_HS_MULTI_SPEED_2X 0x08 |
Mode Configuration for EasyDrive Family | |
| #define | LTC24XX_EZ_MULTI_VIN 0b10000000 |
| #define | LTC24XX_EZ_MULTI_PTAT 0b11000000 |
| #define | LTC24XX_EZ_MULTI_R50 0b10010000 |
| #define | LTC24XX_EZ_MULTI_R55 0b10000000 |
| #define | LTC24XX_EZ_MULTI_R60 0b10100000 |
| #define | LTC24XX_EZ_MULTI_SLOW 0b10000000 |
| #define | LTC24XX_EZ_MULTI_FAST 0b10001000 |
Single-Ended Channel Configuration | |
Channel selection for all multi-channel, differential input ADCs, even those that only require 8 bits of configuration (no further options.) Most devices in this category require a second byte of configuration for speed mode, temperature sensor selection, etc., but for the sake of simplicity a single function will be used to read all devices, sending zeros in the second configuration byte if only the channel is specified. Applicable devices: Easy Drive: LTC2486, LTC2487, LTC2488, LTC2489, LTC2492, LTC2493, LTC2494, LTC2495, LTC2496, LTC2497, LTC2498, LTC2499 First Generation Differential: LTC2414, LTC2418, LTC2439 High Speed: LTC2442, LTC2444, LTC2445, LTC2448, LTC2449 | |
| #define | LTC24XX_MULTI_CH_CH0 0xB0 |
| #define | LTC24XX_MULTI_CH_CH1 0xB8 |
| #define | LTC24XX_MULTI_CH_CH2 0xB1 |
| #define | LTC24XX_MULTI_CH_CH3 0xB9 |
| #define | LTC24XX_MULTI_CH_CH4 0xB2 |
| #define | LTC24XX_MULTI_CH_CH5 0xBA |
| #define | LTC24XX_MULTI_CH_CH6 0xB3 |
| #define | LTC24XX_MULTI_CH_CH7 0xBB |
| #define | LTC24XX_MULTI_CH_CH8 0xB4 |
| #define | LTC24XX_MULTI_CH_CH9 0xBC |
| #define | LTC24XX_MULTI_CH_CH10 0xB5 |
| #define | LTC24XX_MULTI_CH_CH11 0xBD |
| #define | LTC24XX_MULTI_CH_CH12 0xB6 |
| #define | LTC24XX_MULTI_CH_CH13 0xBE |
| #define | LTC24XX_MULTI_CH_CH14 0xB7 |
| #define | LTC24XX_MULTI_CH_CH15 0xBF |
Differential Channel Configuration | |
See note for single-ended configuration above. | |
| #define | LTC24XX_MULTI_CH_P0_N1 0xA0 |
| #define | LTC24XX_MULTI_CH_P1_N0 0xA8 |
| #define | LTC24XX_MULTI_CH_P2_N3 0xA1 |
| #define | LTC24XX_MULTI_CH_P3_N2 0xA9 |
| #define | LTC24XX_MULTI_CH_P4_N5 0xA2 |
| #define | LTC24XX_MULTI_CH_P5_N4 0xAA |
| #define | LTC24XX_MULTI_CH_P6_N7 0xA3 |
| #define | LTC24XX_MULTI_CH_P7_N6 0xAB |
| #define | LTC24XX_MULTI_CH_P8_N9 0xA4 |
| #define | LTC24XX_MULTI_CH_P9_N8 0xAC |
| #define | LTC24XX_MULTI_CH_P10_N11 0xA5 |
| #define | LTC24XX_MULTI_CH_P11_N10 0xAD |
| #define | LTC24XX_MULTI_CH_P12_N13 0xA6 |
| #define | LTC24XX_MULTI_CH_P13_N12 0xAE |
| #define | LTC24XX_MULTI_CH_P14_N15 0xA7 |
| #define | LTC24XX_MULTI_CH_P15_N14 0xAF |
Oversample Ratio (OSR) Commands | |
| #define | LTC24XX_MULTI_CH_OSR_64 0x10 |
| #define | LTC24XX_MULTI_CH_OSR_128 0x20 |
| #define | LTC24XX_MULTI_CH_OSR_256 0x30 |
| #define | LTC24XX_MULTI_CH_OSR_512 0x40 |
| #define | LTC24XX_MULTI_CH_OSR_1024 0x50 |
| #define | LTC24XX_MULTI_CH_OSR_2048 0x60 |
| #define | LTC24XX_MULTI_CH_OSR_4096 0x70 |
| #define | LTC24XX_MULTI_CH_OSR_8192 0x80 |
| #define | LTC24XX_MULTI_CH_OSR_16384 0x90 |
| #define | LTC24XX_MULTI_CH_OSR_32768 0xF0 |
| void LTC24XX_calibrate_voltage | ( | int32_t | zero_code, |
| int32_t | fs_code, | ||
| float | zero_voltage, | ||
| float | fs_voltage, | ||
| float * | LTC24XX_lsb, | ||
| int32_t * | LTC24XX_offset_code | ||
| ) |
Calculate the lsb weight and offset code given a full-scale code and a measured zero-code.
| zero_code | Measured code with the inputs shorted to ground |
| fs_code | Measured code at nearly full-scale |
| zero_voltage | Measured zero voltage |
| fs_voltage | Voltage measured at input (with voltmeter) when fs_code was read from ADC |
| LTC24XX_lsb | Overwritten with lsb weight (in volts) |
| LTC24XX_offset_code | Overwritten with offset code (zero code) |
Definition at line 427 of file LTC24XX_general.cpp.
| float LTC24XX_diff_code_to_calibrated_voltage | ( | int32_t | adc_code, |
| float | LTC24XX_lsb, | ||
| int32_t | LTC24XX_offset_code | ||
| ) |
Calculates the voltage corresponding to an ADC code, given lsb weight (in volts) and the calibrated ADC offset code (zero code that is subtracted from adc_code).
Applies to differential input, SPI interface parts.
| adc_code | Code read from ADC |
| LTC24XX_lsb | LSB weight (in volts) |
| LTC24XX_offset_code | The calibrated offset code (This is the ADC code zero code that will be subtracted from adc_code) |
Definition at line 409 of file LTC24XX_general.cpp.
| float LTC24XX_diff_code_to_voltage | ( | int32_t | adc_code, |
| float | vref | ||
| ) |
Calculates the voltage corresponding to an ADC code, given the reference voltage.
Applies to differential input parts (LTC2410 type input)
| adc_code | Code read from ADC |
| vref | Reference voltage |
Definition at line 389 of file LTC24XX_general.cpp.
| int8_t LTC24XX_EOC_timeout | ( | uint8_t | cs, |
| uint16_t | miso_timeout | ||
| ) |
Checks for EOC with a specified timeout.
Applies to all SPI interface delta sigma ADCs that have SINC4 rejection, does NOT apply to LTC2450/60/70 family.
| cs | Chip Select pin |
| miso_timeout | Timeout (in milliseconds) |
Definition at line 82 of file LTC24XX_general.cpp.
| int8_t LTC24XX_I2C_16bit_command_24bit_data | ( | uint8_t | i2c_address, |
| uint8_t | adc_command_high, | ||
| uint8_t | adc_command_low, | ||
| int32_t * | adc_code, | ||
| uint16_t | eoc_timeout | ||
| ) |
Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result.
| i2c_address | I2C address of device |
| adc_command_high | First command byte written to LTC24XX |
| adc_command_low | Second command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
| eoc_timeout | Timeout (in milliseconds) |
| int8_t LTC24XX_I2C_16bit_command_32bit_data | ( | uint8_t | i2c_address, |
| uint8_t | adc_command_high, | ||
| uint8_t | adc_command_low, | ||
| int32_t * | adc_code, | ||
| uint16_t | eoc_timeout | ||
| ) |
Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result.
| i2c_address | I2C address of device |
| adc_command_high | First command byte written to LTC24XX |
| adc_command_low | Second command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
| eoc_timeout | Timeout (in milliseconds) |
Definition at line 350 of file LTC24XX_general.cpp.
| int8_t LTC24XX_I2C_24bit_data | ( | uint8_t | i2c_address, |
| int32_t * | adc_code, | ||
| uint16_t | eoc_timeout | ||
| ) |
Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result.
Applies to: LTC2483 (only this lonely one!)
| i2c_address | I2C address of device |
| adc_code | 4 byte conversion code read from LTC24XX |
| eoc_timeout | Timeout (in milliseconds) |
| int8_t LTC24XX_I2C_32bit_data | ( | uint8_t | i2c_address, |
| int32_t * | adc_code, | ||
| uint16_t | eoc_timeout | ||
| ) |
Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result.
Data is formatted to match the SPI devices, with the MSB in the bit 28 position.
| i2c_address | I2C address of device |
| adc_code | 4 byte conversion code read from LTC24XX |
| eoc_timeout | Timeout (in milliseconds) |
Definition at line 298 of file LTC24XX_general.cpp.
| int8_t LTC24XX_I2C_8bit_command_24bit_data | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| int32_t * | adc_code, | ||
| uint16_t | eoc_timeout | ||
| ) |
Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result.
Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result.
| i2c_address | I2C address of device |
| adc_command | 1 byte command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
| eoc_timeout | Timeout (in milliseconds) |
Definition at line 268 of file LTC24XX_general.cpp.
| int8_t LTC24XX_I2C_8bit_command_32bit_data | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| int32_t * | adc_code, | ||
| uint16_t | eoc_timeout | ||
| ) |
Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result.
| i2c_address | I2C address of device |
| adc_command | 1 byte command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
| eoc_timeout | Timeout (in milliseconds) |
Definition at line 326 of file LTC24XX_general.cpp.
| float LTC24XX_SE_code_to_voltage | ( | int32_t | adc_code, |
| float | vref | ||
| ) |
Calculates the voltage corresponding to an ADC code, given the reference voltage.
Applies to Single-Ended input parts (LTC2400-type input)
| adc_code | Code read from ADC |
| vref | Reference voltage |
Definition at line 375 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_16bit_command_24bit_data | ( | uint8_t | cs, |
| uint8_t | adc_command_high, | ||
| uint8_t | adc_command_low, | ||
| int32_t * | adc_code | ||
| ) |
Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result.
Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result.
| cs | Chip Select pin |
| adc_command_high | First command byte written to LTC24XX |
| adc_command_low | Second command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
Definition at line 216 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_16bit_command_32bit_data | ( | uint8_t | cs, |
| uint8_t | adc_command_high, | ||
| uint8_t | adc_command_low, | ||
| int32_t * | adc_code | ||
| ) |
Reads from LTC24XX ADC that accepts a 16 bit configuration and returns a 32 bit result.
| cs | Chip Select pin |
| adc_command_high | First command byte written to LTC24XX |
| adc_command_low | Second command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
Definition at line 136 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_24bit_data | ( | uint8_t | cs, |
| int32_t * | adc_code | ||
| ) |
Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result.
| cs | Chip Select pin |
| adc_code | 4 byte conversion code read from LTC24XX |
Definition at line 176 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_2ch_ping_pong_24bit_data | ( | uint8_t | cs, |
| uint8_t * | adc_channel, | ||
| int32_t * | code | ||
| ) |
Reads from LTC24XX two channel "Ping-Pong" ADC, placing the channel information in the adc_channel parameter and returning the 32 bit result with the channel bit cleared so the data format matches the rest of the family.
Reads from LTC24XX two channel "Ping-Pong" ADC, placing the channel information in the adc_channel parameter and returning the 32 bit result with the channel bit cleared so the data format matches the rest of the family.
| cs | Chip Select pin |
| adc_channel | Returns channel number read. |
| code | 4 byte conversion code read from LTC24XX |
Definition at line 239 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_2ch_ping_pong_32bit_data | ( | uint8_t | cs, |
| uint8_t * | adc_channel, | ||
| int32_t * | code | ||
| ) |
Reads from LTC24XX two channel "Ping-Pong" ADC, placing the channel information in the adc_channel parameter and returning the 32 bit result with the channel bit cleared so the data format matches the rest of the family.
| cs | Chip Select pin |
| adc_channel | Returns channel number read. |
| code | 4 byte conversion code read from LTC24XX |
Definition at line 155 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_32bit_data | ( | uint8_t | cs, |
| int32_t * | adc_code | ||
| ) |
Reads from LTC24XX ADC that has no configuration word and returns a 32 bit result.
| cs | Chip Select pin |
| adc_code | 4 byte conversion code read from LTC24XX |
Definition at line 103 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_8bit_command_16bit_data | ( | uint8_t | cs, |
| uint8_t | adc_command, | ||
| int32_t * | adc_code | ||
| ) |
Reads from LTC24XX ADC that accepts a 8 bit configuration and returns a 16 bit result.
| cs | Chip Select pin |
| adc_command | First command byte written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
| void LTC24XX_SPI_8bit_command_24bit_data | ( | uint8_t | cs, |
| uint8_t | adc_command, | ||
| int32_t * | adc_code | ||
| ) |
Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result.
Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result.
| cs | Chip Select pin |
| adc_command | 1 byte command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
Definition at line 195 of file LTC24XX_general.cpp.
| void LTC24XX_SPI_8bit_command_32bit_data | ( | uint8_t | cs, |
| uint8_t | adc_command, | ||
| int32_t * | adc_code | ||
| ) |
Reads from LTC24XX ADC that accepts an 8 bit configuration and returns a 32 bit result.
| cs | Chip Select pin |
| adc_command | 1 byte command written to LTC24XX |
| adc_code | 4 byte conversion code read from LTC24XX |
Definition at line 118 of file LTC24XX_general.cpp.
| #define LTC24XX_CS QUIKEVAL_CS |
Define the SPI CS pin.
Definition at line 125 of file LTC24XX_general.h.
| #define LTC24XX_EZ_MULTI_FAST 0b10001000 |
Definition at line 158 of file LTC24XX_general.h.
| #define LTC24XX_EZ_MULTI_PTAT 0b11000000 |
Definition at line 149 of file LTC24XX_general.h.
| #define LTC24XX_EZ_MULTI_R50 0b10010000 |
Definition at line 152 of file LTC24XX_general.h.
| #define LTC24XX_EZ_MULTI_R55 0b10000000 |
Definition at line 153 of file LTC24XX_general.h.
| #define LTC24XX_EZ_MULTI_R60 0b10100000 |
Definition at line 154 of file LTC24XX_general.h.
| #define LTC24XX_EZ_MULTI_SLOW 0b10000000 |
Definition at line 157 of file LTC24XX_general.h.
| #define LTC24XX_EZ_MULTI_VIN 0b10000000 |
Definition at line 148 of file LTC24XX_general.h.
| #define LTC24XX_HS_MULTI_KEEP_PREVIOUS_MODE 0x80 |
Definition at line 136 of file LTC24XX_general.h.
| #define LTC24XX_HS_MULTI_KEEP_PREVIOUS_SPEED_RESOLUTION 0x00 |
Definition at line 137 of file LTC24XX_general.h.
| #define LTC24XX_HS_MULTI_SPEED_1X 0x00 |
Definition at line 138 of file LTC24XX_general.h.
| #define LTC24XX_HS_MULTI_SPEED_2X 0x08 |
Definition at line 139 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH0 0xB0 |
Definition at line 182 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH1 0xB8 |
Definition at line 183 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH10 0xB5 |
Definition at line 192 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH11 0xBD |
Definition at line 193 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH12 0xB6 |
Definition at line 194 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH13 0xBE |
Definition at line 195 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH14 0xB7 |
Definition at line 196 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH15 0xBF |
Definition at line 197 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH2 0xB1 |
Definition at line 184 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH3 0xB9 |
Definition at line 185 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH4 0xB2 |
Definition at line 186 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH5 0xBA |
Definition at line 187 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH6 0xB3 |
Definition at line 188 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH7 0xBB |
Definition at line 189 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH8 0xB4 |
Definition at line 190 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_CH9 0xBC |
Definition at line 191 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_1024 0x50 |
Definition at line 246 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_128 0x20 |
Definition at line 243 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_16384 0x90 |
Definition at line 250 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_2048 0x60 |
Definition at line 247 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_256 0x30 |
Definition at line 244 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_32768 0xF0 |
Definition at line 251 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_4096 0x70 |
Definition at line 248 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_512 0x40 |
Definition at line 245 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_64 0x10 |
Definition at line 242 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_OSR_8192 0x80 |
Definition at line 249 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P0_N1 0xA0 |
Definition at line 206 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P10_N11 0xA5 |
Definition at line 221 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P11_N10 0xAD |
Definition at line 222 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P12_N13 0xA6 |
Definition at line 224 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P13_N12 0xAE |
Definition at line 225 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P14_N15 0xA7 |
Definition at line 227 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P15_N14 0xAF |
Definition at line 228 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P1_N0 0xA8 |
Definition at line 207 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P2_N3 0xA1 |
Definition at line 209 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P3_N2 0xA9 |
Definition at line 210 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P4_N5 0xA2 |
Definition at line 212 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P5_N4 0xAA |
Definition at line 213 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P6_N7 0xA3 |
Definition at line 215 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P7_N6 0xAB |
Definition at line 216 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P8_N9 0xA4 |
Definition at line 218 of file LTC24XX_general.h.
| #define LTC24XX_MULTI_CH_P9_N8 0xAC |
Definition at line 219 of file LTC24XX_general.h.