![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC2499: 24-Bit, 16-Channel Delta Sigma ADCs with Easy Drive Input Current Cancellation. More...
Library for LTC2499: 24-Bit, 16-Channel Delta Sigma ADCs with Easy Drive Input Current Cancellation.
Definition in file LTC2499.cpp.
Go to the source code of this file.
Functions | |
| uint8_t | LTC2499_read (uint8_t i2c_address, uint8_t adc_command_high, uint8_t adc_command_low, int32_t *adc_code, uint16_t timeout) |
| Reads from LTC2499. More... | |
| float | LTC2499_code_to_voltage (int32_t adc_code, float vref) |
| Calculates the voltage corresponding to an adc code, given the reference (in volts) More... | |
| float LTC2499_code_to_voltage | ( | int32_t | adc_code, |
| float | vref | ||
| ) |
Calculates the voltage corresponding to an adc code, given the reference (in volts)
| adc_code | Code read from adc |
| vref | VRef (in volts) |
Definition at line 87 of file LTC2499.cpp.
| uint8_t LTC2499_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command_high, | ||
| uint8_t | adc_command_low, | ||
| int32_t * | adc_code, | ||
| uint16_t | timeout | ||
| ) |
Reads from LTC2499.
| i2c_address | I2C address (7-bit format) for part |
| adc_command_high | High byte command written to LTC2499 |
| adc_command_low | Low byte command written to LTC2499 |
| adc_code | 4 byte conversion code read from LTC2499 |
| timeout | Timeout in ms |
Definition at line 80 of file LTC2499.cpp.