![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC2473: 16-Bit, Delta Sigma ADC with I2C interface. More...
Library for LTC2473: 16-Bit, Delta Sigma ADC with I2C interface.
Definition in file LTC2473.cpp.
Go to the source code of this file.
Functions | |
| uint8_t | LTC2473_read (uint8_t i2c_address, int32_t *adc_code, uint16_t timeout) |
| Reads from LTC2473. More... | |
| uint8_t | LTC2473_write (uint8_t i2c_address, uint8_t adc_command) |
| Writes to the LTC2473. More... | |
| float | LTC2473_code_to_voltage (int32_t adc_code, float vref) |
| Calculates the voltage corresponding to an ADC code, given the reference (in volts) More... | |
| float LTC2473_code_to_voltage | ( | int32_t | adc_code, |
| float | vref | ||
| ) |
Calculates the voltage corresponding to an ADC code, given the reference (in volts)
| adc_code | Code read from adc |
| vref | VRef (in volts) |
Definition at line 94 of file LTC2473.cpp.
| uint8_t LTC2473_read | ( | uint8_t | i2c_address, |
| int32_t * | adc_code, | ||
| uint16_t | timeout | ||
| ) |
Reads from LTC2473.
| i2c_address | I2C address (7-bit format) for part |
| adc_code | 2 byte conversion code read from LTC2473 |
| timeout | The timeout in (microseconds) |
Definition at line 77 of file LTC2473.cpp.
| uint8_t LTC2473_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command | ||
| ) |
Writes to the LTC2473.
| i2c_address | I2C address (7-bit format) for part |
| adc_command | Command byte written to LTC2473 |
Definition at line 85 of file LTC2473.cpp.