![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC2461: 16-Bit I2C Delta Sigma ADCs with 10ppm/C Max Precision Reference. More...
Library for LTC2461: 16-Bit I2C Delta Sigma ADCs with 10ppm/C Max Precision Reference.
Definition in file LTC2461.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTC2461_read (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads the ADC and returns 16-bit data. More... | |
| int8_t | LTC2461_command (uint8_t i2c_address, uint8_t adc_command) |
| Write a 16-bit command to the ADC. More... | |
| float | LTC2461_code_to_voltage (uint16_t adc_code, float LTC2461_lsb, int32_t LTC2461_offset_code) |
| Calculates the LTC2309 input unipolar voltage. More... | |
| void | LTC2461_cal_voltage (uint16_t zero_code, uint16_t fs_code, float zero_voltage, float fs_voltage, float *LTC2461_lsb, int32_t *LTC2461_offset_code) |
| Calibrate the lsb. More... | |
| void LTC2461_cal_voltage | ( | uint16_t | zero_code, |
| uint16_t | fs_code, | ||
| float | zero_voltage, | ||
| float | fs_voltage, | ||
| float * | LTC2461_lsb, | ||
| int32_t * | LTC2461_offset_code | ||
| ) |
Calibrate the lsb.
| zero_code | Code from zero reading |
| fs_code | Full-scale code |
| zero_voltage | Measured zero voltage |
| fs_voltage | Measured full-scale voltage |
| LTC2461_lsb | Return LSB value (volts) |
| LTC2461_offset_code | Return Offset code |
Definition at line 111 of file LTC2461.cpp.
| float LTC2461_code_to_voltage | ( | uint16_t | adc_code, |
| float | LTC2461_lsb, | ||
| int32_t | LTC2461_offset_code | ||
| ) |
Calculates the LTC2309 input unipolar voltage.
| adc_code | Raw ADC code |
| LTC2461_lsb | LSB value (volts) |
| LTC2461_offset_code | Offset code |
Definition at line 103 of file LTC2461.cpp.
| int8_t LTC2461_command | ( | uint8_t | i2c_address, |
| uint8_t | adc_command | ||
| ) |
Write a 16-bit command to the ADC.
Derived from 2655.
| i2c_address | I2C address of the LTC2461. |
| adc_command | ADC command to be written to the LTC2461. |
Definition at line 93 of file LTC2461.cpp.
| int8_t LTC2461_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads the ADC and returns 16-bit data.
| i2c_address | I2C address of the LTC2461. |
| adc_command | ADC command to be written to the LTC2461. |
| adc_code | Returns code read from ADC. |
Definition at line 82 of file LTC2461.cpp.