![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Functions | |
| static void | read_LTC2449 (float vref, uint16_t eoc_timeout, uint16_t channel_delay) |
| Reads the LTC2449 and displays the results. More... | |
| static void | print_all (float *results) |
| Displays the the data in the array. More... | |
| static void | print_prompt () |
| Print the Prompt. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Macros | |
| #define | CS QUIKEVAL_CS |
| LTC2449: 24-Bit High Speed 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution. More... | |
Variables | |
| const uint8_t | SINGLE_ENDED_CONFIG_ARRAY [16] |
| Lookup table to build the command for single-ended mode. More... | |
| const uint8_t | DIFF_CONFIG_ARRAY [16] |
| Lookup table to build the command for differential mode. More... | |
| const uint8_t | OSR_CONFIG_ARRAY [10] |
| Lookup table to build the OSR command. More... | |
|
static |
Repeats Linduino loop.
Definition at line 121 of file LTC2449_Datalogger.ino.
|
static |
Displays the the data in the array.
Definition at line 191 of file LTC2449_Datalogger.ino.
|
static |
Print the Prompt.
Definition at line 159 of file LTC2449_Datalogger.ino.
|
static |
Reads the LTC2449 and displays the results.
Definition at line 170 of file LTC2449_Datalogger.ino.
|
static |
Initialize Linduino.
Definition at line 98 of file LTC2449_Datalogger.ino.
| #define CS QUIKEVAL_CS |
LTC2449: 24-Bit High Speed 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution.
The LTC2449 is a 16-channel (8-differential) high speed 24-bit No Latency Delta Sigma ADCs. They use a proprietary delta-sigma architecture enabling variable speed/resolution. Through a simple 4-wire serial interface, ten speed/resolution combinations 6.9Hz/280nVRMS to 3.5kHz/25uVRMS (4kHz with external oscillator) can be selected with no latency between conversion results or shift in DC accuracy (offset, full-scale, linearity, drift). Additionally, a 2X speed mode can be selected enabling output rates up to 7kHz (8kHz if an external oscillator is used) with one cycle latency.
http://www.linear.com/product/LTC2449
http://www.linear.com/product/LTC2449#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.The chip select
Definition at line 66 of file LTC2449_Datalogger.ino.
| const uint8_t DIFF_CONFIG_ARRAY[16] |
Lookup table to build the command for differential mode.
Build the command for differential mode
Definition at line 78 of file LTC2449_Datalogger.ino.
| const uint8_t OSR_CONFIG_ARRAY[10] |
Lookup table to build the OSR command.
Build the command for different OSR modes
Definition at line 86 of file LTC2449_Datalogger.ino.
| const uint8_t SINGLE_ENDED_CONFIG_ARRAY[16] |
Lookup table to build the command for single-ended mode.
Builds the command for single-ended mode
Definition at line 71 of file LTC2449_Datalogger.ino.