![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2418: 16-Channel 24-Bit No Latency Delta-Sigma ADC. More...
LTC2418: 16-Channel 24-Bit No Latency Delta-Sigma ADC.
The LTC2414/LTC2418 are 8-/16-channel (4-/8-differential) micropower 24-bit
delta-sigma analog-to-digital converters. They operate from 2.7V to 5.5V and
include an integrated oscillator, 2ppm INL and 0.2ppm RMS noise. They use
delta-sigma technology and provide single cycle settling time for multiplexed
applications. Through a single pin, the LTC2414/LTC2418 can be configured for
better than 110dB differential mode rejection at 50Hz or 60Hz +/-2%, or they can
be driven by an external oscillator for a user-defined rejection frequency. The
internal oscillator requires no external frequency setting components.
SPI DATA FORMAT (MSB First):
Byte #1 Byte #2 Byte #3 Byte #4
Data Out : !EOC DMY SIG D22 D21 D20 D19 D18 D17 D16 D15 D14 D13 D12 D11 D10 D9 D8 D7 D6 D5 D4 D3 D2 D1 D0 SGL OS S2 S1 S0 PAR
Data In : 1 0 EN SGL OS S2 S1 S0 X X X X X X X X X X X X X X X X X X X X X X X X
!EOC : End of Conversion Bit (Active Low)
DMY : Dummy Bit (Always 0)
SIG : Sign Bit (1-data positive, 0-data negative)
Dx : Data Bits
EN : Enable Bit (0-keep previous mode, 1-change mode)
SGL : Enable Single-Ended Bit (0-differential, 1-single-ended)
OS : ODD/Sign Bit
Sx : Address Select Bit
PAR : Parity Bit
Command Byte
1 0 EN SGL OS S2 S1 S0 Comments
1 0 0 X X X X X Keep Previous Mode
1 0 1 0 X X X X Differential Mode
1 0 1 1 X X X X Single-Ended Mode
Example Code:
Read Channel 0 in Single-Ended mode
uint16_t miso_timeout = 1000;
adc_command = LTC2418_CH0; // Build ADC command for channel 0
if(LTC2418_EOC_timeout(LTC2418_CS, miso_timeout)) // Check for EOC
return(1);
LTC2418_read(LTC2418_CS, adc_command, &adc_code); // Throws out last reading
if(LTC2418_EOC_timeout(LTC2418_CS, miso_timeout)) // Check for EOC
return(1);
LTC2418_read(LTC2418_CS, adc_command, &adc_code); // Obtains the current reading and stores to adc_code variable
// Convert adc_code to voltage
adc_voltage = LTC2418_code_to_voltage(adc_code, LTC2418_lsb , LTC2418_offset_code);http://www.linear.com/product/LTC2418
http://www.linear.com/product/LTC2418#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2418: 16-Channel 24-Bit No Latency Delta-Sigma ADC
Definition in file LTC2418.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2418_EOC_timeout (uint8_t cs, uint16_t miso_timeout) |
| Checks for EOC with a specified timeout. More... | |
| void | LTC2418_read (uint8_t cs, uint8_t adc_command, uint32_t *adc_code) |
| Reads the LTC2418 result and programs the configuration for the next conversion. More... | |
| float | LTC2418_code_to_voltage (int32_t adc_code, float LTC2418_lsb, int32_t LTC2418_offset_code) |
| Calculates the LTC2418 input bipolar voltage. More... | |
| void | LTC2418_cal_voltage (int32_t zero_code, int32_t fs_code, float zero_voltage, float fs_voltage, float *LTC2418_lsb, int32_t *LTC2418_offset_code) |
| Calibrate the lsb. More... | |
Macros | |
| #define | LTC2418_CS QUIKEVAL_CS |
| Define the SPI CS pin. More... | |
LTC2418 Single-Ended configuration bytes | |
Address bytes with enable sequence prepended | |
| #define | LTC2418_CH0 0xB0 |
| #define | LTC2418_CH1 0xB8 |
| #define | LTC2418_CH2 0xB1 |
| #define | LTC2418_CH3 0xB9 |
| #define | LTC2418_CH4 0xB2 |
| #define | LTC2418_CH5 0xBA |
| #define | LTC2418_CH6 0xB3 |
| #define | LTC2418_CH7 0xBB |
| #define | LTC2418_CH8 0xB4 |
| #define | LTC2418_CH9 0xBC |
| #define | LTC2418_CH10 0xB5 |
| #define | LTC2418_CH11 0xBD |
| #define | LTC2418_CH12 0xB6 |
| #define | LTC2418_CH13 0xBE |
| #define | LTC2418_CH14 0xB7 |
| #define | LTC2418_CH15 0xBF |
LTC2418 Differential configuration bytes | |
Address bytes with enable sequence prepended | |
| #define | LTC2418_P0_N1 0xA0 |
| #define | LTC2418_P1_N0 0xA8 |
| #define | LTC2418_P2_N3 0xA1 |
| #define | LTC2418_P3_N2 0xA9 |
| #define | LTC2418_P4_N5 0xA2 |
| #define | LTC2418_P5_N4 0xAA |
| #define | LTC2418_P6_N7 0xA3 |
| #define | LTC2418_P7_N6 0xAB |
| #define | LTC2418_P8_N9 0xA4 |
| #define | LTC2418_P9_N8 0xAC |
| #define | LTC2418_P10_N11 0xA5 |
| #define | LTC2418_P11_N10 0xAD |
| #define | LTC2418_P12_N13 0xA6 |
| #define | LTC2418_P13_N12 0xAE |
| #define | LTC2418_P14_N15 0xA7 |
| #define | LTC2418_P15_N14 0xAF |
| void LTC2418_cal_voltage | ( | int32_t | zero_code, |
| int32_t | fs_code, | ||
| float | zero_voltage, | ||
| float | fs_voltage, | ||
| float * | LTC2418_lsb, | ||
| int32_t * | LTC2418_offset_code | ||
| ) |
Calibrate the lsb.
| zero_code | Offset (Code) |
| fs_code | Code measured with full-scale input applied |
| zero_voltage | Measured zero voltage |
| fs_voltage | Measured full-scale voltage |
| LTC2418_lsb | Returns LSB value (volts) |
| LTC2418_offset_code | Returns Offset (Code) |
Definition at line 117 of file LTC2418.cpp.
| float LTC2418_code_to_voltage | ( | int32_t | adc_code, |
| float | LTC2418_lsb, | ||
| int32_t | LTC2418_offset_code | ||
| ) |
Calculates the LTC2418 input bipolar voltage.
| adc_code | Raw ADC code |
| LTC2418_lsb | LSB value (volts) |
| LTC2418_offset_code | Offset (Code) |
Definition at line 107 of file LTC2418.cpp.
| int8_t LTC2418_EOC_timeout | ( | uint8_t | cs, |
| uint16_t | miso_timeout | ||
| ) |
Checks for EOC with a specified timeout.
| cs | Chip Select pin |
| miso_timeout | Timeout (ms) |
Definition at line 73 of file LTC2418.cpp.
| void LTC2418_read | ( | uint8_t | cs, |
| uint8_t | adc_command, | ||
| uint32_t * | adc_code | ||
| ) |
Reads the LTC2418 result and programs the configuration for the next conversion.
| cs | Chip Select pin |
| adc_command | Command byte |
| adc_code | Returns raw 32-bit code read from ADC |
Definition at line 92 of file LTC2418.cpp.
| #define LTC2418_CS QUIKEVAL_CS |