![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2326-16: 16-Bit, 250ksps Pseudo-differential input ADC. More...
LTC2326-16: 16-Bit, 250ksps Pseudo-differential input ADC.
LTC2326-18: 18-Bit, 250ksps Pseudo-differential input ADC. LTC2327-16: 16-Bit, 500ksps Pseudo-differential input ADC LTC2327-18: 18-Bit, 500ksps Pseudo-differential input ADC LTC2328-16: 16-Bit, 1Msps Pseudo-differential input ADC LTC2328-18: 18-Bit, 1Msps Pseudo-differential input ADC LTC2336-18: 18-Bit, 250ksps Fully-differential input ADC LTC2337-18: 18-Bit, 500ksps Fully-differential ADC LTC2338-18: 18-Bit, 1Msps Fully-differential input ADC
The following parts (DUT) are pin-compatible, 16/18-bit A/D converters with serial I/O, and an internal reference:
LTC2326-16: 16-Bit, 250ksps Pseudo-differential input ADC.
LTC2326-18: 18-Bit, 250ksps Pseudo-differential input ADC.
LTC2327-16: 16-Bit, 500ksps Pseudo-differential input ADC
LTC2327-18: 18-Bit, 500ksps Pseudo-differential input ADC
LTC2328-16: 16-Bit, 1Msps Pseudo-differential input ADC
LTC2328-18: 18-Bit, 1Msps Pseudo-differential input ADC
LTC2336-18: 18-Bit, 250ksps Fully-differential input ADC
LTC2337-18: 18-Bit, 500ksps Fully-differential ADC
LTC2338-18: 18-Bit, 1Msps Fully-differential input ADC
Example Code:
Read ADC input.
LTC2338_read(LTC2338_CS, &adc_code); // Throws out last reading
LTC2338_read(LTC2338_CS, &adc_code); // Obtains the current reading and stores to adc_code variable
// Convert adc_code to voltage
adc_voltage = LTC2338_code_to_voltage(adc_code, vref);http://www.linear.com/product/LTC2326-16 http://www.linear.com/product/LTC2326-18 http://www.linear.com/product/LTC2327-16 http://www.linear.com/product/LTC2327-18 http://www.linear.com/product/LTC2328-16 http://www.linear.com/product/LTC2328-18 http://www.linear.com/product/LTC2336-18 http://www.linear.com/product/LTC2337-18 http://www.linear.com/product/LTC2338-18
http://www.linear.com/product/LTC2326-16#demoboards http://www.linear.com/product/LTC2326-18#demoboards http://www.linear.com/product/LTC2327-16#demoboards http://www.linear.com/product/LTC2327-18#demoboards http://www.linear.com/product/LTC2328-16#demoboards http://www.linear.com/product/LTC2328-18#demoboards http://www.linear.com/product/LTC2336-18#demoboards http://www.linear.com/product/LTC2337-18#demoboards http://www.linear.com/product/LTC2338-18#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2338: 16/18-bit 1Msps ADC
Definition in file LTC2338.h.
Go to the source code of this file.
Functions | |
| void | LTC2338_read (uint8_t cs, int32_t *ptr_adc_code) |
| Reads the LTC2338 and returns 32-bit data in 2's complement format. More... | |
| float | LTC2338_code_to_voltage (int32_t adc_code, float vref) |
| Calculates the LTC2338 input voltage given the binary data and lsb weight. More... | |
Macros | |
| #define | LTC2338_CS QUIKEVAL_CS |
| Define the SPI CS pin. More... | |
LTC2338 Channel Address | |
| #define | LTC2338_ADDRESS 0x00 |
| float LTC2338_code_to_voltage | ( | int32_t | adc_code, |
| float | vref | ||
| ) |
Calculates the LTC2338 input voltage given the binary data and lsb weight.
| adc_code | Raw ADC code |
| vref | Reference voltage |
Definition at line 123 of file LTC2338.cpp.
| void LTC2338_read | ( | uint8_t | cs, |
| int32_t * | ptr_adc_code | ||
| ) |
Reads the LTC2338 and returns 32-bit data in 2's complement format.
| cs | Chip Select Pin |
| ptr_adc_code | Returns code read from ADC (from previous conversion) |
Definition at line 101 of file LTC2338.cpp.
| #define LTC2338_CS QUIKEVAL_CS |