![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2305: 8-channel, 12-Bit SAR ADC with I2C interface. More...
LTC2305: 8-channel, 12-Bit SAR ADC with I2C interface.
The LTC2305 is a low noise, low power, 8-channel, 12-bit successive
approximation ADC with an I2C compatible serial interface. This ADC includes an
internal reference and a fully differential sample-and-hold circuit to reduce
common mode noise. The LTC2305 operates from an internal clock to achieve a fast
1.3 microsecond conversion time.
The LTC2305 operates from a single 5V supply and draws just 300 microamps at a
throughput rate of 1ksps. The ADC enters nap mode when not converting, reducing
the power dissipation.
I2C DATA FORMAT (MSB First):
Byte #1 Byte #2
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK SD OS S1 S0 UNI SLP X X SACK
Byte #3 Byte #4 Byte #5
Repeat Start SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK D11 D10 D9 D8 D7 D6 D5 D4 MACK D3 D2 D1 D0 X X X X MNACK STOP
SACK : Slave Acknowledge
MACK : Master Acknowledge
MNACK : Master Not Acknowledge
SD : Single, Differential# Bit
OS : ODD, Sign# Bit
Sx : Address Select Bit
COM : CH7/COM Configuration Bit
UNI : Unipolar, Bipolar# Bit
SLP : Sleep Mode Bit
Dx : Data Bits
X : Don't care
Example Code:
Read Channel 0 in Single-Ended Unipolar mode
adc_command = LTC2305_CH0 | LTC2305_UNIPOLAR_MODE; // Build ADC command for channel 0
ack |= LTC2305_read(LTC2305_I2C_ADDRESS, adc_command, &adc_code); // Throws out last reading
ack |= LTC2305_read(LTC2305_I2C_ADDRESS, adc_command, &adc_code); // Obtains the current reading and stores to adc_code variable
// Convert adc_code to voltage
adc_voltage = LTC2305_unipolar_code_to_voltage(adc_code, LTC2305_lsb, LTC2305_offset_code);http://www.linear.com/product/LTC2305
http://www.linear.com/product/LTC2305#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2305: 8-channel, 12-Bit SAR ADC with I2C interface
Definition in file LTC2305.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2305_read (uint8_t i2c_address, uint8_t adc_command, uint16_t *ptr_adc_code) |
| Reads 12-bit code from LTC2305, programs channel and mode for next conversion. More... | |
| float | LTC2305_code_to_voltage (uint16_t adc_code, float LTC2305_vref, uint8_t uni_bipolar) |
| Calculates the LTC2305 input voltage. More... | |
Macros | |
I2C addresses | |
Un-comment the address corresponding to the LTC2305's address | |
| #define | LTC2305_I2C_ADDRESS 0x08 |
Single-Ended Channel Configuration | |
| #define | LTC2305_CH0 0xC0 |
| #define | LTC2305_CH1 0x80 |
LTC2305 Configuration Bits | |
| #define | LTC2305_SLEEP_MODE 0x04 |
| #define | LTC2305_EXIT_SLEEP_MODE 0x00 |
| #define | LTC2305_UNIPOLAR_MODE 0x08 |
| #define | LTC2305_BIPOLAR_MODE 0x00 |
| #define | LTC2305_SINGLE_ENDED_MODE 0x80 |
| #define | LTC2305_DIFFERENTIAL_MODE 0x00 |
| #define | LTC2305_P0_N1 0x00 |
| #define | LTC2305_P1_N0 0x40 |
| #define | LTC2301 1 |
| #define | LTC2305 0 |
| float LTC2305_code_to_voltage | ( | uint16_t | adc_code, |
| float | LTC2305_vref, | ||
| uint8_t | uni_bipolar | ||
| ) |
Calculates the LTC2305 input voltage.
| adc_code | Code read from ADC |
| LTC2305_vref | LSB value (volts) |
Definition at line 103 of file LTC2305.cpp.
| int8_t LTC2305_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | ptr_adc_code | ||
| ) |
Reads 12-bit code from LTC2305, programs channel and mode for next conversion.
| i2c_address | I2C address of device |
| adc_command | ADC command / address bits |
| ptr_adc_code | Returns code read from ADC |
Definition at line 86 of file LTC2305.cpp.