![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LT3965 - Octal Matrix LED Bypass Switch. More...
LT3965 - Octal Matrix LED Bypass Switch.
The LT3965 is an LED bypass switching device for dimming indiviadual LEDs in a
string using a common current source. It features eight individually controlled
floating source N-channel MOSFET switches rated for 17V/330 mΩ. The eight
switches can be connected in parallel and/or in series to bypass current around
one or more LEDs in a string. The LT3965 as a slave uses the I2C serial interface
to communicate with the master. Each of eight channels can be independently
programmed to bypass the LED string in constant on, constant off, dimming without
fade transition or dimming with fade transition mode.
WRITE PROTOCOLS (MSB FIRST):
Byte #1 Byte #2 Byte #3
ACMODE WRITE 0 1 0 A4 A3 A2 A1 0(W) B7 B6 B5 B4 B3 B2 B1 B0
SCMODE WRITE SHORT 1 0 1 A4 A3 A2 A1 0(W) 0 C3 C2 C1 B3 B2 B1 B0
SCMODE WRITE LONG 1 0 1 A4 A3 A2 A1 0(W) 1 C3 C2 C1 B11 B10 B9 B8 B7 B6 B5 B4 B3 B2 B1 B0
BCMODE WRITE 0 0 0 1 1 0 0 0(W)
W : I2C Write (0)
R : I2C Read (1)
Ax : Device Address
Bx : Data Bits
Cx : Channel Addresshttp://www.linear.com/product/LT3965
http://www.linear.com/product/LT3965#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LT3965: Octal Matrix LED Bypass Switch
Definition in file LT3965.h.
Go to the source code of this file.
Functions | |
| int8_t | i2c_acwrite (uint8_t address, uint8_t value) |
| ACMODE Write Command to write a "value" byte to device at "address". More... | |
| int8_t | i2c_acread (uint8_t address, uint8_t *values) |
| ACMODE Read Command to read 3 data bytes from device at "address". More... | |
| int8_t | i2c_scwriteshort (uint8_t address, uint8_t channel, uint8_t data_SCMREG) |
| SCMODE Write Command Short Format to write a "value" byte to device at "address". More... | |
| int8_t | i2c_scwritelong (uint8_t address, uint8_t channel, uint8_t data_SCMREG, uint8_t dimming_value) |
| SCMODE Write Command Long Format to write 2 "value" bytes to device at "address". More... | |
| int8_t | i2c_scwriteshort_scread (uint8_t address, uint8_t channel, uint8_t data_SCMREG, uint8_t *values) |
| SCMODE Write Short + SCMODE Read Command. More... | |
| int8_t | i2c_bcread (uint8_t *value) |
| BCMODE Read Command. More... | |
Macros | |
| #define | UP 1 |
| #define | DOWN 0 |
| #define | TRUE 1 |
| #define | FALSE 0 |
| #define | ALERTPIN 2 |
| #define | PWMPIN 7 |
| #define | LOADPIN 9 |
| #define | BUTTONPIN 12 |
| #define | REDLED 11 |
LT3965 I2C 7-BIT DEVICE ADDRESS | |
| #define | address1 0b00000000 |
| #define | address2 0b00001111 |
| #define | AC_ADDR_0 0x20 |
| #define | SC_ADDR_0 0x50 |
| #define | BC_ADDR 0x0C |
| #define | TM_ADDR 0x73 |
8 CHANNELS | |
| #define | CHANNEL0 0X00 |
| #define | CHANNEL1 0X01 |
| #define | CHANNEL2 0X02 |
| #define | CHANNEL3 0X03 |
| #define | CHANNEL4 0X04 |
| #define | CHANNEL5 0X05 |
| #define | CHANNEL6 0X06 |
| #define | CHANNEL7 0X07 |
| int8_t i2c_acread | ( | uint8_t | address, |
| uint8_t * | values | ||
| ) |
ACMODE Read Command to read 3 data bytes from device at "address".
Definition at line 83 of file LT3965.cpp.
| int8_t i2c_acwrite | ( | uint8_t | address, |
| uint8_t | value | ||
| ) |
ACMODE Write Command to write a "value" byte to device at "address".
Definition at line 73 of file LT3965.cpp.
| int8_t i2c_bcread | ( | uint8_t * | value | ) |
BCMODE Read Command.
Definition at line 135 of file LT3965.cpp.
| int8_t i2c_scwritelong | ( | uint8_t | address, |
| uint8_t | channel, | ||
| uint8_t | data_SCMREG, | ||
| uint8_t | dimming_value | ||
| ) |
SCMODE Write Command Long Format to write 2 "value" bytes to device at "address".
Definition at line 107 of file LT3965.cpp.
| int8_t i2c_scwriteshort | ( | uint8_t | address, |
| uint8_t | channel, | ||
| uint8_t | data_SCMREG | ||
| ) |
SCMODE Write Command Short Format to write a "value" byte to device at "address".
Definition at line 93 of file LT3965.cpp.
| int8_t i2c_scwriteshort_scread | ( | uint8_t | address, |
| uint8_t | channel, | ||
| uint8_t | data_SCMREG, | ||
| uint8_t * | values | ||
| ) |
SCMODE Write Short + SCMODE Read Command.
Definition at line 121 of file LT3965.cpp.