![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC726B-A (or DC726A-A) Demonstration Board. More...
Linear Technology DC726B-A (or DC726A-A) Demonstration Board.
LTC6903: 1kHz to 68MHz Serial Port Programmable Oscillator
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a precision voltage source and a precision voltmeter (to monitor voltage source). No external power supply is required. Ensure JP1 is installed in the default position from the factory. Demo Board Configuration: To properly use this program with the DC72B-A (or the DC726A-A) demo board, JMP 2 needs to be set to QuikEval. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC6903
http://www.linear.com/product/LTC6903#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC726B_A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | settings () |
| Configures the output. More... | |
| static void | set_frequency () |
| Sets the output frequency. More... | |
| static void | manually_set_reg () |
| Manually Sets OCT and DAC Code. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | output_config = LTC6903_CLK_ON_CLK_INV_ON |
| Keeps track of output configuration. More... | |
|
static |
Repeats Linduino loop.
Definition at line 103 of file DC726B_A.ino.
|
static |
Manually Sets OCT and DAC Code.
Definition at line 176 of file DC726B_A.ino.
|
static |
Prints main menu.
Definition at line 145 of file DC726B_A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 130 of file DC726B_A.ino.
|
static |
Sets the output frequency.
Definition at line 156 of file DC726B_A.ino.
|
static |
Configures the output.
Definition at line 202 of file DC726B_A.ino.
|
static |
Initialize Linduino.
Definition at line 93 of file DC726B_A.ino.
|
static |
Keeps track of output configuration.
Definition at line 90 of file DC726B_A.ino.