![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Analog Devices DC2515 Demonstration Board. More...
Analog Devices DC2515 Demonstration Board.
LTC6810: 6-Channel Battery Stack Monitors
*NOTES * Setup: * Set the terminal baud rate to 115200 and select the newline terminator. * Ensure all jumpers on the demo board are installed in their default positions from the factory. * Refer to Demo Manual. * *USER INPUT DATA FORMAT: * decimal : 1024 * hex : 0x400 * octal : 02000 (leading 0) * binary : B10000000000 * float : 1024.0 *
https://www.analog.com/en/products/ltc6810-1.html
Copyright 2019(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC2515.ino.
Go to the source code of this file.
Functions | |
| static void | measurement_loop (uint8_t datalog_en) |
More... | |
| static void | print_menu (void) |
More... | |
| static void | print_wrconfig (void) |
More... | |
| static void | print_rxconfig (void) |
More... | |
| static void | print_cells (uint8_t datalog_en) |
More... | |
| static void | print_aux (uint8_t datalog_en) |
More... | |
| static void | print_stat (void) |
More... | |
| static void | print_sumofcells (void) |
More... | |
| static void | print_svolt (uint8_t datalog_en) |
More... | |
| static void | check_mux_fail (void) |
More... | |
| static void | print_selftest_errors (uint8_t adc_reg,int8_t error) |
More... | |
| static void | print_digital_redundancy_errors (uint8_t adc_reg,int8_t error) |
More... | |
| static void | print_open_wires (void) |
More... | |
| static void | print_pec_error_count (void) |
More... | |
| static int8_t | select_s_pin (void) |
More... | |
| static void | print_wrpwm (void) |
More... | |
| static void | print_rxpwm (void) |
More... | |
| static void | print_wrcomm (void) |
/prints data which is written on COMM register onto the serial port More... | |
| static void | print_rxcomm (void) |
More... | |
| static void | print_sid (void) |
More... | |
| static void | reverse_isospi_direction (void) |
More... | |
| static void | check_mute_bit (void) |
More... | |
| static void | print_conv_time (uint32_t conv_time) |
More... | |
| static void | check_error (int error) |
More... | |
| static void | serial_print_text (char data[]) |
More... | |
| static void | serial_print_hex (uint8_t data) |
More... | |
| char | read_hex (void) |
More... | |
| char | get_char (void) |
More... | |
| static void | setup () |
More... | |
| static void | loop () |
More... | |
| static void | run_command (uint32_t cmd) |
More... | |
Macros | |
| #define | ENABLED 1 |
| #define | DISABLED 0 |
| #define | DATALOG_ENABLED 1 |
| #define | DATALOG_DISABLED 0 |
Variables | |
| const uint8_t | TOTAL_IC = 2 |
| Number of ICs in the daisy chain. More... | |
| const uint8_t | ADC_OPT = ADC_OPT_DISABLED |
| ADC Mode option bit. More... | |
| const uint8_t | ADC_CONVERSION_MODE = MD_7KHZ_3KHZ |
| ADC Mode. More... | |
| const uint8_t | ADC_DCP = DCP_DISABLED |
| Discharge Permitted. More... | |
| const uint8_t | CELL_CH_TO_CONVERT = CELL_CH_ALL |
| Channel Selection for ADC conversion. More... | |
| const uint8_t | AUX_CH_TO_CONVERT = AUX_CH_ALL |
| Channel Selection for ADC conversion. More... | |
| const uint8_t | STAT_CH_TO_CONVERT = STAT_CH_ALL |
| Channel Selection for ADC conversion. More... | |
| const uint8_t | SEL_ALL_REG = REG_ALL |
| Register Selection. More... | |
| const uint8_t | SEL_REG_A = REG_1 |
| Register Selection. More... | |
| const uint8_t | SEL_REG_B = REG_2 |
| Register Selection. More... | |
| const uint16_t | OV_THRESHOLD = 41000 |
| Over voltage threshold ADC Code. More... | |
| const uint16_t | UV_THRESHOLD = 30000 |
| Under voltage threshold ADC Code. More... | |
| const uint16_t | MEASUREMENT_LOOP_TIME = 500 |
| Loop Time in milliseconds(ms) More... | |
| const uint8_t | WRITE_CONFIG = DISABLED |
| This is to ENABLED or DISABLED writing into to configuration registers in a continuous loop. More... | |
| const uint8_t | READ_CONFIG = DISABLED |
| This is to ENABLED or DISABLED reading the configuration registers in a continuous loop. More... | |
| const uint8_t | MEASURE_CELL = ENABLED |
| This is to ENABLED or DISABLED measuring the cell voltages in a continuous loop. More... | |
| const uint8_t | MEASURE_AUX = DISABLED |
| This is to ENABLED or DISABLED reading the auxiliary registers in a continuous loop. More... | |
| const uint8_t | MEASURE_STAT = DISABLED |
| This is to ENABLED or DISABLED reading the status registers in a continuous loop. More... | |
| const uint8_t | PRINT_PEC = DISABLED |
| This is to ENABLED or DISABLED printing the PEC Error Count in a continuous loop. More... | |
| cell_asic | BMS_IC [TOTAL_IC] |
| Global Battery Variable. More... | |
| bool | ISOSPI_DIR =BMS_IC[0].isospi_reverse |
| bool | ADCOPT = false |
| ADC Mode option bit. More... | |
| bool | REFON = true |
| Reference Powered Up Bit. More... | |
| bool | GPIOBITS [4] = {false,true,true,true} |
| GPIO Pin Control // Gpio 1,2,3,4. More... | |
| static uint16_t | UV =UV_THRESHOLD |
| Under voltage Comparison Voltage. More... | |
| static uint16_t | OV =OV_THRESHOLD |
| Over voltage Comparison Voltage. More... | |
| bool | DCCBITS [6] = {false,false,false,false,false,false} |
| Discharge cell switch //Dcc 1,2,3,4,5,6. More... | |
| bool | DCCBIT_0 = false |
| Discharge cell switch //Dcc 0 // For discharging optional 7th cell. More... | |
| bool | MCAL = false |
| Enable Multi-Calibration. More... | |
| bool | EN_DTMEN = true |
| Enable Discharge timer monitor. More... | |
| bool | DIS_RED = false |
| Disable Digital Redundancy Check. More... | |
| bool | FDRF = false |
| Force digital Redundancy Failure. More... | |
| bool | SCONV = true |
| Enable Cell Measurement Redundancy using S Pin. More... | |
| bool | DCTOBITS [4] = {true,false,true,false} |
| Discharge Time Out Value //Dcto 0,1,2,3 // Programed for 4 min. More... | |
| char | hex_digits [16] |
More... | |
| char | hex_to_byte_buffer [5] |
More... | |
| char | byte_to_hex_buffer [3] |
More... | |
|
static |
Function to check error flag and print PEC error message
Definition at line 1233 of file DC2515.ino.
|
static |
Function to check the Mute bit in the Status Register
Definition at line 1206 of file DC2515.ino.
|
static |
Function to check the MUX fail bit in the Status Register
Definition at line 943 of file DC2515.ino.
| char get_char | ( | void | ) |
|
static |
|
static |
For writing/reading configuration data or measuring cell voltages or reading aux register or reading status register in a continuous loop
Definition at line 628 of file DC2515.ino.
|
static |
Prints GPIO voltage codes and Vref2 voltage code onto the serial port
Definition at line 812 of file DC2515.ino.
|
static |
|
static |
|
static |
Prints Errors Detected during Digital Redundancy test
Definition at line 983 of file DC2515.ino.
|
static |
|
static |
Prints Open wire test results to the serial port
Definition at line 1002 of file DC2515.ino.
|
static |
|
static |
Prints received data from COMM register onto the serial port
Definition at line 1137 of file DC2515.ino.
|
static |
Prints the configuration data that was read back from the LTC6810 to the serial port.
Definition at line 753 of file DC2515.ino.
|
static |
Prints the PWM configuration data that was read back from the LTC6810 to the serial port.
Definition at line 1085 of file DC2515.ino.
|
static |
|
static |
|
static |
Prints Status voltage codes and Vref2 voltage code onto the serial port
Definition at line 853 of file DC2515.ino.
|
static |
Prints Status voltage codes for SOC onto the serial port
Definition at line 888 of file DC2515.ino.
|
static |
|
static |
/prints data which is written on COMM register onto the serial port
Definition at line 1109 of file DC2515.ino.
|
static |
Prints the configuration data that is going to be written to the LTC6810 to the serial port.
Definition at line 725 of file DC2515.ino.
|
static |
Prints PWM the configuration data that is going to be written to the LTC6810 to the serial port.
Definition at line 1057 of file DC2515.ino.
| char read_hex | ( | void | ) |
Read 2 hex characters from the serial buffer and convert them to a byte
Definition at line 1293 of file DC2515.ino.
|
static |
Function to reverse the direction of ISOSPI communication when the ICs are connected in daisy chain
Definition at line 1191 of file DC2515.ino.
|
static |
|
static |
|
static |
|
static |
|
static |
| #define DATALOG_DISABLED 0 |
Definition at line 84 of file DC2515.ino.
| #define DATALOG_ENABLED 1 |
Definition at line 83 of file DC2515.ino.
| #define DISABLED 0 |
Definition at line 82 of file DC2515.ino.
| #define ENABLED 1 |
Definition at line 81 of file DC2515.ino.
| const uint8_t ADC_CONVERSION_MODE = MD_7KHZ_3KHZ |
ADC Mode.
Definition at line 124 of file DC2515.ino.
| const uint8_t ADC_DCP = DCP_DISABLED |
Discharge Permitted.
Definition at line 125 of file DC2515.ino.
| const uint8_t ADC_OPT = ADC_OPT_DISABLED |
ADC Mode option bit.
Definition at line 123 of file DC2515.ino.
| bool ADCOPT = false |
ADC Mode option bit.
Definition at line 163 of file DC2515.ino.
| const uint8_t AUX_CH_TO_CONVERT = AUX_CH_ALL |
Channel Selection for ADC conversion.
Definition at line 127 of file DC2515.ino.
Global Battery Variable.
Definition at line 156 of file DC2515.ino.
| char byte_to_hex_buffer[3] |
Buffer for ASCII hex to byte conversion
Definition at line 1284 of file DC2515.ino.
| const uint8_t CELL_CH_TO_CONVERT = CELL_CH_ALL |
Channel Selection for ADC conversion.
Definition at line 126 of file DC2515.ino.
| bool DCCBIT_0 = false |
Discharge cell switch //Dcc 0 // For discharging optional 7th cell.
Definition at line 169 of file DC2515.ino.
| bool DCCBITS[6] = {false,false,false,false,false,false} |
Discharge cell switch //Dcc 1,2,3,4,5,6.
Definition at line 168 of file DC2515.ino.
| bool DCTOBITS[4] = {true,false,true,false} |
Discharge Time Out Value //Dcto 0,1,2,3 // Programed for 4 min.
Definition at line 175 of file DC2515.ino.
| bool DIS_RED = false |
Disable Digital Redundancy Check.
Definition at line 172 of file DC2515.ino.
| bool EN_DTMEN = true |
Enable Discharge timer monitor.
Definition at line 171 of file DC2515.ino.
| bool FDRF = false |
Force digital Redundancy Failure.
Definition at line 173 of file DC2515.ino.
| bool GPIOBITS[4] = {false,true,true,true} |
GPIO Pin Control // Gpio 1,2,3,4.
Definition at line 165 of file DC2515.ino.
| char hex_digits[16] |
Hex conversion constants
Definition at line 1268 of file DC2515.ino.
| char hex_to_byte_buffer[5] |
Global Variables
Definition at line 1276 of file DC2515.ino.
| bool ISOSPI_DIR =BMS_IC[0].isospi_reverse |
Definition at line 158 of file DC2515.ino.
| bool MCAL = false |
Enable Multi-Calibration.
Definition at line 170 of file DC2515.ino.
| const uint8_t MEASURE_AUX = DISABLED |
This is to ENABLED or DISABLED reading the auxiliary registers in a continuous loop.
Definition at line 143 of file DC2515.ino.
| const uint8_t MEASURE_CELL = ENABLED |
This is to ENABLED or DISABLED measuring the cell voltages in a continuous loop.
Definition at line 142 of file DC2515.ino.
| const uint8_t MEASURE_STAT = DISABLED |
This is to ENABLED or DISABLED reading the status registers in a continuous loop.
Definition at line 144 of file DC2515.ino.
| const uint16_t MEASUREMENT_LOOP_TIME = 500 |
Loop Time in milliseconds(ms)
Definition at line 137 of file DC2515.ino.
|
static |
Over voltage Comparison Voltage.
Definition at line 167 of file DC2515.ino.
| const uint16_t OV_THRESHOLD = 41000 |
| const uint8_t PRINT_PEC = DISABLED |
This is to ENABLED or DISABLED printing the PEC Error Count in a continuous loop.
Definition at line 145 of file DC2515.ino.
| const uint8_t READ_CONFIG = DISABLED |
This is to ENABLED or DISABLED reading the configuration registers in a continuous loop.
Definition at line 141 of file DC2515.ino.
| bool REFON = true |
Reference Powered Up Bit.
Definition at line 164 of file DC2515.ino.
| bool SCONV = true |
Enable Cell Measurement Redundancy using S Pin.
Definition at line 174 of file DC2515.ino.
| const uint8_t SEL_ALL_REG = REG_ALL |
Register Selection.
Definition at line 129 of file DC2515.ino.
| const uint8_t SEL_REG_A = REG_1 |
Register Selection.
Definition at line 130 of file DC2515.ino.
| const uint8_t SEL_REG_B = REG_2 |
Register Selection.
Definition at line 131 of file DC2515.ino.
| const uint8_t STAT_CH_TO_CONVERT = STAT_CH_ALL |
Channel Selection for ADC conversion.
Definition at line 128 of file DC2515.ino.
| const uint8_t TOTAL_IC = 2 |
Number of ICs in the daisy chain.
Definition at line 120 of file DC2515.ino.
|
static |
Under voltage Comparison Voltage.
Definition at line 166 of file DC2515.ino.
| const uint16_t UV_THRESHOLD = 30000 |
| const uint8_t WRITE_CONFIG = DISABLED |
This is to ENABLED or DISABLED writing into to configuration registers in a continuous loop.
Definition at line 140 of file DC2515.ino.