![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC2405A Demonstration Board. More...
Linear Technology DC2405A Demonstration Board.
LTM2893-1: 100MHz ADC SPI Isolator LTC2328-18: 18-Bit, 1Msps Pseudo-differential input ADC Max SCK rate is 100MHz.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a voltage source (preferably low-noise) and a precision voltmeter. Ensure all jumpers on the demo board are installed in their default positions from the factory. Refer to Demo Manual DC2405A. How to test: The voltage source should be connected between inputs AIN and GND2. Ensure both inputs are within their specified absolute input voltage range. Ensure the voltage source is set within the range of -10.24V to +10.24V (single ended voltage range). (Swapping input voltages results in a reversed polarity reading.) USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTM2893
http://www.linear.com/product/LTM2893#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC2405A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| static void | menu_1_read_input () |
| Read channel. More... | |
| static void | menu_2_select_bits () |
| Select number of bits. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | LTC2328_bits = 18 |
| Default set for 18 bits. More... | |
| static float | LTC2328_vref = 10.24 |
|
static |
Repeats Linduino loop.
Definition at line 117 of file DC2405A.ino.
|
static |
|
static |
|
static |
Prints main menu.
Definition at line 243 of file DC2405A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 226 of file DC2405A.ino.
|
static |
|
static |
Initialize Linduino.
Definition at line 99 of file DC2405A.ino.
|
static |
Default set for 18 bits.
Definition at line 94 of file DC2405A.ino.
|
static |
Definition at line 95 of file DC2405A.ino.