![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2380-24: Low Noise, High Speed, 24-Bit SAR ADC With Digital Filter. More...
LTC2380-24: Low Noise, High Speed, 24-Bit SAR ADC With Digital Filter.
http://www.linear.com/product/LTC2380-24
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC2289AA.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | menu_1_read_input () |
| Read Input voltage. More... | |
| static void | menu_2_select_gain_compression () |
| Select gain compression. More... | |
| static void | configureCNV () |
| Function to configure CNV pin as an output. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Macros | |
| #define | LTC2380_CNV QUIKEVAL_CS |
Variables | |
| static uint8_t | LTC2380_dgc = 0 |
| Default set for no gain compression. More... | |
| static float | LTC2380_vref = 10 |
| static float | voltage |
|
static |
Function to configure CNV pin as an output.
Definition at line 188 of file DC2289AA.ino.
|
static |
Repeats Linduino loop.
Definition at line 87 of file DC2289AA.ino.
|
static |
|
static |
|
static |
Prints main menu.
Definition at line 164 of file DC2289AA.ino.
|
static |
Prints the title block when program first starts.
Definition at line 173 of file DC2289AA.ino.
|
static |
Initialize Linduino.
Definition at line 74 of file DC2289AA.ino.
| #define LTC2380_CNV QUIKEVAL_CS |
Definition at line 58 of file DC2289AA.ino.
|
static |
Default set for no gain compression.
Definition at line 69 of file DC2289AA.ino.
|
static |
Definition at line 70 of file DC2289AA.ino.
|
static |
Definition at line 71 of file DC2289AA.ino.