![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC2222AB Demonstration Board. More...
Linear Technology DC2222AB Demonstration Board.
LTC2508: 32-Bit Over-Sampling ADC with Configurable Digital Filter
NOTES This code is used in the case where DRDY triggers a hardware interrupt on Linduino, and then the data is read. This makes data acquisition faster. Set the terminal baud rate to 115200 and select the newline terminator. Provide an external voltage supply of +/-9V or 10 V. Drive MCLK with an external CLK source. Connect DRDY to INT1 pin. Connect QUIKEVAL_GPIO pin to the SYNC pin. 16 bits of configuration data: 1 0 0 0 0 0 0 0 0 SEL0 SEL1 0 0 0 0 0 In the Linduino code, data is continuously captured in the interrupt service routine and printed out to the serial console as hex values. Converting the data to voltage can be done later. The serially printed out data is logged into a file using TeraTerm. The data is read out, converted to voltage and plotted using a Python script. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2508
http://www.linear.com/product/LTC2508#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC2222_interrupt_driven_read.ino.
Go to the source code of this file.
Functions | |
| static void | sneaker_port_init () |
| Send configuration data through sneaker port. More... | |
| static void | initialise_i2c_data (uint16_t value, uint8_t i2c_data[48]) |
| static void | setup () |
| static void | loop () |
| static void | read_data_ISR () |
Variables | |
| static float | VREF = 5.0 |
| static uint16_t | global_config_data = CONFIG_DF_256 |
| const byte | interruptPin = 0 |
|
static |
Definition at line 188 of file DC2222_interrupt_driven_read.ino.
|
static |
Definition at line 107 of file DC2222_interrupt_driven_read.ino.
|
static |
Definition at line 112 of file DC2222_interrupt_driven_read.ino.
|
static |
Definition at line 97 of file DC2222_interrupt_driven_read.ino.
|
static |
Send configuration data through sneaker port.
Send a SYNC pulse after configuration.
Definition at line 158 of file DC2222_interrupt_driven_read.ino.
|
static |
Definition at line 88 of file DC2222_interrupt_driven_read.ino.
| const byte interruptPin = 0 |
Definition at line 94 of file DC2222_interrupt_driven_read.ino.
|
static |
Definition at line 87 of file DC2222_interrupt_driven_read.ino.