![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC4316: Single/Dual I2C SMBUS ADDRESS REMAPPER. More...
Library for LTC4316: Single/Dual I2C SMBUS ADDRESS REMAPPER.
Definition in file DC2217A.ino.
Go to the source code of this file.
Functions | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino Loop. More... | |
| static void | print_title () |
| Print the title block. More... | |
| static void | print_prompt () |
| Print the main menu prompt. More... | |
| static void | menu_1_scan_addresses () |
| Scan I2C Bus for addresses. More... | |
| static uint8_t | menu_2_DAC () |
| DAC Control Menu. More... | |
Variables | |
| static int8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| const char | ack_error [] = "Error: No Acknowledge. Check I2C Address." |
| Error message. More... | |
| const int | LTC4316_OFFSET = 0x78 |
| Demoboard offset. More... | |
| const int | LTC2631_GLOBAL_ADDRESS = 0x73 |
| Global address of LTC2631 DAC. More... | |
| const int | LTC2631_JP_ADDRESS_1 = 0x12 |
| Jumper Setting 1 on Demoboard. More... | |
| const int | LTC2631_JP_ADDRESS_2 = 0x11 |
| Jumper Setting 2 on Demoboard. More... | |
| const int | LTC2631_JP_ADDRESS_3 = 0x10 |
| Jumper Setting 3 on Demoboard. More... | |
| const int | EEPROM_ADDRESS = 0x50 |
| EEPROM Address on Demoboard. More... | |
|
static |
Repeats Linduino Loop.
Definition at line 123 of file DC2217A.ino.
|
static |
Scan I2C Bus for addresses.
Definition at line 184 of file DC2217A.ino.
|
static |
DAC Control Menu.
Definition at line 252 of file DC2217A.ino.
|
static |
Print the main menu prompt.
Definition at line 175 of file DC2217A.ino.
|
static |
Print the title block.
Definition at line 161 of file DC2217A.ino.
|
static |
Initialize Linduino.
Definition at line 103 of file DC2217A.ino.
| const char ack_error[] = "Error: No Acknowledge. Check I2C Address." |
Error message.
Definition at line 93 of file DC2217A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 91 of file DC2217A.ino.
| const int EEPROM_ADDRESS = 0x50 |
EEPROM Address on Demoboard.
Definition at line 100 of file DC2217A.ino.
| const int LTC2631_GLOBAL_ADDRESS = 0x73 |
Global address of LTC2631 DAC.
Definition at line 96 of file DC2217A.ino.
| const int LTC2631_JP_ADDRESS_1 = 0x12 |
Jumper Setting 1 on Demoboard.
Definition at line 97 of file DC2217A.ino.
| const int LTC2631_JP_ADDRESS_2 = 0x11 |
Jumper Setting 2 on Demoboard.
Definition at line 98 of file DC2217A.ino.
| const int LTC2631_JP_ADDRESS_3 = 0x10 |
Jumper Setting 3 on Demoboard.
Definition at line 99 of file DC2217A.ino.
| const int LTC4316_OFFSET = 0x78 |
Demoboard offset.
Change to correct value if EXT offset if chosen.
Definition at line 95 of file DC2217A.ino.