![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
DC1954A LTC6954: Low Phase Noise, Triple Output Clock Distribution Divider/Driver. More...
DC1954A LTC6954: Low Phase Noise, Triple Output Clock Distribution Divider/Driver.
Setup:
Set the terminal baud rate to 115200 and select the newline terminator.
Refer to Demo Manual DC1954A.
Ensure all jumpers are installed in the factory default positions.
One 3.3V power supplies ia needed for this demo board
An input signal is also needed for this demo board, refer to the
DC1954 Demo Manual for details.
Command Description:
*****Main Menu*****
1- Load Default Settings- Loads the SPI map that is identical to file
LTC6954.6954set that is supplied with the LTC6954_GUI and mentioned
in the DC1954A user's manual.
2- READ/WRITE to Registers Addresses- Selecting this option will cause all the registers to
be read, stored to variables, and displayed. The user will then have the option
to write to one register address at a time.
3- READ/WRITE to Registers Fields- Selecting this option will allow the user
to read or write to one register field name at a time.
4- This function stores the current SPI settings in the demo boards EEPROM
5- This function loads SPI settings from the demo boards EEPROM to the device
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0http://www.linear.com/product/LTC6954
http://www.linear.com/product/LTC6954#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1954A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | menu_1_load_default_settings () |
| Menu 1: Load Default SPI Register Settings This function identifies which of the 4 LTC6954 frequency versions are connected. More... | |
| static void | menu_2_RW_to_reg_addresss () |
| Menu 2: Reads and/or Writes the SPI register address This function reads and displays all SPI register address settings in HEX format. More... | |
| static void | menu_3_RW_to_reg_field () |
| Menu 3: Reads and/or Writes individual SPI fields This function provides the user with a list of all SPI fields. More... | |
| static void | menu_4_store_settings () |
| Store PLL settings to nonvolatile EEPROM on demo board. More... | |
| static void | menu_5_restore_settings () |
| Read stored PLL settings from nonvolatile EEPROM on demo board. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| long | field_menu_RW (long field_val, char field_name[], uint8_t f) |
| Support function for function menu_3_RW_to_reg_field displays current state of select field provides user the option to write to that field or return to menu. More... | |
Variables | |
| static uint8_t | ref_out = 0 |
| Used to keep track of reference out status. More... | |
| static int8_t | demo_board_connected |
| Demo Board Name stored in QuikEval EEPROM. More... | |
| static uint8_t | First_Run =0 |
| if first time through loop = 0, otherwise=1 More... | |
| long field_menu_RW | ( | long | field_val, |
| char | field_name[], | ||
| uint8_t | f | ||
| ) |
Support function for function menu_3_RW_to_reg_field displays current state of select field provides user the option to write to that field or return to menu.
| field_val | current state of the selected field |
| field_name | SPI Field name selected |
| f | SPI field identifier identifies selected fields information in SPI MAP arrays |
Definition at line 289 of file DC1954A.ino.
|
static |
|
static |
Menu 1: Load Default SPI Register Settings This function identifies which of the 4 LTC6954 frequency versions are connected.
Based on the version connected, this function loads the register settings referenced in the DC1954A demo manual's quick start section. The register settings loaded are the same as the LTC6954_GUI 6954set files LTC6954.6954set. The setting loaded with this function assume the DC1954A's loop filter has not been modified.
Definition at line 199 of file DC1954A.ino.
|
static |
Menu 2: Reads and/or Writes the SPI register address This function reads and displays all SPI register address settings in HEX format.
It then provides an option to modify(write to) individual registers one at time
EXAMPLE:
Definition at line 235 of file DC1954A.ino.
|
static |
Menu 3: Reads and/or Writes individual SPI fields This function provides the user with a list of all SPI fields.
The user can select a SPI field to read its current value. Then the user will be provided with an option to write to that field or return to the selection menu.
EXAMPLE:
Definition at line 349 of file DC1954A.ino.
|
static |
Store PLL settings to nonvolatile EEPROM on demo board.
Definition at line 603 of file DC1954A.ino.
|
static |
Read stored PLL settings from nonvolatile EEPROM on demo board.
Definition at line 629 of file DC1954A.ino.
|
static |
Prints main menu.
Definition at line 683 of file DC1954A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 665 of file DC1954A.ino.
|
static |
|
static |
Demo Board Name stored in QuikEval EEPROM.
Definition at line 109 of file DC1954A.ino.
|
static |
if first time through loop = 0, otherwise=1
Definition at line 110 of file DC1954A.ino.
|
static |
Used to keep track of reference out status.
Definition at line 108 of file DC1954A.ino.