![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1880A Demonstration Board. More...
Linear Technology DC1880A Demonstration Board.
SETUP: Set the terminal baud rate to 115200 and select the newline terminator. External power supply is required. USER INPUT DATA FORMAT: decimal : 14 hex : 0x0E (Data), 0xE (Reg)
http://www.linear.com/product/LTC2874
http://www.linear.com/product/LTC2874#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
IO-Link is a registered trademark of PROFIBUS User Organization (PNO).
Definition in file DC1880A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Print the title block. More... | |
| static void | print_prompt () |
| Print main menu and prompt user for an input command. More... | |
| static uint8_t | reg_test () |
| Test register number against valid range for Write. More... | |
| static void | print_warning_prompt () |
| Print warning prompt. More... | |
| static void | menu_1_cq (void) |
| Menu 1: Enable/Disable CQ output for specified port. More... | |
| static void | menu_2_lplus (void) |
| Menu 2: Enable/Disable L+ output for specified port. More... | |
| static void | menu_3_wakeup_cq (void) |
| Menu 3: Generate Wake-Up Request (WURQ) on CQ output. More... | |
| static void | menu_4_24v_mode (void) |
| Menu 4: Change value of 24VMODE bit. More... | |
| static void | menu_5_sio_mode (void) |
| Menu 5: Change SIO_MODE setting for specified port. More... | |
| static void | menu_6_set_illm (void) |
| Menu 6: Change ILLM setting for specified port. More... | |
| static void | menu_7_clear_event (void) |
| Menu 7: Clear all Event registers. More... | |
| static void | menu_8_update_all (void) |
| Menu 8: Update all registers. More... | |
| static void | menu_9_reset (void) |
| Menu 9: Reset LTC2874. More... | |
| static void | menu_10_read_register (void) |
| Menu 10: Read byte of data from a register. More... | |
| static void | menu_11_write_register (void) |
| Menu 11: Write byte of data to a register. More... | |
| static void | menu_12_read_bit (void) |
| Menu 12: Read one bit from a register. More... | |
| static void | menu_13_write_bit_set (void) |
| Menu 13: Set one bit in writable register. More... | |
| static void | menu_14_write_bit_clr (void) |
| Menu 14: Clear one bit in writable register. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| char | demo_name [] = "DC1880" |
| Demo Board Name stored in QuikEval EEPROM. More... | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
|
static |
Repeats Linduino loop.
Definition at line 138 of file DC1880A.ino.
|
static |
Menu 10: Read byte of data from a register.
Definition at line 471 of file DC1880A.ino.
|
static |
Menu 11: Write byte of data to a register.
Definition at line 495 of file DC1880A.ino.
|
static |
Menu 12: Read one bit from a register.
Definition at line 521 of file DC1880A.ino.
|
static |
Menu 13: Set one bit in writable register.
Definition at line 553 of file DC1880A.ino.
|
static |
Menu 14: Clear one bit in writable register.
Definition at line 580 of file DC1880A.ino.
|
static |
Menu 1: Enable/Disable CQ output for specified port.
Definition at line 223 of file DC1880A.ino.
|
static |
Menu 2: Enable/Disable L+ output for specified port.
Definition at line 273 of file DC1880A.ino.
|
static |
Menu 3: Generate Wake-Up Request (WURQ) on CQ output.
Definition at line 323 of file DC1880A.ino.
|
static |
Menu 4: Change value of 24VMODE bit.
Definition at line 344 of file DC1880A.ino.
|
static |
Menu 5: Change SIO_MODE setting for specified port.
Definition at line 364 of file DC1880A.ino.
|
static |
Menu 6: Change ILLM setting for specified port.
Definition at line 400 of file DC1880A.ino.
|
static |
Menu 7: Clear all Event registers.
Definition at line 440 of file DC1880A.ino.
|
static |
Menu 8: Update all registers.
Definition at line 451 of file DC1880A.ino.
|
static |
Menu 9: Reset LTC2874.
Definition at line 461 of file DC1880A.ino.
|
static |
Print main menu and prompt user for an input command.
Definition at line 624 of file DC1880A.ino.
|
static |
Print the title block.
Definition at line 607 of file DC1880A.ino.
|
static |
Print warning prompt.
Definition at line 691 of file DC1880A.ino.
|
static |
Test register number against valid range for Write.
Definition at line 651 of file DC1880A.ino.
|
static |
Initialize Linduino.
Definition at line 106 of file DC1880A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 101 of file DC1880A.ino.
| char demo_name[] = "DC1880" |
Demo Board Name stored in QuikEval EEPROM.
Definition at line 97 of file DC1880A.ino.