![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1796A Demonstration Board. More...
Linear Technology DC1796A Demonstration Board.
LTC2364-16: 16-Bit, 250Ksps ADC. LTC2364-18: 18-Bit, 250Ksps ADC. LTC2367-16: 16-Bit, 500Ksps ADC LTC2367-18: 18-Bit, 500Ksps ADC LTC2368-16: 16-Bit, 1Msps ADC LTC2368-18: 18-Bit, 1Msps ADC LTC2369-18: 18-Bit, 1.6Msps ADC LTC2370-16: 16-Bit, 2Msps ADC Max SCK rate is 100MHz.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a voltage source (preferably low-noise) and a precision voltmeter. Ensure all jumpers on the demo board are installed in their default positions from the factory. Refer to Demo Manual DC1796A. How to test: The voltage source should be connected to input AIN+/AIN-. Ensure the input is within its specified absolute input voltage range. (It is easiest to tie the voltage source negative terminal to COM.) Ensure the voltage source is set within the range of 0V to +4.096V. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2364-16 http://www.linear.com/product/LTC2364-18 http://www.linear.com/product/LTC2367-16 http://www.linear.com/product/LTC2367-18 http://www.linear.com/product/LTC2368-16 http://www.linear.com/product/LTC2368-18 http://www.linear.com/product/LTC2369-18 http://www.linear.com/product/LTC2370-16
http://www.linear.com/product/LTC2364-16#demoboards http://www.linear.com/product/LTC2364-18#demoboards http://www.linear.com/product/LTC2367-16#demoboards http://www.linear.com/product/LTC2367-18#demoboards http://www.linear.com/product/LTC2368-16#demoboards http://www.linear.com/product/LTC2368-18#demoboards http://www.linear.com/product/LTC2369-18#demoboards http://www.linear.com/product/LTC2370-16#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1796A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| static void | menu_1_read_input () |
| Read channel. More... | |
| static void | menu_2_select_bits () |
| Select number of bits. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | LTC2370_bits = 18 |
| Default set for 18 bits. More... | |
| static float | LTC2370_vref = 4.096 |
|
static |
Repeats Linduino loop.
Definition at line 132 of file DC1796A.ino.
|
static |
|
static |
|
static |
Prints main menu.
Definition at line 256 of file DC1796A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 232 of file DC1796A.ino.
|
static |
|
static |
Initialize Linduino.
Definition at line 119 of file DC1796A.ino.
|
static |
Default set for 18 bits.
Definition at line 114 of file DC1796A.ino.
|
static |
Definition at line 115 of file DC1796A.ino.