![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1410A-A Demonstration Board. More...
Linear Technology DC1410A-A Demonstration Board.
LTC2498: 24-Bit, 16-Channel Delta Sigma ADC with SPI interface
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a precision voltage source and a precision voltmeter. Additionally, an external power supply is required to provide a negative voltage for Amp V-. Set it to anywhere from -1V to -5V. Set Amp V+ to Vcc. Ensure the COM and REF- pins are connected to ground. The REF+ pin should be connected to +5V. How Measure a Load Cell: The LTC2498 allowas a wide common mode range of 0V to Vcc. The LT1678 OPAMP common mode range is V- + 1.5 to V+ - 0.8V. Ensure the load cell sensor meets the requirments of the ADC and amplifier. After, set the desired gain and read in differential mode. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2498
http://www.linear.com/product/LTC2498#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1410AA.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| static uint8_t | menu_1_read_differential () |
| Read channels in differential mode. More... | |
| static void | set_gain (uint8_t a_pin, uint8_t b_pin, uint8_t gain) |
| Set the Mux select pins to the desired gain. More... | |
| static void | init_gain_pins (uint8_t a_pin, uint8_t b_pin) |
| initialize the MUX select pins More... | |
| static void | menu_2_set_1X2X () |
| Set 1X or 2X mode. More... | |
| static void | menu_3_set_channel_gain () |
| Allows the user to sets the desired gain. More... | |
| static void | print_gain (uint8_t gain) |
| Utility function to display the gain. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Enumerations | |
| enum | Av { unity, g8, g16, g32, unity, g8, g16, g32 } |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static uint8_t | two_x_mode = LTC2498_SPEED_1X |
| The LTC2498 2X Mode settings. More... | |
| static uint8_t | rejection_mode = LTC2498_R50_R60 |
| The LTC2498 rejection mode settings. More... | |
| static float | LTC2498_vref = 5.0 |
| The LTC2498 ideal reference voltage. More... | |
| static uint16_t | eoc_timeout = 250 |
| Timeout in ms. More... | |
| static uint8_t | filt_flag = 1 |
| Keeps track when the filter needs to be rest. More... | |
| static uint8_t | channel_gain [6] = {g32, g32, g32, g32, g32, g32} |
| default is gain 32 More... | |
| const uint8_t | read_command_seq [] |
| Lookup table for reads. More... | |
| static uint8_t | read_gain_seq [] |
| lookup table for gain setting reads More... | |
| const uint8_t | A_PIN = 4 |
| Gain MUX pins. More... | |
| const uint8_t | B_PIN = 7 |
| const float | smoothing_const = .7 |
| Exponential filter smothing constant. More... | |
|
static |
initialize the MUX select pins
Definition at line 352 of file DC1410AA.ino.
|
static |
Repeats Linduino loop.
Definition at line 153 of file DC1410AA.ino.
|
static |
Read channels in differential mode.
Definition at line 212 of file DC1410AA.ino.
|
static |
Set 1X or 2X mode.
Definition at line 465 of file DC1410AA.ino.
|
static |
Allows the user to sets the desired gain.
Definition at line 361 of file DC1410AA.ino.
|
static |
Utility function to display the gain.
Definition at line 445 of file DC1410AA.ino.
|
static |
Prints main menu.
Definition at line 202 of file DC1410AA.ino.
|
static |
Prints the title block when program first starts.
Definition at line 187 of file DC1410AA.ino.
|
static |
|
static |
Set the Mux select pins to the desired gain.
Definition at line 345 of file DC1410AA.ino.
|
static |
Initialize Linduino.
Definition at line 128 of file DC1410AA.ino.
| enum Av |
| Enumerator | |
|---|---|
| unity | |
| g8 | |
| g16 | |
| g32 | |
| unity | |
| g8 | |
| g16 | |
| g32 | |
Definition at line 97 of file DC1410AA.ino.
| const uint8_t A_PIN = 4 |
Gain MUX pins.
Definition at line 121 of file DC1410AA.ino.
| const uint8_t B_PIN = 7 |
Definition at line 122 of file DC1410AA.ino.
default is gain 32
Definition at line 106 of file DC1410AA.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 100 of file DC1410AA.ino.
|
static |
Timeout in ms.
Definition at line 104 of file DC1410AA.ino.
|
static |
Keeps track when the filter needs to be rest.
Definition at line 105 of file DC1410AA.ino.
|
static |
The LTC2498 ideal reference voltage.
Definition at line 103 of file DC1410AA.ino.
| const uint8_t read_command_seq[] |
Lookup table for reads.
Channel read sequence for the demo board
Definition at line 110 of file DC1410AA.ino.
|
static |
lookup table for gain setting reads
The gain sequence for the auto calibration
Definition at line 116 of file DC1410AA.ino.
|
static |
The LTC2498 rejection mode settings.
Definition at line 102 of file DC1410AA.ino.
| const float smoothing_const = .7 |
Exponential filter smothing constant.
Definition at line 125 of file DC1410AA.ino.
|
static |
The LTC2498 2X Mode settings.
Definition at line 101 of file DC1410AA.ino.