![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1186A Demonstration Board. More...
Linear Technology DC1186A Demonstration Board.
LTC2302: 12-Bit, 1-Channel 500ksps SAR ADC with SPI Interface.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. No external power supply is required and it has an on-board reference voltage of 4.096V. The analog input is given at IN+ and IN-. There are options to chose between unipolar and bipolar modes. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2302
http://www.linear.com/product/LTC2302#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1339A.ino.
Go to the source code of this file.
Functions | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static void | menu_1_read_input () |
| Read ADC code and display the measured voltage. More... | |
| static void | menu_2_select_uni_bipolar () |
| Select unipolar (0-VREF) or bipolar (+/- 0.5 x VREF) mode. More... | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
Variables | |
| static uint16_t | uni_bipolar = LTC2302_UNIPOLAR |
| Default set for unipolar mode. More... | |
| static float | LTC2302_vref = 4.096 |
|
static |
Repeats Linduino loop.
Definition at line 95 of file DC1339A.ino.
|
static |
Read ADC code and display the measured voltage.
Definition at line 123 of file DC1339A.ino.
|
static |
Select unipolar (0-VREF) or bipolar (+/- 0.5 x VREF) mode.
Definition at line 138 of file DC1339A.ino.
|
static |
Prints main menu.
Definition at line 182 of file DC1339A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 166 of file DC1339A.ino.
|
static |
Initialize Linduino.
Definition at line 83 of file DC1339A.ino.
|
static |
Definition at line 80 of file DC1339A.ino.
|
static |
Default set for unipolar mode.
Definition at line 79 of file DC1339A.ino.