![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1333A Demonstration Board. More...
Linear Technology DC1333A Demonstration Board.
LTC2640: Single 12-/10-/8-Bit Rail-to-Rail DACs with 10ppm/C Reference Demonstration Circuit DC1333 features the 12-bit versions of the LTC2640.
Linear Technology DC1074A Demonstration Board. LTC2630: Single 12-/10-/8-Bit Rail-to-Rail DACs with Integrated Reference in SC70
NOTES
Setup:
Set the terminal baud rate to 115200 and select the newline terminator. The
program displays calculated voltages which are based on the voltage of the
reference used, be it internal or external. A precision voltmeter is needed to
verify the actual measured voltages against the calculated voltage displayed. If
an external reference is used, a precision voltage source is required to apply
the external reference voltage. A precision voltmeter is also required to measure
the external reference voltage. No external power supply is required. All four
demo board options may be used: DC1333A-A, DC1333A-B, DC1333A-C, or DC1333A-D.
Explanation of Commands:
1- Write to DAC input register: Value is stored in the DAC for updating later,
through a software "Update" command. User will be prompted to enter either a
code in hex or decimal, or a voltage. If a voltage is entered, a code will be
calculated based on the active scaling and reference parameters - ideal values
if no calibration was ever stored. (This is more often used with the
multichannel DACs in the family, where all DACs can be updated at once in
software or by asserting the LDAC# pin.)
2- Write and Update: Similar to item 1, but DAC is updated immediately.
3- Write to DAC: Sends the DAC code to the Input Register.
4- Update DAC: Copies the value from the input register into the DAC Register.
Note that a "write and update" command writes the code to BOTH the input
register and DAC register, so subsequent "update" commands will simply re-copy
the same data (no change in output.)
5- Power Down DAC: Disable DAC output. Power supply current is reduced. DAC code
present in DAC registers at time of shutdown are preserved.
6- Set reference mode: Either internal or external. Selecting external mode
prompts for the external refernce voltage, which is used directly if no
individual DAC calibration is stored. The selection and entered volgage are
stored to EEPROM so it is persisent across reset / power cycles.
7- Calibrate DAC: Use a precision voltmeter to obtain and enter VOUT readings
taken with different DAC codes. Set reference mode FIRST, as values are stored
separately for internal and external reference mode. Entries are used to
calculate the closest code to send to the DAC to achieve an entered voltage.
8- Enable / Disable Calibration: Switch between stored calibration values and
defaults. Calibration parameters are stored separately for internal and
external reference modes. Ideal calibration will be used if the calibration
parameter valid key is not set.
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0http://www.linear.com/product/LTC2640 http://www.linear.com/product/LTC2630
http://www.linear.com/product/LTC2640#demoboards http://www.linear.com/product/LTC2630#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1333A.ino.
Go to the source code of this file.
Functions | |
| static int8_t | restore_calibration () |
| Read stored calibration parameters from nonvolatile EEPROM on demo board. More... | |
| static void | store_calibration () |
| Store measured calibration parameters to nonvolatile EEPROM on demo board. More... | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static int16_t | prompt_voltage_or_code () |
| Prompt user to enter a voltage or digital code to send to DAC. More... | |
| static uint16_t | get_voltage (float LTC2640_lsb, int32_t LTC2640_offset) |
| static uint16_t | get_code () |
| Get code to send to DAC directly, in decimal, hex, or binary. More... | |
| static void | calibrate_dac () |
| Calibrate the selected DAC using a voltmeter. More... | |
| static void | menu_1_write_to_input_register () |
| Write data to input register, but do not update DAC output. More... | |
| static void | menu_2_write_and_update_dac () |
| Write data to DAC register (which updates output immediately) More... | |
| static void | menu_3_update_power_up_dac () |
| Update DAC with data that is stored in input register, power up if sleeping. More... | |
| static void | menu_4_power_down_dac () |
| Power down DAC. More... | |
| static void | menu_5_set_reference_mode () |
| Set reference mode and store to EEPROM. More... | |
| static void | menu_6_calibrate_dacs () |
| Calibrate all DACs by measuring two known outputs. More... | |
| static void | menu_7_enable_calibration () |
| Enable / Disable calibration. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static uint16_t | get_voltage (float LTC2640_lsb, int16_t LTC2640_offset) |
| Get voltage from user input, calculate DAC code based on lsb, offset. More... | |
Macros | |
| #define | EEPROM_CAL_KEY_INT 0x5678 |
| Calibration associated with internal reference. More... | |
| #define | EEPROM_CAL_KEY_EXT 0x9ABC |
| Calibration associated with external reference. More... | |
| #define | REF_INTERNAL LTC2640_CMD_INTERNAL_REFERENCE |
| Stored reference state is Internal. More... | |
| #define | REF_EXTERNAL LTC2640_CMD_EXTERNAL_REFERENCE |
| Stored reference state is External. More... | |
| #define | STORED_REF_STATE_BASE EEPROM_CAL_STATUS_ADDRESS |
| Base address of the stored reference state. More... | |
| #define | INT_CAL_VALID_BASE STORED_REF_STATE_BASE + 2 |
| Base address of the "internal ref calibration valid" flag. More... | |
| #define | INT_CAL_PARAMS_BASE INT_CAL_VALID_BASE + 2 |
| Base address of the internal ref calibration parameters. More... | |
| #define | EXT_CAL_VALID_BASE INT_CAL_PARAMS_BASE + 8 |
| Base address of the "external ref calibration valid" flag. More... | |
| #define | EXT_CAL_PARAMS_BASE EXT_CAL_VALID_BASE + 2 |
| Base address of the external ref calibration parameters. More... | |
| #define | EXT_REF_V_BASE EXT_CAL_PARAMS_BASE + 8 |
| Base address of the stored external reference voltage. More... | |
| #define | LSB_PARAM_ADDR_OFFSET 4 |
| Offset into XXX_CAL_PARAMS_BASE to locate stored LSB parameter. More... | |
Enumerations | |
| enum | { PROMPT_VOLTAGE = 0, PROMPT_CODE = 1 } |
| Used to keep track to print voltage or print code. More... | |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static uint8_t | shift_count = 4 |
| The data align shift count. More... | |
| static uint8_t | reference_mode |
| Tells whether to set internal or external reference. More... | |
| static float | reference_voltage |
| Reference voltage, either internal or external. More... | |
| static float | LTC2640_lsb = 1e-3 |
| DAC lsb. More... | |
| static int16_t | LTC2640_offset = 0 |
| DAC offset. More... | |
|
static |
Calibrate the selected DAC using a voltmeter.
The routine does a linear curve fit given two data points.
Definition at line 567 of file DC1333A.ino.
|
static |
Get code to send to DAC directly, in decimal, hex, or binary.
Definition at line 512 of file DC1333A.ino.
|
static |
|
static |
Get voltage from user input, calculate DAC code based on lsb, offset.
Definition at line 498 of file DC1333A.ino.
|
static |
Repeats Linduino loop.
Definition at line 211 of file DC1333A.ino.
|
static |
Write data to input register, but do not update DAC output.
Definition at line 261 of file DC1333A.ino.
|
static |
Write data to DAC register (which updates output immediately)
Definition at line 274 of file DC1333A.ino.
|
static |
Update DAC with data that is stored in input register, power up if sleeping.
Definition at line 286 of file DC1333A.ino.
|
static |
Power down DAC.
Definition at line 293 of file DC1333A.ino.
|
static |
Set reference mode and store to EEPROM.
Definition at line 300 of file DC1333A.ino.
|
static |
Calibrate all DACs by measuring two known outputs.
Definition at line 324 of file DC1333A.ino.
|
static |
Enable / Disable calibration.
Use with caution - behavior is undefined if you enable calibration and an actual calibration cycle has not been performed.
Definition at line 333 of file DC1333A.ino.
|
static |
Prints main menu.
Definition at line 540 of file DC1333A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 525 of file DC1333A.ino.
|
static |
Prompt user to enter a voltage or digital code to send to DAC.
Definition at line 482 of file DC1333A.ino.
|
static |
Read stored calibration parameters from nonvolatile EEPROM on demo board.
Definition at line 361 of file DC1333A.ino.
|
static |
Initialize Linduino.
Definition at line 180 of file DC1333A.ino.
|
static |
Store measured calibration parameters to nonvolatile EEPROM on demo board.
Definition at line 461 of file DC1333A.ino.
| #define EEPROM_CAL_KEY_EXT 0x9ABC |
Calibration associated with external reference.
Definition at line 127 of file DC1333A.ino.
| #define EEPROM_CAL_KEY_INT 0x5678 |
Calibration associated with internal reference.
Definition at line 126 of file DC1333A.ino.
| #define EXT_CAL_PARAMS_BASE EXT_CAL_VALID_BASE + 2 |
Base address of the external ref calibration parameters.
Definition at line 140 of file DC1333A.ino.
| #define EXT_CAL_VALID_BASE INT_CAL_PARAMS_BASE + 8 |
Base address of the "external ref calibration valid" flag.
Definition at line 139 of file DC1333A.ino.
| #define EXT_REF_V_BASE EXT_CAL_PARAMS_BASE + 8 |
Base address of the stored external reference voltage.
Definition at line 141 of file DC1333A.ino.
| #define INT_CAL_PARAMS_BASE INT_CAL_VALID_BASE + 2 |
Base address of the internal ref calibration parameters.
Definition at line 138 of file DC1333A.ino.
| #define INT_CAL_VALID_BASE STORED_REF_STATE_BASE + 2 |
Base address of the "internal ref calibration valid" flag.
Definition at line 137 of file DC1333A.ino.
| #define LSB_PARAM_ADDR_OFFSET 4 |
Offset into XXX_CAL_PARAMS_BASE to locate stored LSB parameter.
Definition at line 142 of file DC1333A.ino.
| #define REF_EXTERNAL LTC2640_CMD_EXTERNAL_REFERENCE |
Stored reference state is External.
Definition at line 133 of file DC1333A.ino.
| #define REF_INTERNAL LTC2640_CMD_INTERNAL_REFERENCE |
Stored reference state is Internal.
Definition at line 132 of file DC1333A.ino.
| #define STORED_REF_STATE_BASE EEPROM_CAL_STATUS_ADDRESS |
Base address of the stored reference state.
Definition at line 136 of file DC1333A.ino.
| anonymous enum |
Used to keep track to print voltage or print code.
| Enumerator | |
|---|---|
| PROMPT_VOLTAGE | 0 |
| PROMPT_CODE | 1 |
Definition at line 173 of file DC1333A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 163 of file DC1333A.ino.
|
static |
|
static |
DAC offset.
Definition at line 170 of file DC1333A.ino.
|
static |
Tells whether to set internal or external reference.
Definition at line 165 of file DC1333A.ino.
|
static |
Reference voltage, either internal or external.
Definition at line 168 of file DC1333A.ino.
|
static |
The data align shift count.
For 12-bits, shift_count = 4
Definition at line 164 of file DC1333A.ino.